Freedom development platform
  • Products
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Tutorial for FRDM-KL25Z: USB Host Mode Hack for the Freescale Freedom Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 8 Nov 2012 1:49 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:21 AM
  • Views 1536 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

Tutorial for FRDM-KL25Z: USB Host Mode Hack for the Freescale Freedom Board

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

 

  imageimage

 

 

 

On the FRDM-KL25Z Board the target processor supports both USB host and device mode. However, the Freedom board has no jumper or other means to power the USB bus (which is required in the USB host mode). So if I want to get access to a memory stick from the KL25Z, then I’m stuck because the board does not offer that option. Luckily there is an easy hack to work around this.


Looking at the FRDM-KL25Z board schematics, there is 5V available on Pin 10 of J9:

 

 

image

5V on J9 Pin 10 on FRDM-KL25Z Board

 

 

The idea is to power the USB bus with 5V DC from the board itself. Normally I would use an ADML869L or similar device to have stable voltage and over-current protection. But attaching a memory stick or similar should be safe and would be protected through the other circuits and through the protection on my host.

So all what I need is to connect the power supply line on the USB host side of the cable. I cut the cable to prevent the current to flow back, just in case.

Usually in a USB cable the red wire is the VBUS/5V one, which connects to pin 1 of the USB plug. Cutting that cable and connected it with a probe tip:

 

image

Probe Tip to VBUS

 

 

 

That probe tip then connects to pin 10 on J9:

 

image

Power from Pin 10 on J9

 

 

With this I can power devices on the USB bus, and I was able to enumerate a USB memory stick in USB MSD host mode on the KL25Z:

 

image

USB Host powered Memory Stick with the KL25Z Freedom Board

 

 

 

Happy Hosting :-)

  • freescale
  • kinetis
  • usb
  • frdm-kl25z
  • kinetis-l
  • power
  • freedom
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • royce_jp
    royce_jp over 13 years ago

    Please share the code used to access the pen-drive in host mode. Are there any examples of connecting usb mouse / keyboard etc. ? I'm new to ARM , so some example applications of this would be great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • royce_jp
    royce_jp over 13 years ago

    Please share the code used to access the pen-drive in host mode. Are there any examples of connecting usb mouse / keyboard etc. ? I'm new to ARM , so some example applications of this would be great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data