MEMS Sensors Evaluation Board
  • Products
  • Dev Tools
  • MEMS Sensors Evaluation Board
  • More
  • Cancel
MEMS Sensors Evaluation Board
Forum Reverse-engineered sensor.so with source
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join MEMS Sensors Evaluation Board to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 4 subscribers
  • Views 1226 views
  • Users 0 members are here
Related

Reverse-engineered sensor.so with source

Former Member
Former Member over 11 years ago

I have reverse engineered the sensor.so so that it can be compiled for V1.0 (and V2.0) Raspberry Pi Boards.

 

The source is available here: https://github.com/larsch/rpi-mems-sensor

 

I found that sensor.so is based on the bcm2835 library (bcm2835: C library for Broadcom BCM 2835 as used in Raspberry Pi), and is actually in full GPL violation. The sensor-specific function are quite simple though and mostly consist of the register numbers and bus addresses needed to talk to the chip. This could be implemented from scratch using the datasheet. The chips don't really require a "driver" when done this way, as the program basically talks on the I2C bus directly via the bcm2835 library.

 

I've kept it so that everything works the same as the original sensor.so and it is fully compatible with the original Python Scripts (get them from http://git.oschina.net/embest/rpi_sensor_board.git). It is working perfectly on my V1.0 board with all three sensors here, but note that the bcm2835 library needs to be compiled specifically for the V1.0 board.

  • Sign in to reply
  • Cancel
Parents
  • cyph3rpunk
    cyph3rpunk over 10 years ago

    Does anyone have an idea how to get the scripts working with Raspberry Pi 2? Even though the BCM2835 library should work with the Pi2 the resulting sensor.so makes the scripts hang - just like the included one :/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cyph3rpunk
    cyph3rpunk over 10 years ago

    Does anyone have an idea how to get the scripts working with Raspberry Pi 2? Even though the BCM2835 library should work with the Pi2 the resulting sensor.so makes the scripts hang - just like the included one :/