NI LabVIEW Community
  • Products
  • Dev Tools
  • NI LabVIEW Community
  • More
  • Cancel
NI LabVIEW Community
NI Forum PST.. A little project for the Pico SCPI labTool: resistor pass / fail test bed
  • Blog
  • LabVIEW Challenge Blogs
  • Forum
  • Documents
  • Quiz
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI LabVIEW Community to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 131 subscribers
  • Views 1247 views
  • Users 0 members are here
  • pico_usbtmc_scpi
  • labview
  • pico_usb_tmc
Related

PST.. A little project for the Pico SCPI labTool: resistor pass / fail test bed

Jan Cumps
Jan Cumps over 2 years ago

Let's imagine that you have to build a test jig for resistors. The task is to check if they are within tolerance. If the resistor is good, you have to put it in the "good" bin. The others ones need to be rejected.
You can build a LabVIEW process with the Pico SCPI labTool (PST) to run this process. It has the necessary ADC inputs that can be used to test the resistor, and outputs that can control status LEDS*.

Requirements:

  • check tolerance of a resistor. Is its value within range?
  • indicate yes or no
  • indicate if the test jig does not detect a resistor.

image

To test the resistor, you can use a divider, with a high precision known resistor and the "resistor under test" in series. You can sample the connection node with a LabVIEW driver ADC block.
Based on the sampled value, you can make the decision if it's within tolerance, and is allowed to be put in the "good" bin.

The GUI could look like this. The 3 cases are shown:
image

Connect LEDs with a series resistor to the PST digital outputs.
Connect the sample node to a PST analogue input.
Connect the high precision resistor to ground. 
Mount your "resistor under test" between 3.3V and the other side of the high precision one.

image

Flow suggestion:

image

Blocks that look like this are PST LabVIEW driver components:
image
Blocks used:
image
Everything else is out-of-box LabVIEW.

* in a industrial setup, this could be automated. Instead of LEDS, we'd use solenoids to push out-of-spec resistors in the rejected bin. Or sound a horn.
The on-screen button could be replaced by a footswitch or an optocoupler, that would spot if a new resitor is test ready (that is: when we finally implement "digital in" functionality)

 

link to all posts

  • Sign in to reply
  • Cancel
Parents
  • scottiebabe
    scottiebabe over 2 years ago

    Wow! 100

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 2 years ago

    Wow! 100