Atmel Xplained Boards
  • Products
  • Dev Tools
  • Atmel Xplained Boards
  • More
  • Cancel
Atmel Xplained Boards
Forum SAMA5D4 ADC driver - do you know a Linux image that has the driver?
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Atmel Xplained Boards requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 4 subscribers
  • Views 481 views
  • Users 0 members are here
Related

SAMA5D4 ADC driver - do you know a Linux image that has the driver?

Jan Cumps
Jan Cumps over 7 years ago

For the Enchanted Objects Design ChallengeI'm trying to get the ADC Hardware Trigger mechanism working.


I have difficulties with the ADC driver. I am unsure if the 4.7 and 4.6 linux Yocto Poky images have that driver installed.


I have 3 questions :


Is the ADC driver for the sama5d4 included in those Yocto Poky images?

If yes, what's the name of the driver (is it at91_adc)?

If no, is there an image around with the ADC included, or is there a way to get the driver installed on my board running that Yocto Poky image?

 

Here's the blog post that shows what I'm dong: Review 9b: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 2

 

I have issues when the buffer read tool generic_buffer tries to load the driver:

 

Here's where the code fails:

 

    /* Find the device requested */  
    dev_num = find_type_by_name(device_name, "device");  
    if (dev_num < 0) {  
        printf("Failed to find the %s\n", device_name);  
        ret = -ENODEV;  
        goto error_ret;  
    }  
    printf("iio device number being used is %d\n", dev_num); 

 

Error

Failed to find the at91_adc

  • Reply
  • Cancel
  • Cancel

Top Replies

  • noglitch
    noglitch over 7 years ago in reply to Jan Cumps +1 suggested

    Hi,

     

    Due to move to DT, the device name has changed. It is now "fc034000.adc" for this device. So, your command line should be:

    ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous …

  • noglitch
    noglitch over 7 years ago +1 verified

    FYI, I've just updated the Linux4SAM.org page:

    http://www.at91.com/linux4sam/bin/view/Linux4SAM/IioAdcDriver

    to reflect the changes in naming brought by a Device Tree system.

  • noglitch
    noglitch over 7 years ago in reply to Jan Cumps +1

    Oh thanks for the typo correction.

     

    I use the Linux4SAM 4.7 kernel + rootfs image.

    I took the  generic_buffer.c file in the linux-3.18-at91 kernel and compiled it with a Code Sourcery toolchain (Sourcery CodeBench…

  • noglitch
    0 noglitch over 7 years ago

    Hi,

     

    Here's a little bit more documentation about this topic:

    IioAdcDriver < Linux4SAM < TWiki

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to noglitch

    Hi,

     

    That is the guide that I'm following.

    I managed to run the Software Triggered example without any issue. That just works perfectly.

     

    I'm also trying to run the Hardware Triggerd method of that page.

    All steps from the linux command line work, and I can see that there's data in the /dev/iio:device0 character device when I do cat /dev/iio:device0

     

    But when I try to run the tool generic_buffer (I compiled it from source, as explained under 'Testing the buffer' section on that page), it fails.

     

    I used these commands:

     

    modprobe at91_adc
    echo 1 > /sys/bus/iio/devices/iio:device0/scan_elements/in_voltage0_en
    echo "fc034000.adc-dev0-continuous" > /sys/bus/iio/devices/iio:device0/trigger/current_trigger
    echo 100 > /sys/bus/iio/devices/iio:device0/buffer/length
    echo 1 > /sys/bus/iio/devices/iio:device0/buffer/enable

     

    When I run the self-compiled generic_buffer test tool, it fails when trying to find the device by the name 'at91_adc'

     

    ./generic_buffer -n at91_adc -t fc034000.adc-dev0-continuous -l 2

     

    Errors with 'Failed to find the at91_adc '.

     

    I'm not running from my own compiled distro , but have tried this process on the following two downloaded images:

    linux4sam-poky-sama5d4_xplained_hdmi-4.6

    and the new

    linux4sam-poky-sama5d4_xplained-4.7

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago

    It looks as if that at91_adc module is there, bacuase modprobing it works:

     

    root@sama5d4-xplained:~# modprobe at91_adc

     

    just returns

     

    When I give a fake name:

     

    root@sama5d4-xplained:~# modprobe at91_adb

     

    it errors: modprobe: FATAL: Module at91_adb not found.

     

    So that means that at91_adc is there...

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • noglitch
    0 noglitch over 7 years ago in reply to Jan Cumps

    at91_adc is actually compiled in the kernel (not as a module):

    https://github.com/linux4sam/linux-at91/blob/linux-3.18-at91/arch/arm/configs/sama5_defconfig#L237

     

    You can see it probed running this command:

    dmesg | grep  iio

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • noglitch
    0 noglitch over 7 years ago in reply to Jan Cumps

    Hi,

     

    Due to move to DT, the device name has changed. It is now "fc034000.adc" for this device. So, your command line should be:

    ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2

     

    It seems to work on my side:

    root@sama5d4-xplained:~# ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2
    iio device number being used is 0
    iio trigger number being used is 0
    /sys/bus/iio/devices/iio:device0 fc034000.adc-dev0-continuous
    281.000000 
    280.000000 
    274.000000 
    274.000000

    • Cancel
    • Up +1 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to noglitch

    Hi,

     

    I did try that,

    Your output is what I was expecting at my side too. I get a failure (using the 4.7.zip image at the moment)

     

    root@sama5d4-xplained:~# dmesg | grep  iio

    [    2.460000] iio iio:device0: Resolution used: 10 bits

    [    2.460000] iio iio:device0: ADC Touch screen is disabled.

     

     

     

    root@sama5d4-xplained:~# ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2

    Failed to find the fc034000.adc

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • noglitch
    0 noglitch over 7 years ago

    FYI, I've just updated the Linux4SAM.org page:

    http://www.at91.com/linux4sam/bin/view/Linux4SAM/IioAdcDriver

    to reflect the changes in naming brought by a Device Tree system.

    • Cancel
    • Up +1 Down
    • Reply
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to noglitch

    Hi,

    Is the image that you are using with the successful generic_buffer execution available somewhere in binary format?

     

     

     

    (there's a small typo in the command line , for the devtree and non-devtree explanations: ./generic-buffer -> ./generic_buffer)

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
  • noglitch
    0 noglitch over 7 years ago in reply to Jan Cumps

    Oh thanks for the typo correction.

     

    I use the Linux4SAM 4.7 kernel + rootfs image.

    I took the  generic_buffer.c file in the linux-3.18-at91 kernel and compiled it with a Code Sourcery toolchain (Sourcery CodeBench Lite 2014.05-29).

    • Cancel
    • Up +1 Down
    • Reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 7 years ago in reply to noglitch

    Success !!

     

     

    I've uploaded this image:

    ftp://www.at91.com/pub/demo/linux4sam_4.7/linux4sam-poky-sama5d4_xplained-4.7.zip

     

    I did use a different generic_code.c, just downloaded the one from https://github.com/linux4sam/linux-at91/blob/master/drivers/staging/iio/Documentation/generic_buffer.c

    (raw version:https://raw.githubusercontent.com/linux4sam/linux-at91/master/drivers/staging/iio/Documentation/generic_buffer.c)

     

     

    I'm using the GNU toolchain that comes with DS-5 Community Edition

     

     

     

    Invoking: GCC C Linker 4 [arm-linux-gnueabihf]'

    arm-linux-gnueabihf-gcc -static -marm -march=armv7-a -o "generic_buffer"  ./generic_buffer.o  

     

     

     

    Loaded to the board, and this is the result:

     

    root@sama5d4-xplained:~# ./generic_buffer -n fc034000.adc -t fc034000.adc-dev0-continuous -l 2

     

    iio device number being used is 0
    iio trigger number being used is 0
    /sys/bus/iio/devices/iio:device0 fc034000.adc-dev0-continuous
    1017.000000 437.000000 0.000000
    1017.000000 437.000000 119.000000
    1017.000000 437.000000 119.000000
    1017.000000 400.000000 119.000000

    Thank you!

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Cancel
>