Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog ADC on the Odroid
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mconners
  • Date Created: 23 Dec 2014 6:27 PM Date Created
  • Views 2601 views
  • Likes 3 likes
  • Comments 8 comments
  • wiringpi
  • single_board_computer
  • odroid
Related
Recommended

ADC on the Odroid

mconners
mconners
23 Dec 2014

One of the biggest features that the ODROID-C1 (odroid, from now on) has that is different than the Raspberry Pi B+ is the ADC. This is a welcome addition and will allow you to interface with analog sensors in a very simple way.

 

I figured I would use a photocell since I just finished doing a photocell blog project for the B+, so everything was in place.

 

The first thing I did was log into my odroid, and from my home directory type the following commands:

 

git clone https://github.com/hardkernel/wiringPi
cd wiringPi/
./build

 

This built and installed the wiringPi library on my odroid.

 

Next I opened my favorite code editor (not really, but I installed a pretty cool ide from the Lubuntu Software Store, CodeLite) and entered the following code:

 

#include <stdio.h>
#include <time.h>

#include <wiringPi.h>

#define PORT_ADC1   0 


int main (int argc, char *argv[])
{
    static int timer = 0 ;
  int adcValue;

    wiringPiSetup();

    for(;;)    {

        if (millis () < timer)  continue ;

        timer = millis() + 100;

        adcValue = analogRead(PORT_ADC1);

       printf("Value read is %d\n", adcValue);
    }

    return 0 ;
}

 

I attached the code below.

 

time to hook up the circuit:

 

I connected pin 1 of the Odroid to the + power rail on my breadboard

Pin 6 to the - Power rail

straddled a 1K resistor (any value will work) from the - rail to row 10

straddled a photocell over the channel in the middl on row 10

connected a jumper from the power rail to row 10 on the right side of the channel

connected a jumper from pin 40 of the odroid to row 10 of the bread board right between the photocell and the resistor

 

see the image below:

 

image

 

then I typed:

gcc -o photoSensor photoSensor.c -lwiringPi -lpthread

 

and finally:

 

sudo ./photoSensor

 

this gave me an ouput as follows:

 

 

image

 

That was with me waving my hand all above the sensor.

 

This is what the finished product looked like:

 

image

 

This wasn't intended to be a sophisticated project of any kind, just a quick example of how to use the ADC and the wiringPi libraries on the ODROID-C1.

Attachments:
photoSensor.c.zip
  • Sign in to reply

Top Comments

  • mconners
    mconners over 10 years ago in reply to e14 Contributor +2
    I haven't really done any heavy duty programming of the ADC on the Odroid, but there are a couple of forum posts here : ODROID Forum • View topic - Streaming ADC samples without gaps & low jitter ODROID…
  • mconners
    mconners over 11 years ago in reply to johnbeetem +1
    Hey, John, yes it's definitely possible to access those devices as a normal user if the permissions are properly setup. The easiest might be to execute something in the rc or init files during system startup…
  • mconners
    mconners over 11 years ago in reply to johnbeetem +1
    Also, just to answer the question more, I know you got a variety of answers on another post in the file /etc/rc.local you can put a line like chmod 666 /dev/foo and that will be executed on boot that will…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi Michael,

     

    Thanks for the adc example.

    I am new to odroid programming.

    What is the default sampling rate of adc?

    How do i decrease the sampling rate to 256Hz.

    Any help on this is highly appreciable.

    Thanks and Regards,

    sairam

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 10 years ago in reply to e14 Contributor

    I haven't really done any heavy duty programming of the ADC on the Odroid, but there are a couple of forum posts here :

     

    ODROID Forum • View topic - Streaming ADC samples without gaps & low jitter

    ODROID Forum • View topic - A/D inputs

     

    You may be able to find more info there.

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mconners
    mconners over 10 years ago in reply to e14 Contributor

    I haven't really done any heavy duty programming of the ADC on the Odroid, but there are a couple of forum posts here :

     

    ODROID Forum • View topic - Streaming ADC samples without gaps & low jitter

    ODROID Forum • View topic - A/D inputs

     

    You may be able to find more info there.

     

    Mike