• Experts & Guidance
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
    • 'Choose another store...'
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
Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog ODroid - Oh Boy!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Single-Board Computers requires membership for participation - click to join
Blog Post Actions
  • Subscribe by email
  • More
  • Cancel
  • Share
  • Subscribe by email
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mconners
  • Date Created: 23 Dec 2014 12:42 AM Date Created
  • Views 4585 views
  • Likes 10 likes
  • Comments 118 comments
  • odroid
  • c1
Related
Recommended

ODroid - Oh Boy!

mconners
mconners
23 Dec 2014

I recently picked up one of these little ODROID C1 development boards and i have to say I couldn't be happier!

 

It's a Quad Core ARM dev board based on the Amlogic S805 Cortex A5 processor with a Dual Core Mali 450 GPU. It comes with 1 GB of RAM and can can boot from 2 sources eMMC and Micro SD. $36.95 US.

 

It's layout looks very similar to the Raspberry Pi+, and it is almost the same size. Here is a picture of the 2 side by side:

 

image

 

Some of the features:

4 USB Host Ports

Micro Usb OTG Port

Micro HDMI Port

Gigabit ethernet over RJ45

IR Receiver (I guess that would be handy for a remote control if using as a streaming device)

40 Pin Expansion Port containing

2 - I2C Ports

Serial Port

19 GPIO Pins

2 ADC inputs

1.8V Analog reference

3.3 V Out

2 5V outputs

1 SPI Output

RTC with available battery backup.

 

A quick look at the pinout for both  the ODROID C1 and the Raspberry Pi shows they seem to match up with the exception of pins 37,38, and 40 on the ODroid are used for ADC.

 

It's also missing a few things the B+ has built in, like the camera interface, composite video out, discrete audio outputs, and the Display header.

 

This board will run Android or Ubuntu 14.04 LTS, both available from the Hardkernel site.

Installation of the Ubuntu image was a breeze, simply download it, dd the image to a Micro SD card, and boot. Detailed instructions are available on the Hardkernel site.

 

There is a root user and an odroid user, both seem to use the password odroid.

 

The Hardkernel site (as well as their US distributor) have a wide selection of inexpensive accessories for the odroid.

I was foolish and didn't purchase the power supply, which turned out to require a very small connector which was difficult to find. I was able to cobble together a plug using a Radio Shack Adaptaplug socket, a type A (2.5 mm) Adaptaplug tip, and an old phone charger I had lying around. But it would have been cheaper and easier to have purchased it initially from Ameridroid.

 

I did purchase the tinkerers kit which included a breadboard, a breakout board for the GPIO port, a ribbon cable, a bunch of resistors (like 100 or so, I didn't count), 6 tactile buttons, about a dozen LED's in rd green and yellow,  a Photocell sensor, and a bunch of connection wires.

 

The fact that it runs a modern version of Ubuntu makes me happy, the 14.04 LTS version is from April 2014 and since it is an LTS release it will be supported for several years. I run Ubuntu on my main computer and all my laptops, plus my RIoT Board so this thing will fit right in.

 

In conclusion I just have to say this is a great board, and for $35 US, it's tough to beat. My only words of caution are

1) Buy the power supply, it's worth it, or at least the pigtail connector they sell

2) Look on their site to see the limitations on Micro SD cards, they have some that perform better than others, I had one of the poor performers, it works but it is slow on boot

3) If you need a console, buy their USB uart module, they have a goofy molex connector for serial

 

Other than that, I can't complain.

  • Sign in to reply

Top Comments

  • mconners
    mconners over 8 years ago in reply to mconners +3
    With all four cores blazing, it only got up to about 35C. I'm not sure the heat sink is necessary. Mike
  • peteroakes
    peteroakes over 8 years ago +3
    Droid-C1 ordered, along with PSU, Serial Cable and HDMI adapter, now the few days of waiting begins , Oh and an LCD display (Why not) I looks like your all getting this thing to perform quite nicely so…
  • Problemchild
    Problemchild over 8 years ago in reply to johnbeetem +3
    Yes you are (H)alting the Odroid rather than also calling the power off so the power remains on to complete your USB transaction no doubt!! good solution ...nice and easy
Parents
  • Former Member
    Former Member over 8 years ago

    Thanks for the review! Sounds like a better option for a inexpensive genuine Linux computer compared to the Raspberry Pi. Minor sacrifices in add-ons (camera interface, composite video out) grant you more processing power and memory; gives you the ability to run Ubuntu for nearly the same cost as the Pi. Glad to know there's all of these options to raise my kid on!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 8 years ago in reply to Former Member

    Glad you liked it.

     

    I've got a Pi2 coming. I'll see how they compare.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 8 years ago in reply to mconners

    Michael Conners wrote:

     

    I've got a Pi2 coming. I'll see how they compare.

    I tried out a RasPi 2 the first time today.  It went very smoothly, and I really like the Raspbian 2015-02-16 GUI.

     

    I did some crude measurements compiling my own code (some in C, most in GalaxC) and found my ODROID-C1 to be about 20% faster.  This is consistent with the C1's faster clock (1.5GHz versus 900 MHz) and RasPi 2's faster ARM Cortex (A7 versus A5).

     

    My impression is that Chromium on ODROID-C1 is faster than Epiphany on RasPi 2.  However, I've got a USB hard disk on ODROID-C1 and a Class 10 SDcard on RasPi 2, so it's not a clean comparison.

     

    At this point I don't have a good reason to switch to RasPi 2 as my main computer, but it's nice to have it as a backup.  And I'm happy to support XXICC and Flavia on both.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mconners
    mconners over 8 years ago in reply to johnbeetem

    Good news, John. I don't know if you have been keeping up with the C1 software updates, but I noticed on their page recently

    http://odroid.com/dokuwiki/doku.php?id=en:c1_ubuntu_release_note_v1.4

    under the heading

     

    GPU acceleration on the Chromium Web browser

     

    they have instructions for speeding up chromium, so if you haven't done that, it may help even more.

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mconners
    mconners over 8 years ago in reply to johnbeetem

    Good news, John. I don't know if you have been keeping up with the C1 software updates, but I noticed on their page recently

    http://odroid.com/dokuwiki/doku.php?id=en:c1_ubuntu_release_note_v1.4

    under the heading

     

    GPU acceleration on the Chromium Web browser

     

    they have instructions for speeding up chromium, so if you haven't done that, it may help even more.

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data
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
An Avnet Company © 2023 Premier Farnell Limited. All Rights Reserved.