Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Odroid C0
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mconners
  • Date Created: 25 Feb 2016 1:29 PM Date Created
  • Views 1271 views
  • Likes 5 likes
  • Comments 8 comments
  • odroid
  • raspberry-pi
Related
Recommended

Odroid C0

mconners
mconners
25 Feb 2016

I recently picked up one of these sweet little boards, and I have to say I'm pretty pleased. It is a stripped down version of the Odroid C1+, designed to be lighter, and more configurable to suit your end purpose.

It is based on a quad core Amlogic S805 running at 1.5 GHz. It sports 1GB of RAM and both micro SD and emmc slots for storage. Oh, and did I mention it only costs $25. I have to give credit to the folks at ameridroid. I ordered this on a Wednesday night, and it was in my mailbox the following Friday, for ~$5 shipping.

 

Here it is compared to the Original Odroid C1:

 

image

 

As you can see it is quite a bit smaller than the C1 and it comes with most of the connectors unpopulated. The only installed connectors are HDMI, RTC battery, and LiPo connection. It also has an on/off switch.

 

The board does include the charging circuit for the LiPo battery. There is a connector pack available which contains the necessary connectors to fully populate the board. One improvement over the original C1 and what brings it closer to the C1+ is the addition of the I2S connector for high quality digital audio output. The connector pack contains the 40 pin GPIO header, the 7 pin I2S header, the serial connector, the IR receiver, and both a single and double USB connector that you can populate to suit your needs. The connector pack is available for an additional $2.95 and is well worth it. You can even choose to have Ameridroid install some or all of the components for a small fee, some as low as 40 cents.

 

The board boasts a reduction in weight from 40g to 16g, and a 24% reduction in overall board size.

 

The 40 pin GPIO connector pretty much matches up with the Raspberry Pi's connector, with the exception of the built in ADC pins. One of the ADC in pins is connected to the LiPo battery circuit to allow monitoring of the battery's capacity. The 7 pin I2S header matches up with the Odroid HiFi Shield, which features a TI (formerly Burr Brown) PCM 5102 DAC.

 

In addition the GPIO connector provides:

2 - I2C Ports

Serial Port

19 GPIO Pins

2 ADC inputs

1.8V Analog reference

3.3 V Out

2 5V outputs

1 SPI Output

 

The things that they removed from the board were the Gbit ethernet port, 2 USB ports, leaving 2 on board, and the USB OTG port.

 

I will have to say though, I'm not a big fan of their choice of power connector, the 2.5 mm barrel jack is not the easiest in the world to find, and when I first powered this board up I found I did not have a solid power connection and suffered from continuous reboots, but once I figured out the issue it has been rock solid ever since.

 

On my board the first connector I chose to populate was the serial console port, this allowed me to monitor the device on first boot and do some initial configuration. The second connector I chose to populate was the dual USB connector. With this in place I was able to connect a USB keyboard, mouse, and a Edimax WiFi adapter. Once all these things were installed I was able to boot up, connect to my network, update the OS and get started on my journey.

 

All in all I have to say I'm pretty happy with the board, bear in mind with it's light weight, reduced connectivity, and ability to be powered via LiPo battery, it's probably more targeted to be part of a specialized embedded solution that doesn't require networking, or as a wearable of some sort. I would expect, since it uses the same OS images as the C1 and C1+ that the expectation would be that prototyping your solution would be done on one of those devices then the resultant SD card could be placed in the C0 for deployment.

 

As this is pretty much a scaled down version of the C1+, most of the information in ODroid - Oh Boy! is directly relevant to this board, with the exception of the addition of the I2S connector, and the fact that the HDMI connector has been changed to the Type A standard full size connector.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago +2
    Hi Mike, Good to see the C0 innovation - love that it retains the battery charging capability on-board, really helps with portable applications. I feel your pain with the 2.5mm connector, it was the sole…
  • mcb1
    mcb1 over 9 years ago +2
    They are fast sending outside of the states as well. Luckily I ordered the connector kit (you had me worried) and battery, but I don't think I ordered the emmc card when I brought the C1. It will be interesting…
  • mconners
    mconners over 9 years ago in reply to mconners +2
    BTW, the C2's are available for pre-order on http://ameridroid.com Mike
Parents
  • shabaz
    shabaz over 9 years ago

    Hi Mike,

     

    Good to see the C0 innovation - love that it retains the battery charging capability on-board, really helps with portable applications.

    I feel your pain with the 2.5mm connector, it was the sole thing that irritated me on their U3 too.

    Nice that they supply a single and dual USB connector so you can decide which one you need!

    Also for some use-cases you could directly solder a small USB interfaced module and therefore only have one external USB connector I guess!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 9 years ago

    Hi Mike,

     

    Good to see the C0 innovation - love that it retains the battery charging capability on-board, really helps with portable applications.

    I feel your pain with the 2.5mm connector, it was the sole thing that irritated me on their U3 too.

    Nice that they supply a single and dual USB connector so you can decide which one you need!

    Also for some use-cases you could directly solder a small USB interfaced module and therefore only have one external USB connector I guess!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mconners
    mconners over 9 years ago in reply to shabaz

    shabaz wrote:

     

     

    Nice that they supply a single and dual USB connector so you can decide which one you need!

    Also for some use-cases you could directly solder a small USB interfaced module and therefore only have one external USB connector I guess!

    Yes, I thought the same thing.

     

    Mike