Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Resize an SD Card
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 30 Dec 2014 12:25 AM Date Created
  • Views 2082 views
  • Likes 3 likes
  • Comments 12 comments
Related
Recommended

Resize an SD Card

oneleggedredcow
oneleggedredcow
30 Dec 2014

Most of the single board computer images out there are set up for a 4GB SD card, but what if you have a 16 GB card?  When you fire up the image and check the disk size with:

 

df -h .

image

Sometimes it reports that the size of the drive is just 4GB, even though we know that the real size of the drive is 16GB.  Here’s how to change the partition sizes to use the entire space on the SD card.

 

Change Partition Size

I’m going to do this example on an OlinuXino, but the same procedure will work for a Raspberry Pi, SABRE Lite, or other single board computer.

 

To change the partition sizes, fire up the fdisk program:

 

sudo fdisk /dev/mmcblk0

 

Fdisk is a command line utility that allows you to change disk partition sizes.

 

Once inside the fdisk program, it will ask you for what command you want to do.  The first thing that we want to do is print the partition sizes, which is the “p” command:

image

Ok, now we want to delete the partition that currently exists.  Don’t worry, we are going to recreate partition in a second, but this time it is going to take up all of the available space.  If you have multiple partitions, delete the larger one.  Delete the partition with the “d” command:

image

Now, we go about creating a new (larger) partition.  This is done with the “n” command:

image

We want to create a new partition “n” that’s going to be a primary partition “p”, with the same partition number as whatever you deleted in the previous step.  This partition will have the default start position, so just press enter for that question.  We also want the default stop position, which will be to use up all of the disk space.

 

After the new partition is defined, we need to write that to disk with the “w” command.  This will also exit us out of the fdisk program.

image

Now that we have the new allocations defined, in order for them to take effect, we need to restart the board:

 

sudo shutdown –r now

 

When the reboot has completed, we need to do one more command to finish the resizing:

 

sudo resize2fs /dev/mmcblk0p<#>

 

Where <#> is the number of the partition that you deleted and recreated.  Once that completes, then we can check the disk size with:

 

df -h .

image

And see that our OS has expanded to fill the entire microSD card.  Great success!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to gadget.iom +1
    You can achieve the same result using raspi-config. I think you'll find NOOBs already expands the SD card. Mark
  • Problemchild
    Problemchild over 11 years ago +1
    Shaun when you expand the filesystem like this you will be able to extend the last partition on the card as you wont be able to expand the earlier ones past the preexisting partitions, if your large data…
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1 +1
    You win Mark ...... but he is been generic for any old FS on any old board rather than just RPI This seems to be some Olimex board in this case. As I said before I'd use "parted" mainly so you have less…
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    That's a really helpful article oneleggedredcow Thanks! image

     

    A quick note for all the Raspberry Pi users out there... You can achieve the same result using raspi-config.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to gadget.iom

    You can achieve the same result using raspi-config.

    I think you'll find NOOBs already expands the SD card.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1

    Yes Mark by performing this operation but you have to select it as I remember!

    Obviously this is the general case on any lump of hardware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Problemchild

    No selection required...

    image

    http://www.raspberrypi.org/documentation/configuration/raspi-config.md

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago in reply to Problemchild

    No selection required...

    image

    http://www.raspberrypi.org/documentation/configuration/raspi-config.md

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1

    You win Mark image...... but  he is been generic for any old FS on any old board rather than just RPI This seems to be some Olimex board in this case.

    As I said before I'd use "parted" mainly so you have less opportunity to screw it up.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Problemchild

    Not about winning .... just ensuring that new users don;t receive even more 'misinformation' ...image

     

    Even more painful is if you copy the contents to a larger card, you can't resize it due to how they put the various partitions onto the card.

    So always use the biggest card you think you'll need first.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to mcb1

    Yeah this is obviously not even consistent between various releases of say Noobs vs Rasbian. I'm certain older versions used to have the menu selection any way I've just installed the 24/12 Rasbian and it does ask you thus my assumption that NOOBS  did as well. Any way it seems to be wrong to assume that he's using NOOBs /Rasbian or anything in this context since it's an Olimex part he's working withimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to Problemchild

    Problemchild

    John

    NOOBs installs Raspbian onto the SD card, which does the expanding as part of the process.

    It installs the normal raspbian menus, utilities and of course raspi-config is available.

    Unfortunately even if you copy it all to a new card that has more room you still can't expand it, so there must be a flag set somewhere.

     

    Mark