Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BeagleBoard.org releases Debian for BeagleBone Black
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 61 subscribers
  • Views 4033 views
  • Users 0 members are here
  • debian
  • beaglebone_black
  • open_source
  • sbc
  • single_board_computer
  • oshw
  • bbb
  • BeagleBone
  • beagleboardorg
  • open_hardware
  • bb_black
  • open_source_hardware
  • linux
Related

BeagleBoard.org releases Debian for BeagleBone Black

fustini
fustini over 11 years ago

image

I think this is great news for the usability of BBB, BeagleBoard.org has released Debian image for the BeagleBone Black!

 

BeagleBoard.org - latest-images

BeagleBone (Runs on BeagleBone Black as well without flashing the eMMC)

  • Debian (BeagleBone, BeagleBone Black - 2GB SD) 2014-03-04 - more info - bittorrent
  • Angstrom Distribution (BeagleBone, BeagleBone Black - 4GB SD) 2013-06-20 - more info

BeagleBone Black (eMMC flasher)

  • Debian (BeagleBone Black - 2GB eMMC) 2014-03-04 - more info - bittorrent
  • Angstrom Distribution (BeagleBone Black - 2GB eMMC) 2013-09-04 - more info - bittorrent

BeagleBoard and BeagleBoard-xM

  • Angstrom Distribution (BeagleBoard and BeagleBoard-xM) 2012-01-11 - more info

 

Anyone else excited, too?

 

Cheers,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +1
    Definitely :-) The Angstrom was such a sore point, any other build would have been better. I've only tried the earlier pre-release Debian builds, they were missing a lot of packages, hopefully they are…
  • shabaz
    shabaz over 11 years ago in reply to gihu +1
    Hi Miguel, If it is the debian image from here , then the following credentials can be used: uasername: debian password: temppwd I can't recall what the root password was, but it was either root, temppwd…
  • dennisc
    dennisc over 11 years ago in reply to gihu +1
    Hi Gihu, The root terminal application does not work correctly and will be removed from future releases of Debian. It requires a root password to be entered, and none is assigned by default. You can get…
Parents
  • gihu
    gihu over 11 years ago

    Hi all,

     

     

    I have not found where to put my question,and I have almost no idea of linux...

    I have the Angstrom image on the eMMC, and I boot the debian image from the sd card (no cape used, just keyboard, mouse and a TV connected in the HDMI), the debian starts as a user, and if I want to start root terminal, it asks for a password. Does anyone know that password?

    What I am doing by now is logging out, and after that logging in as root. Is it posible that the debian starts as root instead of user?

     

    I hope any of us can help me.


    Regards,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to gihu

    Hi Miguel,

     

    If it is the debian image from here, then the following credentials can be used:

    uasername: debian

    password: temppwd

     

    I can't recall what the root password was, but it was either root, temppwd or no password was set.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago in reply to gihu

    Hi Miguel,

     

    If it is the debian image from here, then the following credentials can be used:

    uasername: debian

    password: temppwd

     

    I can't recall what the root password was, but it was either root, temppwd or no password was set.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gihu
    gihu over 11 years ago in reply to shabaz

    Thanks shabaz,

     

    The problem is that I cannot use the root terminal, and I don't know if I have the same permissions with the user debian than as a root (I suppose not). I am starting with Linux and sometimes not always I understand how things works... image

    For example, If I try to modify the uEnv.txt file from the desktop envoirement I have in return a no permission message, just to be able from the Desktop I have to log out, and log in as a root.

     

    Fortunately, here in element14 there is quite information about linux in single-board, as BBB

     

    Regards,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to gihu

    Hi Miguel,

     

    I wasn't sure, do you mean you can successfully log in as user debian, but not as root?

    If so, you can execute any root user command by typing 'su' once you're logged in as user debian, from the command line. If you run any program from the GUI that needs root access, it will prompt you for the root password.

    Most of the time you won't want to be root user, and when you do (e.g. to install a program) you can use the 'su' command to become root user.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gihu
    gihu over 11 years ago in reply to shabaz

    Hi Shabaz,

     

    The BBB starts as user (debian image), and if I want to use the root terminal from the GUI, it asks for a password, or even if I try to use 'sudo' in the terminal (not the root one), it also asks for password, and no password is supposed to be set.

    Althouth it is not a big deal.

    What I am doing now is using the debug header, or connect to the BBB from a putty on my PC over the ethernet port on the BBB.

     

    Thank you very much!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dennisc
    dennisc over 11 years ago in reply to gihu

    Hi Gihu,

     

    The root terminal application does not work correctly and will be removed from future releases of Debian. It requires a root password to be entered, and none is assigned by default.

     

    You can get a root login by logging out of the LXDE environment and logging in again as root (with no password). Now you can run GUI apps as root.

     

    I find the default user works best for most things, and sudo works for most things when you need root privledges. If you need a root terminal you can use "sudo su" to get root access, then exit to return to the debian user access. You can run gui apps from the root terminal using the command line, i.e. leafpad filename (editor) or pcmanfm (file manager).

     

    HTH

    Dennis Cote

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gihu
    gihu over 11 years ago in reply to dennisc

    Yeah Dennis!! That is what I am doing by now logging in as a root in the LXDE environment. Changing files like uEnv.txt needs root priviledges, and they are easier to deal with over GUI than over terminal...

     

    Thank you!!