GIZMO 2
  • Products
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Blog Gizmo2: 3D Printable Enclosure - First Iteration
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 26 Jan 2015 9:39 PM Date Created
  • Views 2202 views
  • Likes 0 likes
  • Comments 11 comments
  • enclosure
  • gizmo2
  • 3dprinting
  • printrbot
Related
Recommended

Gizmo2: 3D Printable Enclosure - First Iteration

fvan
fvan
26 Jan 2015

  • Introduction
  • Design
  • Print

 

Introduction

 

To protect my brand new GIZMO 2 board from the pointy and metal objects (and the rest of the mess) scattered around my desk, I decided to design a simple 3D printable enclosure for it, which would still expose all interfaces. I'm no professional designer, so it's more a functional enclosure rather than a fancy looking one image

 

I took various measurements of the board, especially around the ports and started porting this to SketchUp.

 

Design

 

This is what the first version of the design looks like:

imageimage

As I said, the focus is more on the functional side of things. The enclosure has following "features":

  • access to microSD card
  • 1cm standoffs, allowing room for mSATA/mini PCIe device
  • opening for high and low speed card edge connectors
  • opening for all ports: power, hdmi, USB3, audio, USB2 & ethernet
  • removable lid with an opening for the fan

 

I've attached the SketchUp files to this post in case anyone wants to build further from this. After printing, I'll check which adjustments need to be made and

 

Print

 

Having finalised a first version of the model, I tried to print it. The heated bed on my Printrbot was barely large enough, but it fit.

 

I enabled support material when slicing the model because of the many openings. After printing, I was able to easily remove it using small pliers.

There was a little lifting during printing, so the enclosure isn't totally straight, but it's still functional.

 

Here it is, in all its glory:

imageimageimage

Power, USB and Ethernet access is OK. HDMI and audio are a bit off. I'll have to work on that for the next iteration.

 

Hope you like it! Feel free to provide feedback on the enclosure or make your own based on the files attached.

Attachments:
gizmo-bottom.skp.zip
gizmo-top.skp.zip
  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 11 years ago +1
    A nice simple design, I like it... You have beat me to it I have been designing one using OpenSCAD and currently printing first prototype as I write this.
Parents
  • fvan
    fvan over 10 years ago

    Also, keep in mind this as a firs version of a case, I have yet to apply some improvements and corrections. As can be seen in the pictures of the printed case, I had to adapt the opening for the audio jack. You might want to consider Brian's case which appears to be more professional image GIZMO 2 another 3D printed enclosure

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to fvan

    I tried the other design too but same problems (Worse actually) probably due to the very thin walls and no base on the middle part, the top and bottom have minimal curl but it is there

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 10 years ago in reply to Robert Peter Oakes

    Yes the thin walls of my middle part have less area in contact with the bed so are easier to pull off and curl due to the thermal contraction forces as the upper layers cool. Adding a brim helps this as long as the brim has good adhesion to the bed. Keeping the lower layers soft and flexible with a heated bed and a higher ambient temperature helps with this too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bwelsby
    bwelsby over 10 years ago in reply to Robert Peter Oakes

    Yes the thin walls of my middle part have less area in contact with the bed so are easier to pull off and curl due to the thermal contraction forces as the upper layers cool. Adding a brim helps this as long as the brim has good adhesion to the bed. Keeping the lower layers soft and flexible with a heated bed and a higher ambient temperature helps with this too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data