• Experts & Guidance
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
    • Or choose another store...
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
GIZMO 2
  • Products
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum Can the Gizmo 2 Explorer Board be used in place of Arduino Uno?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
GIZMO 2 requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 6 subscribers
  • Views 705 views
  • Users 0 members are here
Related

Can the Gizmo 2 Explorer Board be used in place of Arduino Uno?

monkeyman_stones
monkeyman_stones over 5 years ago

I recently purchased an XYZPrinting da Vinci 2.0 Duo 3D printer and had to replace the cartridges multiple times already at an unreasonable price ($78) for what is only 300G of filament (versus $15 for Inland PLA & ABS 1KG rolls from Micro Center).

I have discovered multiple pages for the resetting of the cartridges and the use of aftermarket filament by way of an Arduino Uno R3. But I own 2 Gizmo 2's with Explorer Boards and it seems likely that they can be used in place of an Arduino Uno. But I have no idea how...

Does anyone know how to use the Gizmo 2 and Explorer Board in place of an Arduino Uno R3 for resetting XYZ Printing cartridges?

 

Thanks for the help,

 

David

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 5 years ago

    The chances of finding someone not only with a 'XYZ Printer', but someone who resets the cartridges with a (approx) $150 'Gizmo 2' board and a Gizmo Explorer card, instead of a $20 Arduino Uno are surely quite slim. So I doubt you'll find that.

     

    Having said that, the Arduino Uno is a (fairly basic) microcontroller, and the Gizmo2 works fast enough that it could likely be used for the task, but it would involve translating the code to run on X86 and your desired OS (e.g. Linux). That's a porting exercise, and it will involve finding out how to control I/O with Gizmo2, and inserting that code into the Arduino code and re-compiling for X86. It is non-trivial if you've not done this before - and harder still if the Arduino code uses things like timers and interrupt functions, because these do not translate into code on (say) Linux in the same way, so you'd also need to understand the Arduino code intent as you're porting it.

     

    So, in summary, I'm (fairly) sure it is possible, but to do it will need a porting exercise because I doubt anyone else has done it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 5 years ago

    The chances of finding someone not only with a 'XYZ Printer', but someone who resets the cartridges with a (approx) $150 'Gizmo 2' board and a Gizmo Explorer card, instead of a $20 Arduino Uno are surely quite slim. So I doubt you'll find that.

     

    Having said that, the Arduino Uno is a (fairly basic) microcontroller, and the Gizmo2 works fast enough that it could likely be used for the task, but it would involve translating the code to run on X86 and your desired OS (e.g. Linux). That's a porting exercise, and it will involve finding out how to control I/O with Gizmo2, and inserting that code into the Arduino code and re-compiling for X86. It is non-trivial if you've not done this before - and harder still if the Arduino code uses things like timers and interrupt functions, because these do not translate into code on (say) Linux in the same way, so you'd also need to understand the Arduino code intent as you're porting it.

     

    So, in summary, I'm (fairly) sure it is possible, but to do it will need a porting exercise because I doubt anyone else has done it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data
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
An Avnet Company © 2023 Premier Farnell Limited. All Rights Reserved.