BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Black Wireless in Altoids Mint Tin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ninjatrent
  • Date Created: 20 Jul 2017 12:48 AM Date Created
  • Views 1891 views
  • Likes 6 likes
  • Comments 4 comments
  • debian
  • octavo
  • iot server
  • texas insruments
  • debian jessie
  • embedded linux
  • internet of things
  • iot platform
  • beagle
  • beagle bone black
  • beagle-bone-black
  • linux software dev
  • beagle_bone
  • iot design
  • beagle bone
  • beagle_bone_black
  • arm
  • ti sitara
  • raspbian jessie
  • BeagleBone Black
  • beagleboneblackwireless
  • raspbian
  • ti
  • beaglebone_black_wireless
  • linux
Related
Recommended

BeagleBone Black Wireless in Altoids Mint Tin

ninjatrent
ninjatrent
20 Jul 2017

BeagleBone Black Wireless in an Altoids Mint Tin

 

image

Curiously Stong Mints? No, but it is quite powerful. It's a BeagleBone Black Wireless!!!

image

The Adafruit Proto Cape Kit fits with lid fully closed. In order to accommodate additional components

such as sensors, wiring, and others things, it will be necessary to find some Nylon Polyamide Standoffs

that are shorter than the 3/16" standoffs used in the photos.

These are the standoffs that came with the Adafruit BeagleBone Proto Plate. 

image

Custom 27mm x 27mm heatsink. Note, the BBB W does not require a heatsink.

This heatsink was hand cut from one that originally came on a PCI graphics card for a desktop PC.

image

The holes for the dual antennas to pass through are marked but not drilled yet.

Currently I am shopping for the correct adapters to utilize different antennas.

The ones that come from the manufacturer are more than sufficient for most applications but

my intended use requires an antenna configuration with greater range.

image

The mounting hardware that was used came from the Adafruit Proto Plate kit.

If you would like to purchase the mounting hardware separately,

the dimensions are as follows:

 

    4 x 4-40 1/2" Metal or Nylon Polyamide Screws

      4 x 4-40 Metal or Nylon Polyamide Hexnuts

      4 x 3/16" Nylon Polyamide Standoffs *

 

*This height will work if the Micro USB is used for power.

If you desire to use the 5V power jack, a shorter standoff must be used.

  • Sign in to reply

Top Comments

  • fvan
    fvan over 8 years ago +1
    How much does the tin impact the wifi signal?
  • ninjatrent
    ninjatrent over 8 years ago in reply to fvan +1
    It has not been tested yet. I still need to cut the holes for the antenna and power cord. It should work fine. I plan to install larger antennas with a separate ferrite ring for each in place of the factory…
Parents
  • fvan
    fvan over 8 years ago

    How much does the tin impact the wifi signal?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fvan
    fvan over 8 years ago

    How much does the tin impact the wifi signal?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ninjatrent
    ninjatrent over 8 years ago in reply to fvan

    It has not been tested yet. I still need to cut the holes for the antenna and power cord. It should work fine. I plan to install larger antennas with a separate ferrite ring for each in place of the factory antenna. I have anticipated there might be issues of interference and or signal strength with the factory antennas.  The ferrite rings should work to prevent interference and the new larger antennas will provide about 5 db gain. I should have the tin complete today.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago in reply to fvan

    I have to make another tin. Also the 3/16" polyamide nylon standoffs are too tall. I will have to order some that are shorter. Everything was looking good until I closed the lid. The 5v power jack is covered partially by the lid. The Micro USB port will power the BBB W also but I have chosen a power supply with the barrel plug for more durability. Thankfully I have a few more Altoids tins. This could have been avoided. It is a reminder for me to finally purchase a caliper for measurement.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.