BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Control Stepper Motors with PRU - Part 5: It Works
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 2 Aug 2019 5:58 PM Date Created
  • Views 2542 views
  • Likes 5 likes
  • Comments 4 comments
Related
Recommended

BeagleBone Control Stepper Motors with PRU - Part 5: It Works

Jan Cumps
Jan Cumps
2 Aug 2019

I'm trying here is to let the real-time units of the BeagleBone generate the signals for a stepper motor.

In this post: it works! Let's put everything together.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Initialise the Sleep and Reset Signals

 

The pins P9_11 and P9_13 are used. I'm controlling them from the Linux command line.

 

BB MUXBB P9Driver function
GPIO_3011nSleep
GPIO_3113Reset

 

To start, set sleep on and reset off

 

sudo -i

# sleep on

echo out > /sys/class/gpio/gpio30/direction
echo 0 > /sys/class/gpio/gpio30/value

# reset off

echo out > /sys/class/gpio/gpio31/direction
echo 0 > /sys/class/gpio/gpio31/value

 

Set the PRU MUX signals and Load PRU Firmware

 

See the post on pin assignments for the PRU. I'm assuming that you created the binary in this post.

 

config-pin P9_31 pruout  
config-pin P9_29 pruout 

 

cp /home/debian/bin/bb_PRU_STEPPER.out /lib/firmware/bb_PRU_STEPPER.out  
echo 'bb_PRU_STEPPER.out' > /sys/class/remoteproc/remoteproc1/firmware  
echo 'start' > /sys/class/remoteproc/remoteproc1/state 

 

Initialise the Stepper Motor Driver via SPI

 

I'm assuming that you installed the SPI overlay as explained in this post and created the binary in this post.

 

/home/debian/bin/bb_LINUX_STEPPER_SPI

 

 

Wake Up the Stepper Motor Driver

 

# sleep off

echo 1 > /sys/class/gpio/gpio30/value

 

At this point everything is prepared, and you are ready to ....

 

Tell PRU to Step the Motor

 

This is it! Let's take 20 steps back and forth:

 

echo "120" > /dev/rpmsg_pru30  
echo "020" > /dev/rpmsg_pru30 

 

 

Submit as many commands as you want.

 

Motor Heat

Once you disable sleep mode, the motor will pull 600 mA. It's locked in position. It will get hot.

If you don't play with the motor, or your device doesn't need the motor be kept locked in position, put the driver back to sleep:

 

cd /sys/class/gpio/gpio30  
echo 0 > value 

 

 

 

 

Finished? Clean Up.

 

echo 'stop' > /sys/class/remoteproc/remoteproc1/state 

 

config-pin P9_31 default  
config-pin P9_29 default 

 

 

Related blog:
BeagleBone Control Stepper Motors with PRU - Part 1: Intentions
BeagleBone Control Stepper Motors with PRU - Part 2: Test Driving Outputs
BeagleBone: Enable SPI with Overlay and from Command Line
BeagleBone Control Stepper Motors with PRU - Part 3: Hardware Provisioning and Wiring
BeagleBone Control Stepper Motors with PRU - Part 4: SPI Setup
BeagleBone Control Stepper Motors with PRU - Part 5: It Works
  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Great finish Jan. DAB
  • Jan Cumps
    Jan Cumps over 6 years ago +1
    The evaluation software for the DRV8711 stepper motor controller kit is very good. You can use it to test the driver IC (you need a MSP-EXP430G2 MSP-EXP430G2 LaunchPad but that one is cheap) You can set…
Parents
  • Jan Cumps
    Jan Cumps over 6 years ago

    The evaluation software for the DRV8711 stepper motor controller kit is very good.

    image

     

    You can use it to test the driver IC (you need a MSP-EXP430G2MSP-EXP430G2 LaunchPad but that one is cheap)

     

    You can set motor control parameters. They are dependent on the (current of the) motor you have,

    Several scenarios can be validated and played with.

    This helps to better understand the datasheet.

    It documents all the register settings and what they do. But getting smooth operation is not that easy by just staring at a PDF.

    With the GUI, you can observe the motor behaviour, and then check what configuration settings were applied to the driver:

    image

     

    You can also evaluate the other way around. If you know the register values that a particular firmware uses, you can enter those values in the GUI.

    The registers are broken up in their meaningful entities. There's support to show the raw HEX values.

     

    You can change the registers in the GUI and write them to the driver IC. You can see the motor's behaviour under the circumstances directly.

    This works more intuitive than changing the code and running the firmware again.

    It also helps to find out what the maximum reliable speed is for your motor in a particular application and what an acceptable acceleration rate looks like.

     

    I used this program in this blog series to set up a smooth full-step motor pattern and to see what frequencies and accelerations are OK for my motor.

    It's part of the next step in the series, where I'll try to let the BB PRU calculate a nice smooth trapezoid velocity ramp.

     

    image

     

    Real good evaluation utilities can give a head start. This GUI has done that in the past when I developed for the programmable timer controller of a Hercules MCU.

    I'm using (and appreciating) it again now for the BeagleBone's PRU programming.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago

    The evaluation software for the DRV8711 stepper motor controller kit is very good.

    image

     

    You can use it to test the driver IC (you need a MSP-EXP430G2MSP-EXP430G2 LaunchPad but that one is cheap)

     

    You can set motor control parameters. They are dependent on the (current of the) motor you have,

    Several scenarios can be validated and played with.

    This helps to better understand the datasheet.

    It documents all the register settings and what they do. But getting smooth operation is not that easy by just staring at a PDF.

    With the GUI, you can observe the motor behaviour, and then check what configuration settings were applied to the driver:

    image

     

    You can also evaluate the other way around. If you know the register values that a particular firmware uses, you can enter those values in the GUI.

    The registers are broken up in their meaningful entities. There's support to show the raw HEX values.

     

    You can change the registers in the GUI and write them to the driver IC. You can see the motor's behaviour under the circumstances directly.

    This works more intuitive than changing the code and running the firmware again.

    It also helps to find out what the maximum reliable speed is for your motor in a particular application and what an acceptable acceleration rate looks like.

     

    I used this program in this blog series to set up a smooth full-step motor pattern and to see what frequencies and accelerations are OK for my motor.

    It's part of the next step in the series, where I'll try to let the BB PRU calculate a nice smooth trapezoid velocity ramp.

     

    image

     

    Real good evaluation utilities can give a head start. This GUI has done that in the past when I developed for the programmable timer controller of a Hercules MCU.

    I'm using (and appreciating) it again now for the BeagleBone's PRU programming.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.