BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BBONE-BLACK-WIRELESS and BB-CAPE-DISP-CT43
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 102 subscribers
  • Views 1067 views
  • Users 0 members are here
Related

BBONE-BLACK-WIRELESS and BB-CAPE-DISP-CT43

teddytronix
teddytronix over 5 years ago

Hello,

I am trying to figure out if the two products in the subject line are compatible without having to jump through those proverbial hoops: the element14 BeagleBone Black Wireless with WiFi & Bluetooth, and the Beaglebone Black Touchscreen Display.

 

Both are currently available at CPC under order codes, respectively, SC14310 and SC14039.

 

I have been reading through a variety of documents, but I am still struggling to come up with a definitive answer. On the CPC site it says, for the touch screen, "connects directly to your BeagleBone" and "plug-and-play functionality with the default Debian operating system". On element14 it states "*PLEASE read the folowing notice regarding product compatibility with BeagleBone Black." which then reveals that firmware updates are required as the element14 B'Bone is different to a standard one. There is then a comment stating that after the firmware upgrade the wireless and bluetooth will not work any longer. Confusing :-)

 

Some documents appear several years old, but I cannot find any notice if they have been superseeded. Or, indeed, found any more recent versions.

 

So, can I just connect SC14310 and SC14039, i.e. element14 BeagleBone Black Wireless with WiFi & Bluetooth and Beaglebone Black Touchscreen Display, to work out-of-the-box(es), or are mods like firmware updates required?

 

After any updates, will all subsystems be functional?

 

Many thanks, for your time,

Teddy

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 5 years ago +3 suggested
    The 'problem' is that you'll have to set this up manually for it to work, basically you need the code / device tree overlay from the image available at 4.3 LCD Display Cape for Beaglebone Board (White…
  • teddytronix
    teddytronix over 5 years ago in reply to cstanton +2 suggested
    Hi Christopher, thanks for the pointers and especially the link to the overlay. Good to see that there is lots of info, too. I have just bought both after realising that they are on very special offer…
  • shabaz
    shabaz over 5 years ago +1 suggested
    Hi Teddy, I don't have these so I'm slightly speculating (and hopefully anyone who owns these and with better information can step in), but I think it's best to assume that it will not be plug-and-play…