BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Need an example of  SPI- TFT touchscreen for pocketbegle
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 5 answers
  • Subscribers 104 subscribers
  • Views 5044 views
  • Users 0 members are here
  • TFT LCD
  • pocketbeagle
  • linux
Related

Need an example of  SPI- TFT touchscreen for pocketbegle

chrischristian14
chrischristian14 over 4 years ago

Hi, I am after adding a touchscreen TFT display to pocketbeagle.

I am already using I/O in C via iobb library, so I am not sure if using a TFT LCD with fbtft driver will conflict with iobb.

There are lot of LCDs available for RPi which should work for pocketbeagle but I am not sure

- How to install fbtft driver - as a module, not built with kernel, I mean use insmod after bootup

- How to modify the driver to tell it to use a specific SPI connectors and how to make sure the driver doesn't mess up existing I/O configuration.

- What are the steps to redirect Xfce environment to the LCD

- And of course the hardware connection.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 4 years ago in reply to chrischristian14 +2 suggested
    Hi Chris, Are you sure about this, because it seems odd to me that a GPU is needed for a driver for SPI to read the normal framebuffer. I'm no expert on it either, so don't want to mislead you if you're…
  • geralds
    geralds over 4 years ago in reply to chrischristian14 +2
    Hi, please look here: Home - Nextion Nextion displays may a solution. They have a controller and communicate via serial connections. But.... it is not cheap because you need something to realise your application…
  • chrischristian14
    chrischristian14 over 4 years ago in reply to geralds +2
    Thanks Gerald, I'll check it out.
  • chrischristian14
    0 chrischristian14 over 4 years ago in reply to geralds

    Hi Gerald,

    Yes the gamepup looks good too, Is my understanding right that all I need to do is add overlay ? as per this wiki ?

    https://github.com/beagleboard/pocketbeagle/wiki/GamePup-capehttp://

    How would I edit it for a different size LCD ? If it is the same as shabaz mentioned then, I might just start from scratch rather than spending anything on this board.

    Thanks,

    Chris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrischristian14
    0 chrischristian14 over 4 years ago in reply to chrischristian14

    I found the information I'll follow this and see where I get.

    https://github.com/Mouser-Electronics/Pocket-Arcadehttp://

    Thnaks Gerald and Shabaz

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds over 4 years ago in reply to chrischristian14

    Hi Chris,

     

    you're welcome.

    The link you've posted looks broken.

    May be this link did you mean.

    GitHub - Mouser-Electronics/Pocket-Arcade: Retro Arcade using the Pocket Beagle

     

    Gerald

    ---

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrischristian14
    0 chrischristian14 over 4 years ago in reply to chrischristian14

    After long time I managed to get back on to this project, I am trying

    https://github.com/danjulio/lepton/tree/master/pocketbeagle/littlevgl_demo

    with this LCD http://www.lcdwiki.com/2.8inch_RPi_Display

    I edited the demo c code in the first link to only initaliize LCD and not the touch screen, as I am first focusing only on the LCD part, however all I get the white blank screen (because of backlight), I am adding the modified main.c here

    #include "lvgl/lvgl.h"
    #include "lv_drivers/display/fbdev.h"
    #include "lv_drivers/indev/evdev.h"
    #include "lv_examples/lv_apps/demo/demo.h"
    #include <unistd.h>
    
    #define DISP_BUF_SIZE (320*240*2)
    
    int main(void)
    {
    	/*LittlevGL init*/
    	lv_init();
    
    	/*Linux frame buffer device init*/
    	fbdev_init();
    
    	/*Linux touchscreen device init*/
    //	evdev_init();
    
    	/*A small buffer for LittlevGL to draw the screen's content*/
    	static lv_color_t buf1[DISP_BUF_SIZE];
    	static lv_color_t buf2[DISP_BUF_SIZE];
    
    	/*Initialize a descriptor for the buffer*/
    	static lv_disp_buf_t disp_buf;
    	lv_disp_buf_init(&disp_buf, buf1, buf2, DISP_BUF_SIZE);
    
    	/*Initialize and register a display driver*/
    	lv_disp_drv_t disp_drv;
    	lv_disp_drv_init(&disp_drv);
    	disp_drv.buffer = &disp_buf;
    	disp_drv.flush_cb = fbdev_flush;
    	lv_disp_drv_register(&disp_drv);
    
    	/*Initialize and register an input device*/
    	/*
    	lv_indev_drv_t indev_drv;
    	lv_indev_drv_init(&indev_drv);
    	indev_drv.type = LV_INDEV_TYPE_POINTER;
    	indev_drv.read_cb = evdev_read;
    	lv_indev_t * my_indev = lv_indev_drv_register(&indev_drv);
    	*/
    
    	 /*Create demo*/
    	demo_create();
    
    	/*Handle LitlevGL tasks (tickless mode)*/
    	while(1) {
    		lv_tick_inc(5);
    		lv_task_handler();
    		usleep(5000);
    	}
    
    	return 0;
    }

    Unfortunately I can't find a simple helloworld  over SPI for the LCD chip ILI9341 as shabaz mentioned before, that would have been a good start but the only example that is simple enough is the above one. The worst case would be to go through datasheet of ILI9341 and write the code from scratch.

    Can anyone please see the above link and my modified code ? If you have any tips it will be great before I start from scratch.

    p.s. : Upon running demo code I can see the framebuffer driver is loaded successfully, and I have checked the connections multiple times.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<