BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Embedded World 2023 - BeaglePlay Give Away, Meet & Greet with Jason Kridner
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 103 subscribers
  • Views 4262 views
  • Users 0 members are here
  • embedded world 2023
Related

Embedded World 2023 - BeaglePlay Give Away, Meet & Greet with Jason Kridner

e14phil
e14phil over 3 years ago

At Embedded World 2023 we are Giving Away up to 10 BeaglePlay®︎ 

Are you attending Embedded World 2023 in person?

We are hosting a giveaway of limited number of BeaglePlay on Wednesday 15th March with the Chance to Meet Jason Kridner, co-founder of the BeagleBoard.org project (https://beagleboard.org/about/jkridner) 

image
BeaglePlay is an open-source single board computer designed to simplify the process of adding sensors, actuators, indicators, human interfaces, and connectivity to a reliable embedded system. It features a powerful 64-bit, quad-core processor and innovative connectivity options, including Wi-Fi, Gigabit Ethernet, sub-GHz wireless, and single-pair Ethernet with power-over-data-line.
With compatibility with 1,000s of off-the-shelf add-ons and a customized Debian Linux image,
BeaglePlay makes expansion and customization easy. It also includes ribbon-cable connections for cameras and touch-screen displays, and a socket for a battery-backed real-time-clock, making it ideal for human-machine interface designs. With its competitive price and user-friendly design, BeaglePlay provides a positivedevelopment experience for users.
  • Multicore A53s with R5, M4s and PRUs processor, TI AM6254
  • Wi-Fi/2.4G, MIMO/5G, SISO M2 1216, TI WL1807 Wi-Fi module, U.FL x2
  • TI BLE/SubG CC1352P7 M4+M0 with BeagleConnect firmware
  • 2GB(1Gb x 16)-1600MHz 3200Mbps DDR
  • Kingston 16GB eMMC
  • Gigabit Ethernet with RJ45 x1, single pair Ethernet and power over with RJ11
  • Power input with USB Type-C
  • HDMI Type-A supports up to Full-HD/1080P with 24-bit RGB
  • Support FPC 22pin CSI and FPC 40pin OLDI
  • 1x MikroBus connector, 1x USB Type-A, 1x micro SD socket, 1x QWIIC, 1x grove connector, 1x RTC
How To Win
EDIT: All BeaglePlay have been collected, thank you to everyone who turned up and entered!
T&C Apply! 
Map 
image
Terms and Conditions

  • Sign in to reply
  • Cancel

Top Replies

  • e14phil
    e14phil over 2 years ago +6
    I got mine here on the community stand at Embedded world!
  • e14phil
    e14phil over 2 years ago in reply to misaz +3
    Thank you for picking up your BeaglePlay!
  • e14phil
    e14phil over 2 years ago in reply to securely +3
    Thank you!!
Parents
  • qba667
    qba667 over 2 years ago

    Having on bard sub-1GHz module together with 2.4 GHz protocols Zigbee, Thread, Ethernet, 5Ghz WiFi and power over RJ 11 make it perfect for my current project.

    Project: Open Source Smart Home Control with Human Machine Interface

    The project aims to provide ready to use platform for home automatization with integrated wireless solution.

    Integrating devices using well know protocols as Zigbee Thread and Amazon Sidewalk (Amazon Echo devices, Ring Security Cams end others) into single platform.

    Power full embedded platform allows hosting of all services on device instead of using cloud providers without additional hardware.

    Operating system: Debian

    Pre-installed software: 

    • Home Assistant - brilliant HMI
    • Node Red for configuration of advanced flows
    • Zigbee2mqtt for integration of Zigbee devices
    • Eclipse Mosquitto - as MQTT Hub
    • Eclipse Ditto - for digital twin representation

    General challenges:

    • Integrate Zigbee2mqtt with BeagleConnect
    • Matter integration
    • Add support for OpenTherm protocol

    Challenges for CC1352P7 BeagleConnect:

    • include support of Elero/Somfy protocols for windows curtains - working prototype on other TI chip
    • include support Bresser Weather Stations

    Challenges for HMI:

    • selection of display and digitizer

    image

    I will be glad to run the project on the BeaglePlay  instead of the RPI 4 with wireless adapters.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • darksidedevel
    darksidedevel over 2 years ago in reply to qba667

    Cool, I was thinking about similar solution!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • darksidedevel
    darksidedevel over 2 years ago in reply to qba667

    Cool, I was thinking about similar solution!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data