BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Embedded World 2023 - BeaglePlay Give Away, Meet & Greet with Jason Kridner
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 103 subscribers
  • Views 4259 views
  • Users 0 members are here
  • embedded world 2023
Related

Embedded World 2023 - BeaglePlay Give Away, Meet & Greet with Jason Kridner

e14phil
e14phil over 3 years ago

At Embedded World 2023 we are Giving Away up to 10 BeaglePlay®︎ 

Are you attending Embedded World 2023 in person?

We are hosting a giveaway of limited number of BeaglePlay on Wednesday 15th March with the Chance to Meet Jason Kridner, co-founder of the BeagleBoard.org project (https://beagleboard.org/about/jkridner) 

image
BeaglePlay is an open-source single board computer designed to simplify the process of adding sensors, actuators, indicators, human interfaces, and connectivity to a reliable embedded system. It features a powerful 64-bit, quad-core processor and innovative connectivity options, including Wi-Fi, Gigabit Ethernet, sub-GHz wireless, and single-pair Ethernet with power-over-data-line.
With compatibility with 1,000s of off-the-shelf add-ons and a customized Debian Linux image,
BeaglePlay makes expansion and customization easy. It also includes ribbon-cable connections for cameras and touch-screen displays, and a socket for a battery-backed real-time-clock, making it ideal for human-machine interface designs. With its competitive price and user-friendly design, BeaglePlay provides a positivedevelopment experience for users.
  • Multicore A53s with R5, M4s and PRUs processor, TI AM6254
  • Wi-Fi/2.4G, MIMO/5G, SISO M2 1216, TI WL1807 Wi-Fi module, U.FL x2
  • TI BLE/SubG CC1352P7 M4+M0 with BeagleConnect firmware
  • 2GB(1Gb x 16)-1600MHz 3200Mbps DDR
  • Kingston 16GB eMMC
  • Gigabit Ethernet with RJ45 x1, single pair Ethernet and power over with RJ11
  • Power input with USB Type-C
  • HDMI Type-A supports up to Full-HD/1080P with 24-bit RGB
  • Support FPC 22pin CSI and FPC 40pin OLDI
  • 1x MikroBus connector, 1x USB Type-A, 1x micro SD socket, 1x QWIIC, 1x grove connector, 1x RTC
How To Win
EDIT: All BeaglePlay have been collected, thank you to everyone who turned up and entered!
T&C Apply! 
Map 
image
Terms and Conditions

  • Sign in to reply
  • Cancel

Top Replies

  • e14phil
    e14phil over 2 years ago +6
    I got mine here on the community stand at Embedded world!
  • e14phil
    e14phil over 2 years ago in reply to misaz +3
    Thank you for picking up your BeaglePlay!
  • e14phil
    e14phil over 2 years ago in reply to securely +3
    Thank you!!
Parents
  • securely
    securely over 2 years ago

    I have the idea of a digital cookbook with shopping list for my kitchen. Using the BeaglePlay as HMI and server seems like a perfect fit. What I need is a fairly sharp display (maybe even a eink display) to read receipts. For the shopping list I would like to see if the board is powerful enough to recognize speech to add elements to the shopping list. The wifi connectivity, the small form-factor, the powerful CPU, and good extentability makes the board very attractive.

    Will be on the embedded word tomorrow. Looking forward to meet you there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14phil
    e14phil over 2 years ago in reply to securely

    Thank you!! 

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14phil
    e14phil over 2 years ago in reply to securely

    Thank you!! 

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data