In this mini blog series we will build an IoT based intruder detection and alert system.
Blogs:
Part1 : Connecting Pir Sensor
Part2 : Capturing intruder image <--- this blog
Part3 : Email Alerts
In previous blog we integrated a PIR sensor to Riotboard for human movement detection.
In this very short guide we will try to capture image once an IR detection is made.
I am using a Logitech C310Logitech C310 USB camera for this purpose.
Connect pir sensor HC-Sr501 and Camera to Riotboard.
to capture image we will use fswebcam tool.
in terminal type:
apt-get install fswebcam
Now we determine the usb device
type "ls /dev/video*" without pluggin camera.
Now pluggin camera to Riotboard, and type "ls /dev/video*"
check for video device in /dev.
the camera hardware is accessible at the device /dev/video2
now add below line to previous code below ln28.
system("fswebcam -d /dev/video2 capture.jpg");
Next we will compile the below code and test.
#include <stdio.h>
#include <fcntl.h>
#include <unistd.h>
#include <string.h>
int main()
{
int ret =0;
int fd=0;
char buf[1];
system("devmem 0x20E00A0 w 0x5 ");
system("echo 113 > /sys/class/gpio/unexport");
system("echo 113 > /sys/class/gpio/export");
usleep(100000);
system("echo in > /sys/class/gpio/gpio113/direction");
usleep(100000);
fd = open("/sys/class/gpio/gpio113/value",O_RDONLY);
while(1)
{
ret = read(fd,buf,sizeof(1));
if(lseek(fd,0,SEEK_SET) < 0) return 1;
if(ret>0 && (atoi(buf)==1))
{
printf("\n\033[031;43m HUMAN DETECTED \033[0m ");
fflush(stdout);
system("fswebcam -d /dev/video2 capture.jpg");
usleep(500000);
}
else
printf("\nNo Detection");
fflush(stdin);
fflush(stdout);
usleep(500000);
}
close(fd);
}
Now perform some hand movement infront of Pir sensor, it will show human detected and captures image as "capture.jpg".
before capture:
after capture:
Now with every pir interrupt we can capture the image of the intruder.
Next time we will add an image based email alert for the above.





Top Comments
-
DAB
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
tusharp
in reply to DAB
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
mrpipes3
in reply to tusharp
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
mrpipes3
in reply to tusharp
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children