Freescale i.MX6 Development Platforms
  • Products
  • Dev Tools
  • Single-Board Computers
  • Freescale i.MX6 Development Platforms
  • More
  • Cancel
Freescale i.MX6 Development Platforms
Forum Debian on Sabre Lite (SD card or SATA)
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Freescale i.MX6 Development Platforms requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 3 subscribers
  • Views 260 views
  • Users 0 members are here
  • single_board_computer
  • single_board_computers
Related

Debian on Sabre Lite (SD card or SATA)

Former Member
Former Member over 9 years ago

Hi,

 

          I would like to use Sabre Lite with debian. I'm using Debian with PandaBoard and I'm quite happy.

 

 

I achieve to use pandaboard with Debian thanks to that post http://alastordmcblog.blogspot.com.es/2012/05/how-to-install-debian-on-pandaboard-do.html . I build a Debian SD Card just using this script in a similar way ./setup_sdcard.sh --mmc /dev/sdc --uboot mx6qsabrelit.

 

 

I tried to boot from this SD Card (two partition) both from full size and small one. But I'm not able to do it. It's seems to be possible as Debian it's mentioned here http://www.eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite#i.MX6xSABRELite-DebianSqueeze6.0.6%28armel%2Farmv4tbased%29RootFileSystem, nevertheless it's not clear (for me) how to put together these things to be able to use it on Sabre Lite (I received Sabre Lite on monday from Farnell)

 

How should I do this to be able to boot from SD card with a Debian Image?

 

Thank you

  • Reply
  • Cancel
  • Cancel
Parents
  • Former Member
    0 Former Member over 9 years ago

    You most likely need to follow the instructions on that page under "SPI -> SD u-boot.imx bootloader" to get an SD card based on Roberts scripts to work.

     

    By default the sabre-lite comes with an old version of uBoot installed in the nand flash which is pre-devicetree. Your image likely has a recent kernel which requires uBoot to pass a sane devicetree before it'll boot. There will be a working version of uBoot on your card, but unless you overwrite the version in nand flash with the SDcard bootloader it'll never get used.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Ok, I have completed "SPI->SH u-boot.imx bootloader" stuff. But I still don't get how to put debian software into the SD CARD. If I use the "

    ./setup_sdcard.sh --mmc /dev/sdc --uboot mx6qsabrelite" recipe from

    http://alastordmcblog.blogspot.com.es/2012/05/how-to-install-debian-on-pandaboard-do.html

     

    I get an SD Card. But If I put that card on the full size SD slot I get:

     

    U-Boot 2013.01-00005-g9febdfc (Jan 21 2013 - 15:52:15)

     

     

    CPU:   Freescale i.MX6Q rev1.0 at 792 MHz

    Reset cause: POR

    Board: MX6Q-Sabre Lite

    DRAM:  1 GiB

    MMC:   FSL_SDHC: 0, FSL_SDHC: 1

    *** Warning - bad CRC, using default environment

     

     

    auto-detected panel HDMI

    enable_hdmi: setup HDMI monitor

    Display: HDMI (1024x768)

    In:    serial

    Out:   serial

    Err:   serial

    Net:   FEC [PRIME]

    Warning: failed to set MAC address

     

     

    Hit any key to stop autoboot:  0

    mmc0 is current device

    mmc0 is current device

    253 bytes read in 34 ms (6.8 KiB/s)

    Running bootscript from mmc ...

    ## Executing script at 12000000

    boot.scr -> uEnv.txt wrapper...

    1009 bytes read in 40 ms (24.4 KiB/s)

    ** File not found uImage **

    bad MBR sector signature 0x0000

    ** Invalid partition 1 **

    ** File not found /dtbs/imx6q-sabrelite.dtb **

    Booting from mmc ...

    Wrong Image Format for bootm command

    ERROR: can't get kernel image!

     

    Could you please tell me which should be the next step.

     

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Have you tried the exact same image in the microSD slot ? 

     

    I can't find details on which is which right now, but one of the SD slots is mmc0, the other is mmc1. So it may simply be that your boot script is looking for the kernel and devicetree files in the empty sd slot and failing. 

     

    From the messages it certainly seems that whatever it's looking at doesn't have any partitions, so either wrong slot, or you somehow built the card incorrectly. Given you're getting the new uBoot off the card, I'm assuming it's built ok, but just in the wrong slot.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Yes I have tried to. If I put the micro-sd (without the full size adapter) in the small slot, I get nothing from the serial port. Also I have tried changing the default file system for the image (with ext2 or other) like:

     

    ./setup_sdcard.sh --mmc /dev/sdb --uboot mx6qsabrelite --rootfs btrfs

     

    Doing any of these I get two partition labeled at the SD card: boot and rootfs. Nevertheless I still keep getting:

     

    U-Boot 2013.01-00005-g9febdfc (Jan 21 2013 - 15:52:15)

     

     

    CPU:   Freescale i.MX6Q rev1.0 at 792 MHz

    Reset cause: POR

    Board: MX6Q-Sabre Lite

    DRAM:  1 GiB

    MMC:   FSL_SDHC: 0, FSL_SDHC: 1

    *** Warning - bad CRC, using default environment

     

     

    auto-detected panel HDMI

    enable_hdmi: setup HDMI monitor

    Display: HDMI (1024x768)

    In:    serial

    Out:   serial

    Err:   serial

    Net:   FEC [PRIME]

    Warning: failed to set MAC address

     

     

    Hit any key to stop autoboot:  0

    mmc0 is current device

    mmc0 is current device

    253 bytes read in 34 ms (6.8 KiB/s)

    Running bootscript from mmc ...

    ## Executing script at 12000000

    boot.scr -> uEnv.txt wrapper...

    1010 bytes read in 40 ms (24.4 KiB/s)

    ** File not found uImage **

    ** File not found uInitrd **

    ** File not found /dtbs/imx6q-sabrelite.dtb **

    Booting from mmc ...

    Wrong Image Format for bootm command

    ERROR: can't get kernel image!

     

     

    I suppose I'm missing "other" thing rather than using the script. By the way this is the log of the script that builds the SD cart (it may help you, to understand what I'm doing wrong):

     

     

    Debug: ARM rootfs: armhf-rootfs-debian-wheezy.tar

    Debug: /sbin/fdisk version:

    fdisk (util-linux-ng 2.17.2)

     

     

    Downloading Device's Bootloader

    -----------------------------

    attempting to use rcn-ee.net for dl files [10 second time out]...

    2013-02-27 22:31:26 URL:http://rcn-ee.net/deb/tools/latest/bootloader-ng [4389/4                                                         389] -> "/tmp/tmp.uufgatOv2E/dl/bootloader-ng" [1]

    --2013-02-27 22:31:26--  http://rcn-ee.net/deb/tools/mx6qsabrelite/u-boot-mx6qsa                                                         brelite-v2013.01-r0.imx

    Resolving rcn-ee.net... 69.163.130.148

    Connecting to rcn-ee.net|69.163.130.148|:80... connected.

    HTTP request sent, awaiting response... 200 OK

    Length: 321172 (314K) [text/plain]

    Saving to: â/tmp/tmp.uufgatOv2E/dl/u-boot-mx6qsabrelite-v2013.01-r0.imxâ

     

     

    100%[======================================>] 321,172     45.0K/s   in 8.8s

     

     

    2013-02-27 22:31:36 (35.6 KB/s) - â/tmp/tmp.uufgatOv2E/dl/u-boot-mx6qsabrelite-v                                                         2013.01-r0.imxâ

     

     

    UBOOT Bootloader: u-boot-mx6qsabrelite-v2013.01-r0.imx

     

     

    Unmounting Partitions

    -----------------------------

     

     

    Using dd to place bootloader on drive

    -----------------------------

    627+1 records in

    627+1 records out

    321172 bytes (321 kB) copied, 0.0656674 s, 4.9 MB/s

    Creating rootfs btrfs Partition

    -----------------------------

    Formating Boot Partition

    -----------------------------

    mke2fs 1.41.12 (17-May-2010)

    Filesystem label=boot

    OS type: Linux

    Block size=1024 (log=0)

    Fragment size=1024 (log=0)

    Stride=0 blocks, Stripe width=0 blocks

    12240 inodes, 48828 blocks

    2441 blocks (5.00%) reserved for the super user

    First data block=1

    Maximum filesystem blocks=50069504

    6 block groups

    8192 blocks per group, 8192 fragments per group

    2040 inodes per group

    Superblock backups stored on blocks:

            8193, 24577, 40961

     

     

    Writing inode tables: done

    Writing superblocks and filesystem accounting information: done

     

     

    This filesystem will be automatically checked every 22 mounts or

    180 days, whichever comes first.  Use tune2fs -c or -i to override.

    Formating rootfs Partition as btrfs

    -----------------------------

     

     

    WARNING! - Btrfs Btrfs v0.19 IS EXPERIMENTAL

    WARNING! - see http://btrfs.wiki.kernel.org before using

     

     

    fs created label rootfs on /dev/sdb2

            nodesize 4096 leafsize 4096 sectorsize 4096 size 14.59GB

    Btrfs Btrfs v0.19

    Populating Boot Partition

    -----------------------------

    Image Name:   wrapper

    Created:      Wed Feb 27 22:31:37 2013

    Image Type:   ARM Linux Script (uncompressed)

    Data Size:    189 Bytes = 0.18 kB = 0.00 MB

    Load Address: 0x00000000

    Entry Point:  0x00000000

    Contents:

       Image 0:      181 Bytes =    0 kB = 0 MB

    `/tmp/tmp.uufgatOv2E/disk/boot.scr' -> `/tmp/tmp.uufgatOv2E/disk/backup/boot.scr                                                         '

    Copying uEnv.txt based boot scripts to Boot Partition

    -----------------------------

    `/tmp/tmp.uufgatOv2E/bootscripts/normal.cmd' -> `/tmp/tmp.uufgatOv2E/disk/uEnv.t                                                         xt'

    -----------------------------

    kernel_file=uImage

    initrd_file=uInitrd

     

     

    initrd_high=0xffffffff

    fdt_high=0xffffffff

     

     

    #Video: Uncomment to override U-Boots value:

    framebuffer=mxcdi1fb

    dvimode=RGB24,1280x720M@60

     

     

     

     

    console=ttymxc1,115200

     

     

    mmcroot=/dev/mmcblk0p2 ro

    mmcrootfstype=btrfs rootwait fixrtc

     

     

    boot_fstype=ext2

    xyz_load_image=${boot_fstype}load mmc 0:1 0x10000000 ${kernel_file}

    xyz_load_initrd=${boot_fstype}load mmc 0:1 0x12000000 ${initrd_file}; setenv ini                                                         trd_size ${filesize}

    xyz_load_dtb=${boot_fstype}load mmc 0:1 0x11ff0000 /dtbs/${dtb_file}

     

     

    xyz_mmcboot=run xyz_load_image; run xyz_load_initrd; run xyz_load_dtb; echo Boot                                                         ing from mmc ...

     

     

    video_args=setenv video video=${framebuffer}:${dvimode}

    device_args=run video_args; run expansion_args; run mmcargs

    mmcargs=setenv bootargs console=${console} ${optargs} ${video} root=${mmcroot} r                                                         ootfstype=${mmcrootfstype} ${expansion}

     

     

    optargs=console=tty0

    expansion_args=setenv expansion

    loaduimage=run xyz_mmcboot; run device_args; bootm 0x10000000 0x12000000:${initr                                                         d_size} 0x11ff0000

     

     

    -----------------------------

    Debug:

    #!/bin/sh

    format=1.0

    board=MX6QSABRELITE_D

     

     

    bootloader_location=dd_uboot_boot

    dd_spl_uboot_seek=

    dd_spl_uboot_bs=

    dd_uboot_seek=2

    dd_uboot_bs=512

     

     

    boot_image=bootm

    boot_script=uEnv.txt

    boot_fstype=ext2

     

     

    serial_tty=ttymxc1

    kernel_addr=0x10000000

    initrd_addr=0x12000000

    load_addr=0x10008000

    dtb_addr=0x11ff0000

    dtb_file=imx6q-sabrelite.dtb

     

     

    usbnet_mem=

     

     

    Debug: Adding Useful scripts from: https://github.com/RobertCNelson/tools

    -----------------------------

    Cloning into /tmp/tmp.uufgatOv2E/disk/tools...

    remote: Counting objects: 417, done.

    remote: Compressing objects: 100% (279/279), done.

    remote: Total 417 (delta 243), reused 282 (delta 115)

    Receiving objects: 100% (417/417), 58.64 KiB, done.

    Resolving deltas: 100% (243/243), done.

    -----------------------------

    Debug: Contents of Boot Partition

    -----------------------------

    total 18K

    drwxr-xr-x  2 root root 1.0K Feb 27 22:31 backup

    -rw-r--r--  1 root root  253 Feb 27 22:31 boot.scr

    drwxr-xr-x  2 root root 1.0K Feb 27 22:31 dtbs

    drwx------  2 root root  12K Feb 27 22:31 lost+found

    -rw-r--r--  1 root root  352 Feb 27 22:31 SOC.sh

    drwxr-xr-x 10 root root 1.0K Feb 27 22:31 tools

    -rw-r--r--  1 root root 1010 Feb 27 22:31 uEnv.txt

    -----------------------------

    Finished populating Boot Partition

    -----------------------------

    Populating rootfs Partition

    Please be patient, this may take a few minutes, as its transfering a lot of file                                                         s..

    -----------------------------

    /home/user/debian-wheezy-minimal-armhf-2013-02-17/armhf-rootfs-debian-wheezy.tar

    296MB 0:00:19 [15.3MB/s] [=================================>] 100%

    Transfer of Base Rootfs is Complete, now syncing to disk...

    -----------------------------

    Finished populating rootfs Partition

    -----------------------------

    setup_sdcard.sh script complete

    -----------------------------

    The default user:password for this image:

    debian:temppwd

    -----------------------------

     

     

     

    Thnak you

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    I don't think there's anything you're doing wrong as such, and the log looks reasonably sane.

     

    Under where it says "Debug: Contents of Boot Partition" I don't see a uImage or uInitrd listed, which might be something to do with it.

     

    I'd start by looking at the card in another system, investigate the contents of uEnv.txt to see where it's trying to load uImage from, then check that there's actually a uImage in that location.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    I don't think there's anything you're doing wrong as such, and the log looks reasonably sane.

     

    Under where it says "Debug: Contents of Boot Partition" I don't see a uImage or uInitrd listed, which might be something to do with it.

     

    I'd start by looking at the card in another system, investigate the contents of uEnv.txt to see where it's trying to load uImage from, then check that there's actually a uImage in that location.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 9 years ago in reply to Former Member

    Ok, I was going to do that, but instead of doing it  I asked for some help to Robert here http://www.eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite#i.MX6xSABRELite-Comments . He told me to check his net install with

    git clone git://github.com/RobertCNelson/netinstall.git,

     

    nevertheless I can now start the installation, but I can't configure Network Interface (as I say on the comments), so, I got stuck at that point...

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
  • rbarraud
    0 rbarraud over 8 years ago in reply to Former Member

    So what happened after this point? Did you give up? :-/

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 8 years ago in reply to rbarraud

    Well,...

     

    After some help of Robert (http://www.eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+Comments https://github.com/RobertCNelson/netinstall/issues/14).

     

    Yes, I did.

     

    Maybe I'll try in the future.

    • Cancel
    • Vote Up 0 Vote Down
    • Reply
    • Verify Answer