• CAN interface in i.MX6 Quad | SABRE LITE

    Hello friends,

     

    Greetings to all!!

     

    Can anybody let me know if you have used the CAN interface and built any application over it?

     

    I am planning to buy development kit for i.MX6 quad for a CAN based project. Please throw some light.

     

    Thanks in advance.

  • Yocto and IMX 6 Element14 devlopment kit

    Good morning,

     

         I just received my IMX 6 Element 14 devlopment Kit and I try to put some free linux on it. My goal is to use the 2D and 3D graphical card's acceleration. So I try first to build the sabre_lite yocto image as in the thread ( https://community…

  • Sabre-Lite Gerbers ?

    Do element14/embest have any plans to make gerbers available ?

     

    It would be useful to be able to seperate VDD_SNVS_IN (G11) from VDDHIGH_IN_1/2 (H9,J9) and connect VDD_SNVS_IN to a 3v coincell to enable a useful RTC. However it's not clear if this would…

  • Will a 2GB version be available ?

    The schematics seem to suggest that the 1GB of onboard memory has the option of using different devices to provide 2GB.

     

    Is there any intention to sell a version of the Sable-Lite with 2GB or the iMX6's theoretical 4GB maximum ?

     

    Having a fast quad-core…

  • Will Element 14 be selling breakout boards/cables for the Sabre-Lite ?

    For example I'd like to be able to do some stuff with the PCIe interface on J23 which is a  "7Pin Connector 53047-0710 Pitch:1.25mm; MOLEX".

     

    When searching for the parts to make up a cable it appears I'll need the following:

    MOLEX - 51021…

  • Differences between Element 14 Sabrelite and Boundary Devices SabreLite

    Hello,

     

    I've been working with the SABRE Lite BSP offered now with WEC2013.

     

    We have 4 of the Element 14 SABRE Lite boards and have successfully booted WinCE 2013, however we have struggled to get HDMI working and some of the board peripherals.

     

    Development…

  • Arch linux ?

    archlinuxarm.org has http://archlinuxarm.org/platforms/armv7/nitrogen6x which while technically for the boundary nitrogen6x board may just be able to boot on a Sabre-Lite.  I'll test it sometime in the next couple of days when my new microSD cards arrive…

  • Boundary Devices iMX6 blog posts

    The Boundary Devices guys have a load of interesting iMX6 info including kernel patches and various fixes in their blog

    http://boundarydevices.com/tag/i-mx6/

  • iMX6 ethernet throughput improvements

    Interesting writeup on improving ethernet throughput from Boundary Devices:

    http://boundarydevices.com/i-mx6-ethernet/

  • CNX iMX6 resources

    Not Sabre-Lite specific, but full of lots of useful info none the less.

    http://www.cnx-software.com/2012/11/18/freescale-i-mx6-resources-development-boards-documentation-source-code-and-tools/

     

    Of interest here might be the Android BSP

  • eewiki - i.MX6 Sabre-Lite

    Lots of useful info on how to compile your own kernel, build your own u-boot, use the usb-otg utils to 'unbrick' your board.

    http://www.eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite

     

    note that if you go this route to get a mainline linux kernel…

  • Freescale iMX6 community

    Lots of useful info for Sabre-Lite / iMX6

    https://community.freescale.com/community/imx

  • Sabre-Lite WinCE BSP

  • Linaro Sabre-Lite resources

  • Sabre-Lite: Embest, an element14 company