Return to MaaXBoard Nano page
I recently designed a frame and stand for the Avnet MaaXBoard MIPI LCD touch display
There were 3 main design goals . . .
Introduction
If you haven't noticed already, the MaaXBoard Mini supports Android 9 out of box! One thing that developers are probably wondering is how do I go through the process of actually developing my own application and deploying it on the MaaXBoard…
Avnet recently released the MaaXBoard Mini which is based on the NXP i.MX 8M Mini Processor.
The MaaXBoard Mini is a low-cost, NXP i.MX 8M Mini processor-based, single-board computer ideal for embedded computing and smart edge IoT applications. The i.MX…
1. Indroduction
Python is a great general purpose high level programming language. It is beneficial for many reasons, one being that its simple syntax rules allows the language code to be readable and maintanable. It is fairly easy to develop also due…
Update:
Want to see how well benchmarking performs on the MaaXBoard Mini? Updated results including the MaaXBoard Mini are HERE.
Introduction
In the past two years, Machine Learning at the edge has proliferated. With more machine learning models capable…
1. Introduction
The MaaXboad by Avnet is based on the NXP i.MX 8M processor running quad Arm Cortex
-A53s and a single Cortex-M4 core. Out of box the MaaXBoard supports both a Debian based linux image and a Android 9 image. In this blog lets discover what…
One of the main key drivers behind hardware adoption tends for any platform to be the availability of software resources. In the case of the MaaXBoard things are no different. Lets discuss what is currently available and what is to come!
First lets talk…
One such demo showcased was an example of a Smart Crane which addresses the…