Technical Library
  • Products
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Forum Programmazione microcontrollore
  • Blog
  • Forum
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Technical Library requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 45 subscribers
  • Views 190 views
  • Users 0 members are here
Related

Programmazione microcontrollore

Former Member
Former Member over 7 years ago

Salve, sono uno studente di ingegneria, avrei bisogno di una mano per imparare a progrmmare un micro MK10DN512ZVLL10.  Qualcuno mi può supportare? 

  • Reply
  • Cancel
  • Cancel

Top Replies

  • Former Member
    Former Member over 7 years ago in reply to balearicdynamics +1

    As for the development environment I installed the Kinetis Design Studio IDE freescale.
    Link:
    http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE

    The card was made entirely by the Uni…

  • Former Member
    Former Member over 7 years ago in reply to balearicdynamics +1

    Should blink an LED, and when you press a button it Mantine on and measures the temperature. I do not know if the operation is so, also because I still have to start with the IDE ..... I did not under…

  • balearicdynamics
    balearicdynamics over 7 years ago

    Maybe, but please share the same language we all are using.

     

    Thanks

    • Cancel
    • Up 0 Down
    • Reply
    • Cancel
  • Former Member
    Former Member over 7 years ago in reply to balearicdynamics

    Ok ok, sorry all.
    I state that I did a test on programming in C ++ but it's the first time I am confronted with a microcontroller. I do not have a deep knowledge mainly because I come from courses in telecommunications (electromagnetism, maxwell, microwave ...)
    The univ. I put it has provision the MK10DN512ZVLL10 integrated on a card.
    The goal is to control 3 inputs (antenna, an accelerometer (LSM330DL) and a strain gauge) and output (linear actuator). For the main program in C i have a idea (maybe), but I have no idea to control the structure of instructions to initialize the register, meters, reading and writing of micro devices ....
    If you want I'll show you an example program that provided me and let's start with that. You have knowledge of the industry? You know someone who has? Tanks at you

    • Cancel
    • Up 0 Down
    • Reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to Former Member

    I think that an example of a program it is a good starting point.

     

    As a matter of fact I don't know this specific micro but I think that it can't be totally different by a lot of other that I have already saw. I will check on the net the architecture. In the meantime, please provide if you the links on the specific board you are using so I can take a look and hopefully help you. Another useful information is knowing what kind of development environment you will use to make this development, i.e. what development platform this board support.

     

    Thank you.

    • Cancel
    • Up 0 Down
    • Reply
    • Cancel
  • Former Member
    Former Member over 7 years ago in reply to balearicdynamics

    As for the development environment I installed the Kinetis Design Studio IDE freescale.
    Link: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE

    The card was made entirely by the University.  I can not find how to send an attachment...

    I'll show the example program?



     

    • Cancel
    • Up +1 Down
    • Reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to Former Member

    To send an attachment program, you can zip it and attach to the post (worst solution) or copy and paste the code selecting the block on the post text. Then with the rightmost button in the editor bar with the ">>" select the syntax highlighting as C/C++ That's all

    • Cancel
    • Up 0 Down
    • Reply
    • Cancel
  • Former Member
    Former Member over 7 years ago in reply to balearicdynamics

    Should blink an LED, and when you press a button it Mantine on and measures the temperature. I do not know if the operation is so, also because I still have to start with the IDE ..... I did not understand much ... I have a lot of question

    #include <MK10DZ10.h>
    #include <stdint.h>
    #include <stdbool.h>
    #include <stdio.h>
    #include "peripherals/tmp102.h"
    #include "core/uart.h"
    
    
    #define LED2_ON  BITBAND_REG(PTB->PDDR, 17) = 1  // set pin dir to output
    #define LED2_OFF BITBAND_REG(PTB->PDDR, 17) = 0  // set pin dir to intput
    
    
    #define STDIO_UART1
    
    
    bool audio_curr = false;
    volatile bool audio_toggle = false;
    volatile bool temperature_comm_ok = false, temperature_comm_err = false;
    void enable_btn_irq();
    
    
    #ifdef STDIO_UART1
    static uint8_t stdio_buff[80];
    static ring_buffer stdio_ring_buffer;
    #endif
    
    
    
    
    static void init_hardware() {
        // enable clock gating for all ports
        SIM->SCGC5 |= (SIM_SCGC5_PORTA_MASK | SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTC_MASK | SIM_SCGC5_PORTD_MASK | SIM_SCGC5_PORTE_MASK);
    
        // pins for voltage regulators
        // 3.0 V
        PORTB->PCR[11] = PORT_PCR_MUX(1);
        BITBAND_REG(PTB->PDDR, 11) = 1;  // output
        PTB->PSOR = (1u << 11);  // output = 1, vreg enabled
        // 3.3 V
        PORTA->PCR[5] = PORT_PCR_MUX(1);
        BITBAND_REG(PTA->PDDR, 5) = 1;  // output
        PTA->PSOR = (1u << 5);  // output = 1, vreg enabled
    
        // pins for LED2 and LED3. By default, output register is 0
        PORTB->PCR[17] = PORT_PCR_MUX(1);
        PORTB->PCR[16] = PORT_PCR_MUX(1);
    
        // pins for buttons: pull-up, interrupt on either edge
        PORTD->PCR[0]  = PORT_PCR_MUX(1) | PORT_PCR_IRQC(11) | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;
        PORTC->PCR[18] = PORT_PCR_MUX(1) | PORT_PCR_IRQC(11) | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;
        PORTC->PCR[17] = PORT_PCR_MUX(1) | PORT_PCR_IRQC(11) | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;
        PORTC->PCR[16] = PORT_PCR_MUX(1) | PORT_PCR_IRQC(11) | PORT_PCR_PE_MASK | PORT_PCR_PS_MASK;
    
        // enable clock gating for PIT
        BITBAND_REG(SIM->SCGC6, SIM_SCGC6_PIT_SHIFT) = 1;
        // enable PIT (periodic interrupt timer)
        PIT->MCR = 0;  // clock enabled
    
        // use PIT channel 1 for debouncing
        PIT->CHANNEL[1].LDVAL = busClock / 50;  // 20 ms between subsequent button events
        PIT->CHANNEL[1].TCTRL = 0;  // initially disabled
        NVIC_SetPriority(PIT1_IRQn, 15);
        NVIC_EnableIRQ(PIT1_IRQn);
    
        // enable IRQ for buttons
        NVIC_SetPriority(PORTC_IRQn, 15);
        NVIC_SetPriority(PORTD_IRQn, 15);
        enable_btn_irq();
    
        // pins for misc. peripherals
        PORTB->PCR[20] = PORT_PCR_MUX(1);  // reset for radio chip
        BITBAND_REG(PTB->PDDR, 20) = 1;  // output
        PORTD->PCR[1] = PORT_PCR_MUX(1);  // LT
        BITBAND_REG(PTD->PDDR, 1) = 1;  // output
        PORTC->PCR[1] = PORT_PCR_MUX(1);  // GPS_EN
        BITBAND_REG(PTC->PDDR, 1) = 1;  // output
        PORTB->PCR[9] = PORT_PCR_MUX(1);  // SENSE_EN
        BITBAND_REG(PTB->PDDR, 9) = 1;  // output
        PORTE->PCR[25] = PORT_PCR_MUX(1);  // AUDIO_EN
        BITBAND_REG(PTE->PDDR, 25) = 1;  // output
    }
    
    
    
    
    int main(void)
    {
        init_hardware();
    
        // blink leds with period = 1s, using PIT channel 0
        //LED_ON(2);
        PIT->CHANNEL[0].LDVAL = busClock / 2u;  // 0.5 s
        PIT->CHANNEL[0].TCTRL = PIT_TCTRL_TEN_MASK | PIT_TCTRL_TIE_MASK;
        NVIC_SetPriority(PIT0_IRQn, 5);
        NVIC_EnableIRQ(PIT0_IRQn);
    
    #ifdef STDIO_UART1
        // enable GPS connector to be used as external UART connection
        PTC->PSOR = (1u << 1);
        ring_buffer_init(&stdio_ring_buffer, stdio_buff, sizeof(stdio_buff), UART1_RX_TX_IRQn, -1);
        uart_enable(1, 115200, true, true, &stdio_ring_buffer);
        printf("ready.\r\n");
    #endif
    
        for(;;) {
            if (audio_toggle) {
                // user toggled the audio
                audio_toggle = false;
                audio_curr = !audio_curr;
                if (audio_curr) {
                    // turn audio on (not implemented)
                    LED2_ON;
                    // read temperature
                    tmp102_enable();
                    tmp102_start_read();
                }
                else {
                    // turn audio off
                    LED2_OFF;
                }
            }
            else if (temperature_comm_ok || temperature_comm_err) {
                printf("Temp: ");
                if (temperature_comm_ok) {
                    uint16_t t = tmp102_get();
                    printf("%u.%u\r\n", t / 16, ((t % 16) * 10 + 8) / 16);
                }
                else printf("ERR\r\n");
                temperature_comm_ok = false;
                temperature_comm_err = false;
                tmp102_disable();
            }
        }
    }
    
    
    
    
    // reimplementation of _write and _read weak functions, to redirect stdio
    //  and not use the default semihosting
    
    int _write (int fd, const void *buf, size_t count) {
        (void)fd;
        (void)buf;
        (void)count;
    #ifdef STDIO_UART1
        return uart_queue_tx(1, buf, count);
    #else
        return 0;
    #endif
    }
    
    int _read (int fd, const void *buf, size_t count) {
        (void)fd;
        (void)buf;
        (void)count;
        return 0;
    }

    • Cancel
    • Up +1 Down
    • Reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to Former Member

    Well, now the scenario is quite celar. And as for what I see in the schematic this micro controller is not so more difficult than many others. Unfortunately I didn't use the IDE you mention (any processor / producer adopt a different C IDE and development environment, sigh!)

     

    I suggest - if I can suggest the steps you need to path - to start first creating the development environment, ide, libraries and all that you have in your documentation to be able to move on the programming questions without problems like where to find a component, why does a part does not work, compile etc.

    The first thing should be - blindy - trying to be able to compile the small program, leaving untouched it and find all the practical issues .e.g. the correct procedure to upload the program to the board, etc.

     

    I suggest also in this phase to see if your board has a bootloader or not, how should be programmed (supposing some kind of hardware connection). Then when you have a sort of running echosystem you can approach the real problems.

     

    Keep us updated.

    • Cancel
    • Up 0 Down
    • Reply
    • Cancel
  • Former Member
    Former Member over 7 years ago in reply to balearicdynamics

    Hi, how are you??


    I did not understand some instructions first. I have some basic questions ...
    For example:

    PORTB->PCR[11] = PORT_PCR_MUX(1);

    BITBAND_REG(PTB->PDDR, 11) = 1;  // output

    PTB->PSOR = (1u << 11);  // output = 1, vreg enabled

    There is a particular reason because it uses PDDR?

    I see in the program of MICRO other GPIO Register Masks. It would have been equal usarne another? And the 17? And (1u<<11)?

    What do this?

    #ifdef STDIO_UART1

    static uint8_t stdio_buff[80];

    static ring_buffer stdio_ring_buffer;

    #endif

    PORTA, PORTB, PORTC what gate is??

    In the program of micro i see 29, what are ??

     

    #define SIM_SCGC6_RTC_MASK                       0x20000000u

    #define SIM_SCGC6_RTC_SHIFT                      29

    • Cancel
    • Up 0 Down
    • Reply