Technical Library
  • Products
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Documents element14: Software examples and demos for the LPC4357-EVB
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: vandana
  • Date Created: 15 Jan 2013 9:42 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:00 AM
  • Views 3921 views
  • Likes 0 likes
  • Comments 21 comments
Related
Recommended

element14: Software examples and demos for the LPC4357-EVB

This document lists the available software examples and demos for the LPC4357-EVB; Details on the examples and testing are provided in the User Manual.

 

Simply click on the links to download the code!

 

Examples 1 - Core & Drivers - (required for all examples)

Examples 2 - GPIO, SDRAM, I2C - Accelerometer, USB, LCD, Touch Screen

Examples 3 - I2S

Examples 4 - Dual-Core

Examples 5 - SD Card

 

Demo 1 - emWin Graphics

Demo 2 - Micrium uC/OS-III

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Former Member
    Former Member over 13 years ago +1
    Following the instructions on the enclosed 'Quick start guide' does not result in the driver for the VCOM installing. If this product is not compatible with Windows 8 or 64-bit Windows 7 then put that…
Parents
  • Former Member
    Former Member over 11 years ago

    Had a similar issue on Windows 7 x64. Solved with good quality USB cable and correct USB port selection.

     

    The issue was actually in USB port I've been using. Software uses USB device discovery features that requires full USB data cable (no the chap one) and full USB protocol standard support from the controller. So to say, many "front panel" USB 2.0/3.0 ports are also missing full USB support. So I end up connecting my board to the rear USB 1.0/2.0 port (they are usually the first 2-3 ports, where people used to plug mouse and keyboard before). All works like a charm.

     

    I had a very similar issue with Sony camcorder about a year before as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 11 years ago

    Had a similar issue on Windows 7 x64. Solved with good quality USB cable and correct USB port selection.

     

    The issue was actually in USB port I've been using. Software uses USB device discovery features that requires full USB data cable (no the chap one) and full USB protocol standard support from the controller. So to say, many "front panel" USB 2.0/3.0 ports are also missing full USB support. So I end up connecting my board to the rear USB 1.0/2.0 port (they are usually the first 2-3 ports, where people used to plug mouse and keyboard before). All works like a charm.

     

    I had a very similar issue with Sony camcorder about a year before as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data