EAGLE User Support (English) Using different types of thermal connection on a single polygon?
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 354 views
  • Users 0 members are here
  • thermals
  • polygon
Related

Using different types of thermal connection on a single polygon?

Former Member
Former Member over 14 years ago

Hello,
Is it possible to use a thermal connection to a via and a solid connection  to a SMD pad on a single polygon?  Or is it just best to use two separate  polygons with the same name, with one having the thermals where I want, making  sure the two polygons touch to form a single "trace"?
Thank you for your assistance
Jeff

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 14 years ago

    Am 12.05.2011 03:03, schrieb jbliss:

    Hello,

     

    Is it possible to use a thermal connection to a via and a solid connection

     

    DRC - Supply - Generate thermal for vias

     

    > to a SMD pad on a single polygon?

     

    Open library

    Edit package

    CHANGE Thermal off .. click on SMD you will change **

     

    HELP CHANGE --> Pad/via/smd flags

    HELP SMD --> NOTHERMALS

    HELP POLYGON ---> Thermals || Polygon parameters

      • HELP GROUP

     

     

    Or is it just best to use two separate

    > polygons with the same name, with one having the thermals where I want,

    > making  sure the two polygons touch to form a single "trace"?

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 14 years ago

    Is Eagle similar to Altium/Protel?   If so you can set up separate rules for the polygon pours based on whether it is a via or pad, etc.

     

    Message was edited:  (I didn't see the name of the forum when I asked if OP was using Altium!)