EAGLE User Support (English) how to configure wires
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 181 subscribers
  • Views 536 views
  • Users 0 members are here
Related

how to configure wires

Former Member
Former Member over 12 years ago

I am designing an antenna, the corner of the wires should be right angle. By the corner, I mean the corner of a straight wire. For example, when I draw a straight wire 0.5mm wide, 10mm long, but the corner seems to be rounded. How should I change the 4 corners to right corner?

 

Thanks!

  • Sign in to reply
  • Cancel
  • jameslittlefield
    0 jameslittlefield over 12 years ago

    If you set the miter to 0mil and click on the corners they will become

    right angle instead of beveled.

     

    jim

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to jameslittlefield

    Hi James,

     

    Thanks for your reply. But I do not mean the corner of two perpendicular wires. I mean when I draw a wide and straight wire, how should I change the 4 corners of the wire to right angle?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to Former Member

    Wires only have rounded ends

    Arcs can have square ends

     

    You may be able to make an arc that has so little curvature that it works

    for you as a straight line and thus you can have a square end.

     

    Sadly, if you make an arc with a square end and then change the curvature

    to zero, it reverts to a wire with a round end.

     

    I have not checked if the above is true with the latest version so confirm

    it for yourself.

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 04.11.2013 05:45, Bo Bo wrote:

    I am designing an antenna, the corner of the wires should be right

    angle. By the corner, I mean the corner of a straight wire. For example,

    when I draw a straight wire 0.5mm wide, 10mm long, but the corner seems

    to be rounded. How should I change the 4 corners to right corner?

     

    Design the Antenna as a library part and use an SMD pad as "the Antenna

    wire". They can be rectangular.