After the customer component pad is created, how do I assign the pin name or number to it so it will match the symbol?
After the customer component pad is created, how do I assign the pin name or number to it so it will match the symbol?
On 04/25/2014 05:10 PM, Sean Chew wrote:
After the customer component pad is created, how do I assign the pin
name or number to it so it will match the symbol?
You've created a symbol with pins, and a package with pads. The
next step is to create a device. Add the symbol to the device, then
add the package to the device. Use the "Connect" button to connect the
pins in the symbol to the pads in the package.
Don't forget to set the prefix for the reference designator. This is
how resistors start with "R", capacitors start with "C", and such. If
this is not set, eagle defaults to "U$" for the prefix.
HTH,
- Chuck
8883.att1.html.zip |