I am new to eagle.
Using 7.2.0
I have watched a number of tutorials on create a new part library, although all of them are for older versions then 7.2.0.
I manage to create a part watching a tutorial for V4.x although it was very confusing as a lot of the screen shots didn't jive with 7.2.0
The good thing is my part work in my schematic.
Then thing went wrong.
I created more parts and all seemed to go well, IE; combined a package and a symbol into a device, was able to place part on my schematic.
This is where thing went wrong.
Once the part is placed on the schematic it is frozen. IE: i can not move, rotate, delete ,place nodes or any other operation.
also the part i first designed that uses to work is now frozen.
I have uninstalled 7.2.0 and re installed it but did not fix the problem.
Any ideas what is wrong?
Any leads as to a current tutorial using 7.2.0.
Thank
Norm