Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
Forum Colorsound Power boost noise issue
  • Blog
  • Forums
  • Documents
  • Events
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Autodesk EAGLE requires membership for participation - click to join
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 132 replies
  • Answers 52 answers
  • Subscribers 81 subscribers
  • Views 1490 views
  • Users 0 members are here
  • colorsound power boost issue
Related

Colorsound Power boost noise issue

Andy Betts
Andy Betts over 4 years ago

A while ago I posted regarding transistors etc for a Colorsound Power boost clone pedal I was working on. Well, after many months I've actually finished 2 of them... They are identical to an original right down to the size of the PCB.and the components used. There is one slight difference in so far as the first board was a direct print from an Eagle layout, the second board was a 121 trace of an original PCB, only slightly different from the eagle board.

 

This is the Eagle board

This is board 2, a 121 copy of an original Colorsound Power boost PCB, and also a photo of an original

 

The component side is like this.. mine is on the left, the genuine PCB is on the right. The pots on my board are mounted to the board like the original... Just from the other side. The reason for this is purely down to the thread length on the pots. The thread on my pots isn't long enough to go through the PCB, and then through the enclosure as well.

 

20264850_10155652356109783_7777668817152516572_n.jpg?oh=d17440c16b7064d06164d2a2c9783dba&oe=59EEEC46 

 

The schematic used was this one..... a simple circuit which is basically a pre-amp that boosts the volume and treble and bass.

 

 

The components on the first board were all brand new, where the components on the 2nd board were mostly NOS for a visual vintage vibe.

 

I have an issue on both boards that I'm trying to troubleshoot, and currently i have reached out to 2 DIY effect pedal forums with no real resolution. i'm hoping someone here may be able to point me in the right direction, i'll try to give as much information as possible.

 

I have a cycled ticking noise that increases in volume when you turn the volume up on the pedal. it's not affected by the guitar volume, and stays there even when you turn the guitar down. Check out this video.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 

The last video shows a slight earth problem that may or may not have anything to do with the noise. i thought i'd include it anyway.

 

I have taken voltage readings off my pedal, and compared them to the readings from a genuine pedal (I'll say at this stage that my pedal is exactly the same as the genuine pedal as regards component values)

 

Genuine Pedal voltages

Battery: 18.84V

Q1 C 6.43V B 3.92V E 3.54V

Q2 C 11.53V B 6.44V E 5.82V

Q3 C 10.19V B 2.77V E 2.23V

 

 

My voltages:

Battery: 18.80V

Q1 C 6.37V B 3.90V E 3.52V

Q2 C 11.36V B 6.37V E 5.74V

Q3 C 10.54V B 2.75V E 2.19V

  • Reply
  • Cancel
  • Cancel

Top Replies

  • Andy Betts
    Andy Betts over 4 years ago in reply to michaelkellett +7 verified

    Thanks Michael,

     

    I have a very good update...... I think I've discovered what's causing the issue.

     

    I got home from work early, and while there was nobody in the house I started turning things off…

  • jw0752
    jw0752 over 4 years ago +6 suggested

    Hi Andy, and Others,

     

    Tonight I breadboarded the two transistor input amplifier so that I could see what was happening . Here is my bread board set up.

     

     

    I am using  2N22222N2222 transistors and otherwise I…

  • michaelkellett
    michaelkellett over 4 years ago in reply to Andy Betts +6 suggested

    This has got me so intrigued that I'm unwilling to let it go as an unsolved mystery.

     

    If you want to send me the non working board I'll look at with a scope etc and report back on E14.

     

    MK

Parents
  • jw0752
    0 jw0752 over 4 years ago

    Hi Andy,

    You are getting an oscillation that could come from a number of sources. Here is what I observed as differences between the original and the newer units. By mounting the controls on the opposite side you are loosing the shielding that would have been provided by the metal control housings. In the original the treble at least was grounded on the circuit board.  I would tie the metal control housings together and then to a good common ground. Notice how the original control has the input and output lines carefully run down the sides and away from each other. You might even try putting the input lines in coax to help minimizing the chance that they can couple with the output wires. It isn't obvious why the original switch and your switch are different. The difference may be bringing the input and output lines too close together and letting them couple by capacitance. Instead of tying the grounds together on the input and output jacks you might try tying them together on the ground of the circuit board. Hopefully this will give you some experiments to try out. If it doesn't lead to a solution come back and I will try to think of some more.

    John

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to jw0752

    Hi John, thanks for your reply. I'm off to sunny Yorkshire today until Friday, but will check the groundings at the weekend and report back.... In a nutshell, you suspect it's a ground issue?

    • Cancel
    • Up +1 Down
    • Reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 4 years ago in reply to Andy Betts

    Hi Andy, I would start with the simple things like position of the signal wires. Next I would bring all the ground wires to a common point on the circuit board and eliminate loops and strings. Finally I would look at the proximity of things on the switch to see if that is where the problem comes from. Your noticing that the switch has some hum to it may be the unit trying to tell you something.

    John

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to jw0752

    Hi John,

     

    OK, this is what I'll try.

     

    I'll solder some wire between the 3 pots, connecting them together in a string then finally connect the last one to the ground of the board. I'll do the same with each jack socket. This will mean simply drilling 2 or 3 extra holes in the board.

     

    I'll try my best to separate the wiring, and channel it around the edge of the enclosure.

     

    I'll take plenty of pictures so you can see exactly what I've done.

     

    Andy

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 4 years ago in reply to Andy Betts

    Hi Andy,

    That sounds good. One other suggestion, lets have a 1000uF 25 volt capacitor that we can put on the board from the 18 V plus to the Ground. The length of the power wires up to the AC adapter jack and back to the board could be causing the power to pulse at higher volume.

     

    John

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to jw0752

    I'm not 100% convinced that the DC power lines are an issue as this problem occurs using both DC power and batteries. Here is a gut shot of a reissue power boost with an LED, and a DC power socket. This also has a master volume installed

     

    solasound 18v power boost

     

    The difference between the 2 switches is because of the inclusion of the LED. You need the extra pole for the LED.

    I think this is purely a  shielding/grounding issue as you pointed out initially.

     

    When I get home I'll pull the board out of the enclosure, and connect all the pots together and ground them to the pcb, I'll then just connect a battery, and run the board out of the enclosure... I'm sure the issue wasn't there previously when I ran the board out of the enclosure, but process of elimination looks like the key to this issue.

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 4 years ago in reply to Andy Betts

    Hi Andy,

    I just noticed that the original case and the new case are made of metal and your replica is made of plastic. The metal could have a shielding effect that the plastic doesn't give you. I hope the extra ground wires and the separation of the signal in and out wires solves the problem. Keep in mind there are a few possibilities and I may have missed on my guesses.

    John

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to jw0752

    Hi John,

     

    My case isn't plastic, it's a Hammond enclosure made of aluminium.

     

    You are correct the original cases were made of pressed steel.

     

    UPDATE:

    I have removed the board from the enclosure, and removed all the wires from the board. I'll now start a process of elimination.... first of all I'll tidy up all the wiring with new wires and ground the jack sockets to the board, and then test the board as it is, and post a video.... coming soon

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to Andy Betts

    Ok guys, here's the latest update.

     

    I've removed the board from the enclosure, and the noise is still there. It's been wired as basically as possible. I've wired the treble pot to the ground on the board, as the original pedal had the treble pot grounded directly to the board via the body of the pot.

     

    I've checked and triple checked all soldering on the board and there are no solder bridges that I can see.I'm beginning to think it's the board, and maybe during my design phase I did something wrong somewhere.

     

    Anyway, here's the latest video, i think I need to get this sorted before I stuff it into an enclosure.

     

    This video is unavailable.
    You don't have permission to edit metadata of this video.

    • Cancel
    • Up +1 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 4 years ago in reply to Andy Betts

    Hi Andy,

     

    It is a high gain circuit, perhaps some component values were misread (e.g. red instead of brown) on the resistors? In the photos, some colours look brown on the original, but red on the replica. But it could be lighting conditions.

    It would be worth confirming with a multimeter.

     

    As I understand it is an amp with tone controls. According to the video, it is functioning fine when the volume control on it is set low. At that low setting, is the output comparable to the original amp, at the same setting, or at a higher setting? Due to the long wiring, perhaps there is some instability due to the very high gain as that control is turned.

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to shabaz

    Hi Shabaz,

     

    I can understand your query regarding the resistors values, but the values were taken off the schematic, and confirmed by comparison with the following images. one of these images was taken from a boost pedal that is owned by a forum member over at www.freestompboxes.org. The other is a stock image from the internet.

     

    The schematic was drawn by the forum member (Electric Warrior)

     

    The values were confirmed via a thread on that forum last year. Here's a link to the thread on the forum,

     

    freestompboxes.org • View topic - Colorsound Power Boost 18v

     

     

     

    Power_Boost_05.jpg

     

    powerboost.png

    • Cancel
    • Up +1 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to shabaz

    Hi Shabaz,

     

    I can understand your query regarding the resistors values, but the values were taken off the schematic, and confirmed by comparison with the following images. one of these images was taken from a boost pedal that is owned by a forum member over at www.freestompboxes.org. The other is a stock image from the internet.

     

    The schematic was drawn by the forum member (Electric Warrior)

     

    The values were confirmed via a thread on that forum last year. Here's a link to the thread on the forum,

     

    freestompboxes.org • View topic - Colorsound Power Boost 18v

     

     

     

    Power_Boost_05.jpg

     

    powerboost.png

    • Cancel
    • Up +1 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 4 years ago in reply to Andy Betts

    Hi Andy,

     

    I see.. One other thing that could be worth doing (since your circuit appears to work when the gain is set to the lowest setting) is to swap out the 22uF capacitor at the bottom-left of the circuit diagram (i.e. the one connected to the volume pot) and change it to (say) 10uF, and if that doesn't help, also swap out the 4.7uF capacitor at the bottom-right side (the one in parallel with the 1k resistor) and replace that with 2.2uF.

    The old capacitors may have not had the capacitance to match the value written on them, whereas modern capacitors are a bit more closer to the value printed on them. Half the capacitance could be a possibility.

    Also it could be worth lifting up the variable resistors slightly off the PCB, to see if a few additional mm air gap makes a difference. There could be capacitive coupling if the back of the pots is metal, and that will be reduced if the gap is increased.

    • Cancel
    • Up +2 Down
    • Reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Andy Betts
    0 Andy Betts over 4 years ago in reply to shabaz

    Prior to the latest experiment, the pots has plastic dust covers on them that prevented them from touching the board. i have since removed the plastic covers so that i can ground the metal covers to the board.

    • Cancel
    • Up 0 Down
    • Reply
    • Verify Answer
    • Reject Answer