• Designlink empty when using Modules/Hierarchical design

    I created a hierarchical schematic using Modules and now Designlink does not show any components. The BOM export generates a Bill of Materials to a file. I added a resistor to the top level schematic along with the five Modules on the page and Designlink…

  • Rotate Components Less than 90 degree

    Hi

    I have query on Rotate the components with circular board. I can rotate the component 90 degree rotation without any issue, i need to rotate the components 10 or 20 degree. when i rotate 10 ro 20 degree, iam getting lines and pads are creating like…

  • SUPER-Newbie: Eagle

    Hello Ben and Element14 community,

     

    I'm a freshmen studying to get a bachelor's degree in mechanical engineering. I have a lot of projects that I want to start working on. And know that I've started with the first one on my list, I realized that…

  • Can't resolve implicit power pin conflicts.

    How do I resolve the problem with implicit power pins not being allowed to co exist. When different ICs  on the same project have differing power/GND names. ie. GND and V- etc.Eagle will allow only one name when connecting the signals.I have read many…

  • i need help to calculate the output  voltage i want to find the final equation

    hi all friend

    i can't find the output equation of  output voltage of this is circuit

    can  anyone here guide me

    Attachments:
  • Tyco Electronics Footprints para Eagle

    Buenas. Estoy diseñanado una placa de componentes con Eagle y necesito saber si existe alguna librería o página donde encontrar los footprints de los siguientes conectores de Tyco Electronics:

     

    - 215464-6

    - 188275-6

    - 5179029-2

    - 5177983-2

     

    Muchas gracias de…

  • How do I output a multi page pdf of a multi sheet schematic?

    I asked this in the "ask our expert" discussion, but it seems better to use the forum as a forum rather than lots of discussions under one heading - so I'll ask it again as an easier to track item.

    I have a multi sheet schematic, and I'd…

  • BOM + Design Link suggestions

    Hello,

    I think that every user of EAGLE needs the BOM functionnality. We may have differents need, but the aim is the same : generate a BOM file. So I suggest we discuss about making a unique powerfull ULP that will fit every need.

     

    As far as I am concerned…

  • ULP : Design Link + BOM ?

    Hello,

     

    With all my projects, I use a database with the BOM-AM ulp ftp://ftp.cadsoft.de/eagle/userfiles/ulp/bom-am-17.zip. In the database, every component has a farnell reference. But my manufacturer needs the caracteristics of each of the components.…

  • Add power plane to circuit

    Hello.

     

    I am working on a board file for a quadcopter flight control board. I only had access to the Eagle schematic under Creative Commons so I developed a board file from it but got some help with the routing. The person who did this work didn't seem…

  • CUAUV uses EAGLE PCB tools, win big at RoboSub2014!

    Congrats to the Cornell University, Autonomous Underwater Vehicle team who submerged in success winning 1st place at RoboSub2014 competition!

    Team Leader Mark Lee speaks on how EAGLE PCB tools made the difference.

     

    My name is Mark Lee and I am the leader…

  • Serie de presentaciónes de EAGLE en Español

    Noticias al respecto a nuestra serie de presntaciónes en español de EAGLE

    Queremos dejarles saber a todos aquellos que piensan participar del las clases de EAGLE en español que tendremos un invitado muy especial.  Uno de los co-autores del libro “Diseño…

  • CadSoft Sponsors Virginia Tech Race Team

    Virginia Tech Formula SAE Team

     

    VT Formula SAE is a student-led team that challenges Virginia Tech engineering students to design and fabricate a Formula 1 style race car from initial
    concept to reality. Upon completion of the car, the team participates…

  • Electricity at EAGLE PCB Design BOOT CAMP

    A little over a week ago a group of established engineers, makers, hackers, and students met up for our anticipated EAGLE printed circuit board design Boot Camp held here at our CadSoft Computer US offices in Pembroke Pines, FL. Valuable design information…

  • EAGLE Guided Tour Parts 1 - 17

    Walking you through all the major steps of EAGLE

     

  • Eagle 6.5 Design Link SSL error

    I saw this was a problem in older versions, but in 6.5.0 for Mac when I try to use Design Link to search for parts I get the following error:

     

    Error while accessing 'https://api.element14.com/pffind/services/SearchService':

     

    6 SSL handshake fail…

  • Suggestion for EAGLE

    EAGLE is the best PCB software package I've used so far, as It's easy to use, simple, and has a wide range of existing libraries. However, one thing that I'd really like to see included in it is some sort of 3D view. This is available on other packages…

  • Need devices with multiple packages

    My company has designed boards in EAGLE for years, and it's worked well for us.  However, this year, we had a problem with EAGLE and a composite part that caused a run of boards to be populated incorrectly.  Cadsoft support suggested we post a feature…

  • Shortcut keys

    I would like to be able to assign shortcut keys to single letters, like 'm' for move or 'i' for info, when an item is selected.

     

    I would also like to be able to assign the 'del' key to a function (like delete).

  • Allow creating a schematic without creating a board

    I sometimes just want to create a schematic, to demonstrate signal flow, a system overview, or as a refrence for a freewired system. I find myself troubled by the workaround that I have to do to make this work.

     

    I would like to be able to create library…

  • support for microstrip RF design

    For the wishlist...

     

    It would be really cool to have eagle support for high-frequency RF design and if possible, the ability to read directly from qucs file formats.  Qucs is open-source, has a text-based file format, and supports simulation of several types…

  • Pay Project for Eagle Pro [ w/ point bounty ]

    I've been working in Fritzing and have a working design... that needs to have a final home in Eagle. If you are an experienced PCB designer, forward me your rate.

     

    Cheers,

     

    Rick Winscot

    rick[dot]winscot[at]quilix.com

  • Design Link Not Working