• EAGLE Beginners - Introduccíon a EAGLE. Funcionamiento Basico (Spanish)

    to Coordinated Universal Time
    online
    - Introduction to EAGLE Control Panel - Start a project (Schematic) - Place Components on Schematic and define connections a) Define NETS and BUS b) Schematic with Multiple Sheets c) Move components between Sheets d) Define Labels and XRef e) Use Designlink...
  • EAGLE Beginners - Doing the basics (English)

    to Coordinated Universal Time
    online
    - Introduction to EAGLE Control Panel - Start a project (Schematic) - Place Components on Schematic and define connections a) Define NETS and BUS b) Schematic with Multiple Sheets c) Move components between Sheets d) Define Labels and XRef e) Use Designlink...
  • EAGLE Advanced - Multilayer-Leiterplatten (German)

    to Coordinated Universal Time
    online
    - Short introduction to EAGLE control panel - Load a demonstration board - Run DRC to set up multiple layers a) Explanation of + and * b) Explanation of blind and buried vias c) Advantage and disadvantage of Multi-Layer-Boards - Explanation of the difference...
  • CadSoft EAGLE Introduction via WebEx - (German) - 12.00pm (CET)

    to Coordinated Universal Time
    Online
    This live presentation and Q &A session will be for introducing EAGLE and why it is the highest quality, highest value Schematic Capture and Printed Circuit Board Layout CAD software. Details for accessing the webinar will be mailed to you when you register...
  • CadSoft EAGLE Introduction via WebEx - (Mandarin) - 12.00pm (GMT +8)

    to Coordinated Universal Time
    Online
    This live presentation and Q &A session will be for introducing EAGLE and why it is the highest quality, highest value Schematic Capture and Printed Circuit Board Layout CAD software. In the GMT +8 timezone the webinar will last from 12.00pm until 12...
  • EAGLE Beginners - Doing the Basics with EAGLE V6 (Chinese)

    to Coordinated Universal Time
    online
    Register here
  • EAGLE Version 6 - New Features (English)

    to Coordinated Universal Time
    online
    Register here
  • Rotate Components Less than 90 degree

    Hi

    I have query on Rotate the components with circular board. I can rotate the component 90 degree rotation without any issue, i need to rotate the components 10 or 20 degree. when i rotate 10 ro 20 degree, iam getting lines and pads are creating like…

  • Trying to place track in CadSoft Eagle version 6.

    Hi,

    I have for the last 20 years used Protel in a DOS environment, now thinking it's time to move on  I  am trying to get to grips with another PCB design software to this end I have downloaded CadSoft Eagle version 6 complete with tutorial. Having started…

  • Route command problem

    When I want to draw a route from a pad of let's say a  DIL device then I can do it if I draw it at the top layer side. When I then want to draw a second one from the botom side the route color switches automatically to top again and I have no access…

  • Schematic from board layout?

    I've accidentally deleted folder with files of project that i'm working on.. I've managed to recover .brd file, but I cannot recover .sch one.

     

    Is there any way to get schematic from board layout? I've been lurking around, but still nothing…

  • Jeremy Blum's CadSoft Tutorial 2: Board Layout

    element14's Jeremy Blum takes you through his second CadSoft EAGLE tutorial.

     

  • A good tip is always Useful! EAGLE PCB DESIGN TIPS

    Following this very important tip will command EAGLE to run a check on a list of items, amongst them a check on connectivity, unconnected pins, an open nets. A

    basic procedure that is very important in your PCB design process.


  • Suggestion for EAGLE

    EAGLE is the best PCB software package I've used so far, as It's easy to use, simple, and has a wide range of existing libraries. However, one thing that I'd really like to see included in it is some sort of 3D view. This is available on other packages…

  • automatisches fernhalten bei Leiterbahnenkreuzungen oder mindestabstand der Leiterbahnen

    Guten Tag,
    Ich habe ein kleines problem, bei dem ich bis jetzt keine Antwort gefunden  habe. vielleicht habe ich dies auch nur übersehen:
    Wie kann man einstellen, dass wenn man zb über eine andere  Leiterbahn Layoutet, dies automatisch verboten wird? also…
  • Free EAGLE Workshop in Chicago

     

    Hey Chicago -

     

    If anyone in the area is interested in learning EAGLE, then check out this free workshop in Wicker Park on Thursday:

     

    http://cadsoftusa.com/cslogo.gif

     

    Intro to PCB Layout with EAGLECAD

    Alex Barnett @ dorkbot Chicago on Thursday October 28th at 7pm

     

     

     

     

    I’m looking forward to it!