Hi all,
I am reviewing a design I have made time ago, I have seen that a custom device's layout is not correct. After fixing it (within "package" in the my custom library), I'm trying to update the new layout into the .brd file. Unfortunately, with little…
I have a board that has 20 copies of the same charging circuit and I need to copy the physical layout 20 times (in .brd) while showing up in the schematic correct. I know how to copy the schematic and I know how to copy the board layout (without keeping…
Hi
I have query on Rotate the components with circular board. I can rotate the component 90 degree rotation without any issue, i need to rotate the components 10 or 20 degree. when i rotate 10 ro 20 degree, iam getting lines and pads are creating like…
How do I resolve the problem with implicit power pins not being allowed to co exist. When different ICs on the same project have differing power/GND names. ie. GND and V- etc.Eagle will allow only one name when connecting the signals.I have read many…
Hallo,
ich habe einen Stecker aus einem Phoenix Contact Muster generiert, der mir im Board den Fehler Dimension, Drill Distance und Overlap generiert.
Es geht um den Typ OSTV7203151 (On-Shore Technology) zum Anschluss eines NI myDaq. Die Zeichnung zum Stecker…
Hi,
I started learning Eagle by putting existing boards into the schematic editor and then attempting to do the layout the same as the existing board. The problem I have that not all boards are square or rectangular. How can i redefine the board area to…
Hello, I am trying to route a very simple board, but I get airwires that will not automatically route. Any assistance would be appreciated.
Also, can anyone recommend a board maker in Australia?
Is there any way I can share my board schematic for assistance…
Okay so I am using Eagle PCB Power Tools and gbr274x6 to convert a gerber file to use in Eagle 5.10. Everytime I import my AutoCad(DXF) file into GC Prevue and convert that gerber file into a Eagle file format the polygon is not filled. I am wondering…
Hi,
I have for the last 20 years used Protel in a DOS environment, now thinking it's time to move on I am trying to get to grips with another PCB design software to this end I have downloaded CadSoft Eagle version 6 complete with tutorial. Having started…
I generated the Gerber files and found in the *.dri file that I have two drills with 0.0374inch (T03 0.0374inch 2). In the *.drd file I found them with this parameters:
T03
X10260Y24158
X10260Y26158
how can I found them in the board. What type of measuring…
I installed the above mentioned add in. Actually my board is ready. Then I got this message from that add In. As yo can see in the attached screen shots there are still a couple of very short air wires visible. How can I make them disappear? How serious…
When I want to draw a route from a pad of let's say a DIL device then I can do it if I draw it at the top layer side. When I then want to draw a second one from the botom side the route color switches automatically to top again and I have no access…
I've accidentally deleted folder with files of project that i'm working on.. I've managed to recover .brd file, but I cannot recover .sch one.
Is there any way to get schematic from board layout? I've been lurking around, but still nothing…
Hello everyone
I have been using EAGLE for a while now and I very comfortable with the software. Any way I have been working on automating most of the procedure of double sided PCB since manual way generate errors some time.
I am trying to generate the…
element14's Jeremy Blum takes you through his second CadSoft EAGLE tutorial.
…