Hello,
I want to import SPAC265BC12P0.30 AC-DC Switch to Eagle to design my PCB. But, it is not available in the library. How should I import it?
Thanks
Is there a way to set attributes for a package?
Now that you can do 3d models, I'd like to set things like
5mm height for all DIP08
12mm height for all 0412V resistors
4 mm height for all 0412_15 resistors
etc, instead of doing them for individual parts…
Hi Everybody,
I would like to make something like that :
So I drew polygon around pins 8,9,21,22 and pad for L ( polygon and net name "SW") -> OK
I drew 2nd polygon named "GND" for all the card
When calculated (by "rastnet"), polygons…
Well i am fairly new in electronics so forgive me if my question is too stupid to be explained...
I have a new compact nikon digital camera with hdmi out the camera is capable to feed my tv with my footage in real time...Yet i cant find a way to use it…
Hi,
I have an Eagle project with schematic and board. The board is divided into two smaller boards, the "real" device and a separate debug board. I am now going into full scale manufacturing, so I would like to split the project so that I only send the…
Hi all,
I just started with Eagle and I am amazed how powerful this tool is.I would like to create custom pcb for my already existant parts like Arduino Nano, sensor boards and such.
Process would be consisted of adding custom stuff that I have in library…
Anyone have a Eagle Cad lib for TI TMS320C6657 DSP which footprint is S-PBGA-N625?
Hi,
I'm putting components on both sides of a dual layer board, the problem is that the components are all overlapped and I cant really see what is happening - so I wonder if there is a way to hide the components on the bottom layers whilst I work on the…
Hello,
I'm making a design with Eagle 7.2.0 and using the hierarchy feature. In each hierarchic bloc, the name of each component starts from 1 (U1, U2, ...). The problem is on the PCB design, because the hierarchic bloc name is added in each component…
Compré un relay identificado como HK4100F. He intentado con diferentes partesde Eagle pero no logro hacer coincidir las dimensiones en la PCB con las reales fisicas del componente. Como hago para hacer coincidir ambas partes?
Datasheet: http://ww1.microchip.com/downloads/en/DeviceDoc/22248a.pdf
Not sure if I need to download a new library or if there's something built in that has a similar enough case it will work for my PCB. Thanks!
Hi guys, when I make a custom library I place pads for through hole components.
On single layer I find pad only on bottom layer (of course) but when working on duble layer board I find pad on both layers (top and bottom).
How can I set pad only for bottom…
I'm making a two layer board for the first time, and have come across a question regarding component placement.
Say for example I have a through hole DC-DC converter. This converter has four pins and will be placed on the top of the board, therefore…
hi, thanks for clicking. i've been doing some pcb design, and would like to panelise some. i've tried the panelize.ulp, which works kind of ok, but the label alignment is off and it defeats the object of using it if i then have to manually move all of…
Hi all,
I am reviewing a design I have made time ago, I have seen that a custom device's layout is not correct. After fixing it (within "package" in the my custom library), I'm trying to update the new layout into the .brd file. Unfortunately, with little…
Hello, can anyone tell me is the vias okay like this in the pic? Appreciate lots ^^
Ok,
Im trying to lay out a PCB for my sinor design project and dont have a foot print for a sim card holder the sim card holder i have can be found here C707 10M006 0492 Amphenol-Tuchel Electronics | 361-1021-6-ND | DigiKey if anyone can direct me to…