Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Blog CircuitStudio Routing with Accordions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14softwareuk
  • Date Created: 27 Jul 2017 3:15 PM Date Created
  • Views 4087 views
  • Likes 2 likes
  • Comments 5 comments
  • altium
  • circuit studio
  • pcb design
  • altium circuitstudio
Related
Recommended

CircuitStudio Routing with Accordions

e14softwareuk
e14softwareuk
27 Jul 2017

I've had some support queries recently regarding the suitability of CircuitStudioCircuitStudio for high speed design so I would like to introduce you to what CircuitStudio offers the PCB designer with regards to individual net length tuning rules and accordions.

 

Load up CircuitStudio, pick a PCB project and follow along if you wish. The sample board shown has one net (B6) which we are going to concentrate on. Turn on the PCB net information panel, this will show us the routed and unrouted net lengths and make it easy to select a net and highlight it (as seen in the screenshots).

image

 

Here's the net routed without an accordion. Clicking on the net name in the list on the left will highlight the net on the PCB and also zoom in to focus on it.

image

 

Unroute the connection and then start a new route (R command), hit SHIFT+A to enter accordion mode then TAB to bring up the property dialog.

image

 

Click OK and continue to route, an accordion will be placed as you go. Use SHIFT+A to enter and leave accordion mode anytime during routing. You might end up with something that looks like this.

image

 

When you exit routing mode the net lengths in the left panel will update to show the new routed (and unrouted) length. Let's now set some min/max length rules to see what happens. Rip up the connection, start routing again and use SHIFT+A, TAB to bring up the accordion dialog. This time click the "Create Rule From Length..." option.

image

 

Here we have set the Minimum to 2000mil and the maximum to 4000mil. Click OK to return to the main dialog the select the "From Rules" radio button. Click OK to continue routing.

image

 

This time when you route the net with accordion mode enabled the accordion itself does not follow the whole trace, only partially in order to increase the net length slightly. Also highlighted is an overlay that follows the cursor showing the min/max and current routing lengths - very handy.

image

 

And finally a handy tip, hit SHIFT+F1 whilst routing in accordion mode and you get a list of available shortcuts. As you can see many are related to the accordion mode and let you adjust parameters without having to keep returning to the main dialog.

image

 

Hope these tips have helped and that you all keep enjoying CircuitStudio and producing great boards.

  • Sign in to reply

Top Comments

  • jcbottorff@pmatrix.com
    jcbottorff@pmatrix.com over 8 years ago +1
    Just a little detail, it seems once you create a length design rule from the interactive length tool, it's impossible to edit or delete them, as CircuitStudio does not show any of the high speed design…
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to jcbottorff@pmatrix.com +1
    Whilst true that the rules are somewhat hidden and do not appear in the main Design Rule dialog you can edit them. Just like when setting a rule, start routing, hit SHIFT+A for accordion mode then TAB…
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to saravananeceait +1
    Yes there is, see your other post. I would respectfully ask that you don't spam the forum by asking the same question in multiple places as this just leads to confusion and makes finding the correct answer…
Parents
  • jcbottorff@pmatrix.com
    jcbottorff@pmatrix.com over 8 years ago

    Just a little detail, it seems once you create a length design rule from the interactive length tool, it's impossible to edit or delete them, as CircuitStudio does not show any of the high speed design rules in the normal design rules dialog.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jcbottorff@pmatrix.com
    jcbottorff@pmatrix.com over 8 years ago

    Just a little detail, it seems once you create a length design rule from the interactive length tool, it's impossible to edit or delete them, as CircuitStudio does not show any of the high speed design rules in the normal design rules dialog.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14softwareuk
    e14softwareuk over 8 years ago in reply to jcbottorff@pmatrix.com

    Whilst true that the rules are somewhat hidden and do not appear in the main Design Rule dialog you can edit them. Just like when setting a rule, start routing, hit SHIFT+A for accordion mode then TAB for property dialog. From there select "From Rules" and the existing rule will appear in the right hand box, double click on it to edit. Alternatively just clicking "Create Rule from Length" will overwrite the existing rule. Not found a way to completely delete the rule though but I'm not sure that is actually a necessity.

    • Cancel
    • Vote Up +1 Vote Down