Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum ERROR: Board Stack Report not Working
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Locked Locked
  • Replies 3 replies
  • Subscribers 89 subscribers
  • Views 1733 views
  • Users 0 members are here
  • frontpage
  • board stack report
  • circuitstudio 1.4
  • error
  • circuitstudio
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

ERROR: Board Stack Report not Working

diond31
diond31 over 8 years ago

Hi Element14 Circuitstudio Support,

 

I have two seats of Circuitstudio (running version 1.4).  My seat at home (Windows 7, Microsoft Office 2016) creates the Board Stack Report without any issue (i.e. Excel document showing layers, thicknesses, etc.).  My seat at work (Windows 7, Microsoft Office 2016) produces an "Interface not supported" error message.  It does not work using the Output >> Board Stack Report or Project >> Generate Output >> Report Board Stack (checked).

 

I've searched on-the-line and I'm unable to find a fix (similar to IPC2581 fix) for this issue and frankly I don't understand why it works on one system (home), but not the other (work).  Please help with a solution.

 

Thanks & Best Regards,

Dion

Attachments:
image
image
  • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago

    It could be down to differences in the way Office 2016 is installed. I would suggest trying to make sure the work installation matches home and then perhaps try to repair Office 2016. Is it possible you have had older versions of office installed at home but not at work?

    To repair Office 2016:

    1. Open up the Control Panel on your PC (and show All Control Panel items, if necessary) and click on Programs, then Programs and Features.
    2. Find Microsoft Office 2016 in the list and highlight it.(Selection also say Microsoft Office 365)
    3. Click Change.
    4. Select Quick Repair and Repair then follow the prompts.
    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • diond31
    0 diond31 over 8 years ago in reply to e14softwareuk

    Hey Peter,

     

    Thanks for the suggestion.  Unfortunately, running the repair on Office 2016 didn't work.

     

    I checked the path to Circuitstudio and noticed that its in the 32-bit Program Files (x86) folder.  Therefore, I uninstalled the x64 version of Microsoft Office 2016 (on work machine) and installed the 32-bit version, Viola!  The Board Stack Report now works from both Outputs >> Board Stack Report and Generate Output >> Report Board Stack (checked).

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • e14softwareuk
    0 e14softwareuk over 8 years ago in reply to diond31

    Many thanks for the providing feedback on the solution. Having two virtually identical setups is quite rare so very valuable information that 64-bit Office 2016 looks not to be compatible.