Altium CircuitStudio
  • Products
  • Manufacturers
  • Altium CircuitStudio
  • More
  • Cancel
Altium CircuitStudio
Altium CircuitStudio Forum Altium Showcases TASKING Toolset and LAPACK Performance Libraries for Infineon at Embedded World
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Altium CircuitStudio to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 0 replies
  • Subscribers 88 subscribers
  • Views 308 views
  • Users 0 members are here
  • altium
  • tasking
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Altium Showcases TASKING Toolset and LAPACK Performance Libraries for Infineon at Embedded World

prisma
prisma over 8 years ago


Press Release 1/2018

 

 

Altium Showcases TASKING Toolset and LAPACK Performance Libraries for Infineon at Embedded World

 

Altium displays their TASKINGRegistered Toolset at Embedded World. TASKING delivers a full set of tools to help embedded software developers design and verify real-time, safety-critical, multicore applications. Special focus is on the latest release of the LAPACK Performance Libraries, co-designed with Infineon, aimed at simplifying complex tasks such as ADAS.

 

 

San Diego, Calif. - 27 February 2018 - Altium, a global provider of embedded software tools for automotive technology, is excited to showcase the full TASKING Toolset at Embedded World this month in Nuremberg, Germany. TASKING focuses on providing a full set of embedded software development tools for safety-critical, real-time, multicore applications in the automotive, agricultural and industrial markets.

 

TASKING has expanded its development toolset to meet customers’ needs with tools that improve code generation, enhance use of multicore hardware, and most importantly, fulfill safety requirements. From the compiler and code profiler to the safety checker and cost-efficient debugger, TASKING supplies the tools developers need for the ever-more-complex applications demanded by the rapidly advancing automotive industry.

TASKING Toolset & LAPACK Performance Libraries for Infineon

Co-designed with Infineon, the TASKING Toolset includes several tools that enable developers to maximize performance, especially taking advantage of multicore features and capabilities. The compiler and linker/locator are optimized for multicore operation and allow developers to customize their software builds to exploit all the performance of the hardware.

 

The newly updated LAPACK (Linear Algebra PACKage) Performance Libraries, including Basic Linear Algebra Subroutines (BLAS), is the first production set of LAPACK available in C. This means that developers can cut substantial coding time by calling LAPACK library functions directly in the C code to solve complex mathematical operations. The decades-long use of LAPACK ensures accurate results in a safety-critical environment. In addition, using LAPACK makes application portability much easier.

 

Altium developed the TASKING LAPACK Performance Libraries with Infineon to deliver state-of-the-art applications that are easy to develop and maintain. “Besides TASKING Embedded Profiler, the TASKING Performance Libraries are an additional area where both Infineon Technologies and Altium have been working closely together,” says Mr. Ralf Ködel, Director Product Marketing, Automotive & Industrial MicroController at Infineon Technologies. “Those Libraries will help Infineon AURIXTm customers to speed up computing complex ADAS applications, especially in the areas of radar, sensor fusion and Lidar.”

System Optimization and Improved Safety

In addition to showcasing the updated LAPACK Performance Libraries, TASKING will also highlight the performance-optimizing and safety-critical applications featured in TASKING. The TASKING VX Toolkit for GTM allows developers to generate complex timing and PWM waveforms, while programming in C enables users to quickly design and generate maintainable code. The TASKING Embedded Profiler, co-designed with Infineon experts, allows developers to easily identify and implement code changes, saving considerable time and labor. Also featured is the TASKING Embedded Debugger — a simple, integrated solution for code verification. At an accessible price, developers can now own enough debugger licenses to verify code functionality without delay or interruption in development workflow.

 

Safety is also a priority for any developer designing products for the automotive and agricultural industries. Products must be able to pass the stringent requirements of ISO 26262 to be sold into automotive applications. Among those safety requirements is to ensure that computing systems have freedom from interference. Developers can accelerate and automate analysis to ensure freedom from interference using the TASKING Safety Checker. This tool is the only ASIL-partition-aware static analysis tool, making verification quick and accurate.

Visit the TASKING Booth at Embedded World

Visitors at this year’s Embedded World will have the opportunity to explore all of the new and exciting features available in TASKING. There will be a live demo in Booth #4.240 each day (27 February through 1 March). Attendees can also drop by anytime to talk about TASKING and our complete set of tools.

 

For more information on the TASKING LAPACK Performance Libraries, click here to visit the product webpage. For more information on the TASKING GTM C Compiler, click here.

 

Contacts

Camaryn Bolton

Altium
+1 858 864 1593

pr@altium.com

 

Gabriele Amelunxen
PRismaPR
+49 8106 247 233
info@prismapr.com

 

About TASKING

TASKING is an Altium brand. TASKING development tools are used by carmakers and the world's largest automotive Tier-1 suppliers to develop embedded microcontroller based power train, body control and ADAS related applications around the globe. More than ten thousand users rely on the TASKING development tools to create richer next-generation applications while achieving optimum reliability, security, and performance. In 2017 the TASKING brand celebrates its 40th anniversary of technology leadership, quality tools and customer support excellence.

About Altium

Altium LLC (ASX:ALU) is a multinational software corporation headquartered in San Diego, California, that focuses on electronics design systems for 3D PCB design and embedded system development. Altium products are found everywhere from world leading electronic design teams to the grassroots electronic design community.

 

With a unique range of technologies Altium helps organisations and design communities to innovate, collaborate and create connected products while remaining on-time and on-budget. Products provided are ACTIVEBOMRegistered, ActiveRouteRegistered, Altium DesignerRegistered, Altium VaultRegistered, AutotraxRegistered, CamtasticRegistered, CiivaTm, CIIVA SMARTPARTSRegistered, CircuitMakerRegistered, CircuitStudioRegistered, CodemakerTm, Common Parts LibraryTm, DraftsmanRegistered, DXPTm, EasytraxRegistered, NanoBoardRegistered, NATIVE 3DTm, OCTOMYZERegistered, OctopartRegistered, P-CADRegistered, PCBWORKSRegistered, PDN AnalyzerTm, ProtelRegistered, SitusRegistered, SmartPartsTm and the TASKINGRegistered range of embedded software compilers.

 

Founded in 1985, Altium has offices worldwide, with US locations in San Diego, Boston and New York City, European locations in Karlsruhe, Amersfoort, Kiev, Munich, Markelo and Zug, and Asia Pacific locations in Shanghai, Tokyo and Sydney. For more information, visit www.altium.com. You can also follow and engage with Altium via Facebook, Twitter, LinkedIn and YouTube.

 

  1. www.altium.com