Analog Devices
  • Products
  • Manufacturers
  • Analog Devices
  • More
  • Cancel
Analog Devices
Forum PROBLEM whith MAX17632C
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Analog Devices to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 40 subscribers
  • Views 1485 views
  • Users 0 members are here
Related

PROBLEM whith MAX17632C

Fabrizio70
Fabrizio70 over 1 year ago

v   image

Hi , I have a problem whith  max17632c i use it for dc/dc 24v/5v  .if i put  i small load ( 100mW) the output voltage is 4,0V  , while i put a load of  2W  tthe output voltage go to 2,5V.

then i desolder  the condensator  C1 (2,2 uF 10V ceramic used for bypass ldo pin 2) and i have 5v output  whit load of 2W (the condensator  not  have problem) , Where is the prblem?

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 1 year ago +1
    Since it is a switching regulator, we need to see the PCB. I always suspect layout issues first with switchers. It would also be nice to see the entire schematic. Like with code, snippets rarely contain…
  • Fabrizio70
    Fabrizio70 over 1 year ago in reply to dougw +1 verified
    The output voltage whiout load and c1 installade is 5,09 V , while whit load of 2W and c1 installated is 2,35 v and the voltage on the C1 is 5,06 if i dessolder c1 the output voltage is right 5.06 whit…
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.