Digilent, a National Instruments Company
  • Products
  • Manufacturers
  • Digilent, a National Instruments Company
  • More
  • Cancel
Digilent, a National Instruments Company
Blog Analog Discovery 3 - What's different?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Digilent, a National Instruments Company to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: steveradecky
  • Date Created: 9 Aug 2023 1:38 PM Date Created
  • Views 9692 views
  • Likes 8 likes
  • Comments 4 comments
  • oscilloscope.
Related
Recommended

Analog Discovery 3 - What's different?

steveradecky
steveradecky
9 Aug 2023

This article details the differences in the new Analog Discovery 3 vs the Analog Discovery 2.

Lower Price than Analog Discovery 2

Backwards compatible with Analog Discovery 2 projects — so long as it didn’t use the 1.8 V input setting for digital pins.

Adjustable System Clock Frequency between 50 MHz and 125 MHz, allowing for up to a 125 MS/s simultaneous sampling rate on all channels for the analog inputs, analog outputs, and digital I/O.

All instruments always available in every configuration. No more losing access to digital I/O when allocating more buffer to the Wavegen.

USB Type C connection, USB 2.0 data rate. USB 3.2 Gen 1’s extra throughput didn’t add enough value in most applications.

Two differential 14-bit resolution analog inputs with 9 MHz bandwidth at -3 dB when using the MTE cables. Up to 16 bit resolution when sampling at 1/4 of the system clock frequency. ±2.5 V and ±25 V input ranges. Maximum sample buffer size doubled from 16k to 32k per channel (64k when only using 1 channel). Hardware FIR filters for each input. Record mode rate increased to 10 MS/s. Digital loopback of Wavegen and Power Supply output supported.

Two single ended ±5 V analog outputs with 14-bit resolution and 9 MHz bandwidth at -3 dB when using MTE cables. Maximum sample buffer size doubled from 16k to 32k per channel. FM/PM and AM/SUM buffers on each channel increased to a minimum of 2k samples with 16-bit resolution. Digital loopback of received Scope data supported.

16 digital I/O pins at 3.3 LVCMOS supporting 5 V inputs. Maximum sample size doubled from 16k to 32k per channel. All digital pins and the two trigger pins can have their Pull resistor configured.

– +5 V and -5 V power supplies now supply up to 800 mA (2.4 W) each. Integrated readback of the supplied voltage supported.

Analog Discovery 3

image

  • Sign in to reply
Parents
  • genebren
    genebren over 2 years ago

    A good thing getting better! Now that is the way things are supposed to work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • steveradecky
    steveradecky over 2 years ago in reply to genebren

    Yep! We agree!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • steveradecky
    steveradecky over 2 years ago in reply to genebren

    Yep! We agree!