HARTING
  • Products
  • Manufacturers
  • HARTING
  • More
  • Cancel
HARTING
Blog PushPull: A secure fit with just one click
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join HARTING to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: martinbatin
  • Date Created: 14 Nov 2018 4:57 PM Date Created
  • Views 4982 views
  • Likes 3 likes
  • Comments 6 comments
  • iiot
  • signal
  • electronic device
  • connector
  • wire & cable
  • harting
  • pushpull
  • robust
  • industry 4
  • power cables
  • data
  • robust lock
Related
Recommended

PushPull: A secure fit with just one click

martinbatin
martinbatin
14 Nov 2018

A secure fit with just one click

There are many factors to consider when it comes to choosing a suitable connector for panels or control cabinets. Robustness, reliability and adaptability are all high on the list, but as businesses embrace more flexible production processes, simple handling and ease of use are becoming increasingly important.

Control cabinets often contain a myriad of switches and connections, so the ability to quickly and efficiently disconnect and reconnect the industrial lifelines of data, signal and power are vital if expensive machine downtime is to be avoided. That’s where HARTING’s PushPull technology comes into its own!

Developed with the user in mind, the PushPull family is available in a range of materials to suit your requirements. From the robust V4 Industrial with its housing that protects from aggressive industrial chemicals to the sleek M12 with its capacity to deliver data transfer rates of up to 10GBit/s, the entire ranges relies on a simple yet effective connection method.

image

Simple operation

As its name suggests, PushPull incorporates an uncomplicated connection and termination technique that ensures absolute dependency and reliability. This intuitive, tool-free method guarantees an error-free connection as the two sections click into place, the audible feedback indicating the connection is secure. The sturdy housing is also inscribed with pronounced contours, which gives the operator a firm grip on the connector, even in the most challenging industrial environments. All these features allow interfaces to be changed quickly and easily without the need for specialist training.

Colour coding

To further simplify the process and eliminate the possibility of incorrect connections, HARTING has fitted the PushPull range with colour-coded marks. The first is a yellow triangle which appears on both the plug and socket, meaning it’s incredibly easy to ensure both connections are orientated correctly before they are mated. This saves time for the operator, especially on projects where many interfaces need to be connected!

Secondly, the user has the option to allocate colour codes to each PushPull plug and socket in an installation. For example, they could easily colour code data, signal and power lines to ensure each line can be easily identified; a simple system to help reduce cabling errors.

Secure and adaptable

In addition to the audible click, the PushPull range also comes with a spin-lock which firmly secures the connecter in a mated condition, preventing any inadvertent disconnection. Simply plug in the PushPull then rotate the ring one-eighth of a turn clockwise to lock and secure the connection.

Finally, when it comes to variety, the PushPull range can handle all your requirements. Whether you’re looking to transmit data via an RJ45 or 690V / 16A of power via 5 poles, HARTING’s range of interfaces, inserts and housing materials can provide universal solutions for your specific applications.

 

Click here for PushPull

  • Sign in to reply

Top Comments

  • martinbatin
    martinbatin over 7 years ago +2
    Hello both, Apologies for the button not working but I have fixed it, should be working now! Kind regards, Martin
  • gadget.iom
    gadget.iom over 7 years ago +1
    Not sure if it's just me, but the "Click here for PushPull" button doesn't seem to work.
  • shabaz
    shabaz over 7 years ago in reply to gadget.iom +1
    Interesting connectors.. I notice they have LAN connectors in this series too. The link doesn't work for me either.
Parents
  • martinbatin
    martinbatin over 7 years ago

    Hello both,

     

    Apologies for the button not working but I have fixed it, should be working now!

     

    Kind regards,

     

    Martin

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • martinbatin
    martinbatin over 7 years ago

    Hello both,

     

    Apologies for the button not working but I have fixed it, should be working now!

     

    Kind regards,

     

    Martin

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • gadget.iom
    gadget.iom over 7 years ago in reply to martinbatin

    Thanks. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • martinbatin
    martinbatin over 7 years ago in reply to gadget.iom

    You're welcome!
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.