Intel
  • Products
  • Manufacturers
  • Intel
  • More
  • Cancel
Intel
Blog CapperLabs Greenhouse Controller - Blog 6 - Automatic Vent
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Intel to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rsc
  • Date Created: 25 Apr 2017 2:06 PM Date Created
  • Views 1304 views
  • Likes 3 likes
  • Comments 5 comments
  • greenhouse
  • intel_project
  • intel edison
Related
Recommended

CapperLabs Greenhouse Controller - Blog 6 - Automatic Vent

rsc
rsc
25 Apr 2017

CapperLabs Greenhouse Controller Table of Contents

Blog 1 Introduction
Blog 2 System Components
Blog 3 Intel Edison
Blog 4 Grove-y
Blog 5 Round and Round
Blog 6 Automatic Vent

Getting back to the Greenhouse project, my first sub-system to control is the window vent.

The greenhouse came with two vent actuators, one manual, and one automatic based on internal temperature.

The automatic opener works ok, but can't tell if its raining outside and the opening temperature can't be adjusted.

Here's the original assembly:

image

The unit operates using a cylinder containing a wax mixture that expands with increased temperature.

My goal is to replace the cylinder with a screw drive and stepping motor.

This is the screw drive I removed from some old equipment:

image

Modifications are needed to adapt the screw drive brass bearing holder to the lever arm:

image

After a few hours of cutting/grinding/pulling hair out/swearing, and a bandage or two, the screw drive is complete:

The screw nut is attached to the end of a brass pipe so I can get about 3 inches of travel to allow the actuator arms to open fully.

The pipe was used to allow the screw to close the actuator without traveling out the end of the unit.

image

Now all I need to do is attach the stepper motor to the screw shaft and connect it to a motor controller.

The Edison will control motor microstepping and direction.  I may need to add limit switches also, since there isn't any location feedback.

The SeedStudio motor shield doesn't work with the Edison Arduino board - probably not enough GPIO drive current.  I may use an aux Arduino to run the motor and send commands from the Edison.  Here's a short video of the Arduino controlling the stepper motor.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +1
    I agree, limit switches are a necessary item. You also might consider a rain sensor to close the window if the weather turns nasty. DAB
  • rsc
    rsc over 5 years ago in reply to dubbie +1
    It's been so hot this summer I've left the window and door open on the greenhouse all day all month and had to put a tarp on the roof to keep the sun out. Scott
Parents
  • rocburn
    rocburn over 5 years ago

    Thanks for sharing Automatic Vent. I like all the points that you have mentioned. We recently wrote one blog on Natural Ventilation Types, Working and Benefits which is really helpful for every homeowner (https://www.window-openers.com/news/natural-ventilation-types-benefits/). Sorry for the link, but we thought it might be helpful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rocburn
    rocburn over 5 years ago

    Thanks for sharing Automatic Vent. I like all the points that you have mentioned. We recently wrote one blog on Natural Ventilation Types, Working and Benefits which is really helpful for every homeowner (https://www.window-openers.com/news/natural-ventilation-types-benefits/). Sorry for the link, but we thought it might be helpful.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.