It's been a very hot summer, and vents haven't been enough to cool the greenhouse - even with a green tarp on the roof and the door open.
The temperature inside has been over 100F during peak sun hours.
I don't like to leave the door open because any number of critters tend to wander inside.
I've been using a floor fan next to the door to help exchange air. This week I added a 6-inch fan and louvered vent so I can control it with a relay.
Here's a pic:
I've been working more with the LattePanda board these past few weeks rather than the Edison board.
I haven't decided what platform I will use for the final controller. I'm planning on mounting the space heater and watering system next.
So many projects...........
Scott
Top Comments
I have water from the house. I have some water tanks I plan to use for a plant watering closed-system. I thought about evaporative cooling, but I think it would cause mold to build up.
I also have a portable…
Yes a farmer's work is never done. Too hot, too cold, too wet, too dry. It just never ends.
I do like your setup. It will take you a while to work out the best heating and cooling technics.
Do you have…
Are those Jalapenos?
Remember, peppers are heavy feeders, so make sure you give them the nutrients they need to grow big and HOT!
DAB