<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/"><channel><title>Protect your DUT with power supply features including a watchdog timer</title><link>https://community.element14.com/products/manufacturers/keysight/w/documents/23653/protect-your-dut-with-power-supply-features-including-a-watchdog-timer</link><description /><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>Protect your DUT with power supply features including a watchdog timer</title><link>https://community.element14.com/products/manufacturers/keysight/w/documents/23653/protect-your-dut-with-power-supply-features-including-a-watchdog-timer</link><pubDate>Tue, 09 Nov 2021 17:06:09 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:1f584986-9b47-459c-b568-f13f37ad18ce</guid><dc:creator>keysight</dc:creator><comments>https://community.element14.com/products/manufacturers/keysight/w/documents/23653/protect-your-dut-with-power-supply-features-including-a-watchdog-timer#comments</comments><description>Current Revision posted to Documents by keysight on 11/9/2021 5:06:09 PM&lt;br /&gt;
&lt;p class="entry-title post-title" style="margin:0;"&gt;&lt;em&gt;&lt;span style="font-size:10pt;"&gt;This and other great power products tips and tricks can be found on the &lt;a class="jive-link-external-small" href="http://powersupplyblog.tm.agilent.com/" rel="nofollow ugc noopener" target="_blank"&gt;Watt&amp;#39;s Up? Blog&lt;/a&gt;&lt;/span&gt;.&lt;/em&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:14pt;"&gt;&lt;a class="jive-link-external-small" href="http://powersupplyblog.tm.agilent.com/2012/03/protect-your-dut-with-power-supply.html" rel="nofollow ugc noopener" target="_blank"&gt;Protect your DUT with power supply features including a watchdog timer&lt;/a&gt; &lt;/span&gt;&lt;/p&gt;&lt;p class="post-header" style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;The two biggest threats of damage to your device under test (DUT) from a power supply perspective are excessive voltage and excessive current. There are various protection features built into quality power supplies that will protect your DUT from exposure to these destructive forces. There are also some other not-so-common features that can prove to be invaluable in certain applications.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Soft limits&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;The first line of defense against too much voltage or current can be using soft limits (when available). These are maximum values for voltage and current you can set that later prevent someone from setting output voltage or current values that exceed your soft limit settings. If someone attempts to set a higher value (either from the front panel or over the programming interface), the power supply will ignore the request and generate an error. While this feature is useful to prevent accidentally setting voltages or currents that are too high, it cannot protect the DUT if the voltage or current actually exceeds a value due to another reason. Over-voltage protection and over-current protection must be used for these cases.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Over-voltage protection&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;Over-voltage protection (OVP) is a feature that uses an OVP setting (separate from the output voltage setting). If the actual output voltage reaches or exceeds the OVP setting, the power supply shuts down its output, protecting the DUT from excessive voltage. The figure below shows a power supply output voltage heading toward 20 V with an OVP setting of 15 V. The output shuts down when the voltage reaches 15 V.&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;a href="http://4.bp.blogspot.com/-luYy6J9PLyg/T3Tjz9PmRYI/AAAAAAAAALo/qqR664YX8sg/s1600/OVP%2Bexample.jpg" rel="nofollow ugc noopener" target="_blank"&gt;&lt;img alt="image" border="0" class="jiveImage" src="http://4.bp.blogspot.com/-luYy6J9PLyg/T3Tjz9PmRYI/AAAAAAAAALo/qqR664YX8sg/s400/OVP%2Bexample.jpg" style="margin:0 auto 10px;text-align:center;"  /&gt;&lt;/a&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;Some power supplies have an SCR (silicon-controlled rectifier) across their output that gets turned on when the OVP trips essentially shorting the output as quickly as possible. Again, the idea here is to protect the DUT from excessive voltage by limiting the voltage magnitude and exposure time as much as possible. The SCR circuit is sometimes called a “crowbar” circuit since it acts like taking a large piece of metal, such as a crowbar, and placing it across the power supply output terminals.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Over-current protection&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;Over-current protection (OCP) is a feature that uses the constant current (CC) setting. If the actual output current reaches or exceeds the constant current setting causing the power supply to go into CC mode, the power supply shuts down its output, protecting the DUT from excessive current. The figure below shows a power supply output current heading toward 3 A with a CC setting of 1 A and OCP turned on. The power supply takes just a few hundred microseconds to register the over-current condition and then shut down the output. The CC and OCP circuits are not perfect, so you can see the current exceed the CC setting of 1 A, but it does so for only a brief time.&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;a href="http://1.bp.blogspot.com/-JGfl_21oWc8/T3TkIWOlldI/AAAAAAAAAL0/Q0CLViaLLkU/s1600/OCP%2Bexample.jpg" rel="nofollow ugc noopener" target="_blank"&gt;&lt;img loading="lazy" alt="image" border="0" class="jiveImage" src="http://1.bp.blogspot.com/-JGfl_21oWc8/T3TkIWOlldI/AAAAAAAAAL0/Q0CLViaLLkU/s400/OCP%2Bexample.jpg" style="margin:0 auto 10px;text-align:center;"  /&gt;&lt;/a&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;The OCP feature can be turned on or off and works in conjunction with the CC setting. The CC setting prevents the output current from exceeding the setting, but it does not shut down the output if the CC value is reached. If OCP is turned off and CC occurs, the power supply will continue producing current at the CC value basically forever. This could damage some DUTs as the undesired current flows continuously through the DUT. If OCP is turned on and CC occurs, the power supply will shut down its output, eliminating the current flowing to the DUT.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;Note that there are times when briefly entering CC mode is expected and an OCP shutdown would be a problem. For example, if the load on the power supply has a large input capacitor, and the output voltage is set to go from zero to the programmed value, the cap will draw a large inrush current that could temporarily cause the power supply to go into CC mode while charging the cap. This short time in CC mode may be expected and considered acceptable, so there is another feature associated with the OCP setting that is a delay time. Upon a programmed voltage change (such as from zero to the programmed value as mentioned above), the OCP circuit will temporarily ignore the CC status just for the delay time, therefore avoiding nuisance OCP tripping.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Remote inhibit&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;Remote inhibit (or remote shutdown) is a feature that allows an external signal, such as a switch opening or closing, to shutdown the output of the power supply. This can be used for protection in a variety of ways. For example, you might wire this input to an emergency shutdown switch in your test system that an operator would use if a dangerous condition was observed such as smoke coming from your DUT. Or, the remote inhibit could be used to protect the test system operator by being connected to a micro switch on a safety cover for the DUT. If dangerous voltages are present on the DUT when operating, the micro switch could disable DUT power when the cover is open.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Watchdog timer&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;The watchdog timer is a unique feature on some Keysight power supplies, such as the N6700 series. This feature looks for any interface bus activity (LAN, GPIB, or USB) and if no bus activity is detected by the power supply for a time that you set, the power supply output shuts down. This feature was inspired by one of our customers testing new chip designs. The engineer was running long-term reliability testing including heating and cooling of the chips. These tests would run for weeks or even months. A computer program was used to control the N6700 power supplies that were responsible for heating and cooling the chips. If the program hung up, it was possible to burn up the chips. So the engineer expressed an interest in having the power supply shut down its own outputs if no commands were received by the power supply for a length of time indicating that the program has stopped working properly. The watchdog timer allows you to set delay times from 1 to 3600 seconds.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;strong&gt;Other protection features that protect the power supply itself&lt;/strong&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;There are some protection features that indirectly protect your DUT by protecting the power supply itself, such as over-temperature (OT) protection. If the power supply detects an internal temperature that exceeds a predetermined limit, it will shut down its output. The temperature may rise due to an unusually high ambient temperature, or perhaps due to a blocked or incapacitated cooling fan. Shutting down the output in response to high temperature will prevent other power supply components from failing that could lead to a more catastrophic condition.&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;One other way in which a power supply protects itself is with an internal reverse protection diode across its output terminals. As part of the internal design, there is often a polarized electrolytic capacitor across the output terminals of a power supply. If a reverse voltage from an external power source was applied across the output terminals, the cap (or other internal circuitry) could easily be damaged. The design includes a diode across the output terminals with its cathode connected to the positive terminal and its anode connected to the negative terminal. The diode will conduct if a reverse voltage from an external source is applied across the output terminals, thereby preventing the reverse voltage from rising above a diode drop and damaging other internal components.&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;

&lt;div style="font-size: 90%;"&gt;Tags: current, application, tips, modular_power_supply, battery, voltage, modular, demo, demonstration, Application Notes, dc, power, n6700, 6030a, agilent&lt;/div&gt;
</description></item></channel></rss>