Phoenix Contact
  • Products
  • Manufacturers
  • Phoenix Contact
  • More
  • Cancel
Phoenix Contact
Blog Is there a place for Raspberry Pi and other single board computers within the industrial market place?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Phoenix Contact to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: garynelson
  • Date Created: 6 Apr 2020 1:15 PM Date Created
  • Views 2633 views
  • Likes 8 likes
  • Comments 6 comments
  • phoenix contact
Related
Recommended

Is there a place for Raspberry Pi and other single board computers within the industrial market place?

garynelson
garynelson
6 Apr 2020

 

The Raspberry Pi single board computer, and in particular models 3B and the new 3B+ model, has found itself being considered by design engineers as a viable solution for industrial applications. With the Bluetooth and wireless capabilities of this innovative small form factor computer system the Raspberry Pi lends itself perfectly to be used in remote monitoring applications on the factory floor. The ability to send data to a cloud based server remotely giving the status of any machine in real time is an increasingly important solution in helping prevent potentially costly machine down times.

 

One of the challenges faced by design engineers using single board computers is how to package the product in order to suit the working environment it will face when it’s finally finished and released. The decisions around what interfaces the product will need to have users interacting with also has to be considered especially when deciding upon the physical size of the end product. With the advancement in technology and the birth of Industrie 4.0 the product ultimately designed may need to have a smaller form factor than has been traditionally used and space will therefore be at a premium. One additional consideration is where the unit is to be mounted i.e. on the din rail within a cabinet, as a stand-alone unit or perhaps even wall mounted. All of these decisions made by a design engineer can ultimately mean that the only way of housing the product is with a bespoke enclosure solution which can be costly and add long lead-times to receive the first off samples.

 

When designing electronic devices around the Raspberry Pi the choice of available enclosures can be overwhelming especially for non-industrial applications. If you are developing home based media servers or a small scale router you are ideally looking for something aesthetically pleasing as well as functional.

 

At Phoenix Contact we offer a number of innovative enclosure solutions based on the standard form factors of embedded system printed circuit boards (PCB’s) and have some specifically designed to accommodate the Raspberry Pi. If you require Din rail, wall or even table top mounting we have flexible solutions to meet your needs. Our universal case system (UCS) has the additional flexibility of removable flat side walls for any customisation requirements you may have and is available in 4 sizes, 2 heights and 2 colours as standard.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
image

  • Sign in to reply

Top Comments

  • garynelson
    garynelson over 6 years ago in reply to shabaz +4
    Hi Shabaz, Thanks for sharing your design I always enjoy seeing how people have used our products in their projects and designs as they are always so varied! I'm pleased you were happy with the RPI-BC…
  • shabaz
    shabaz over 6 years ago +3
    Hi Gary, I used the RPI-BC enclosure with Pi 4 for this open hardware project called VIKI: The RPI-BC is very good, but with the slight limitation was that it was quite small, and the cut-outs were only…
  • shabaz
    shabaz over 6 years ago +3
    For anyone interested in seeing the RPI-BC enclosure in bits, this is what comes in the RPI-BC kit RPI-BC kit (spares and accessories are orderable separately too): The black pieces are PCB supports that…
Parents
  • garynelson
    garynelson over 6 years ago

    Hi Allen,

    We have worked with a number of industrial customers who were using the off the shelf Raspberry Pi 3B & 3B+ for their designs and needed an enclosure that sits on a DIN rail with easy access to the ports. The designs have ranged from reporting modules along a production line sending status reports via blue-tooth to a cloud based server, to industrial I/O modules. Our RPI-BC enclosure was the first version released that is purely based on a DIN rail and we have sold 10's of 1000's of them to industrial customers since it's launch. The latest enclosure system we have is our UCS-RPI which is being used by customers designing 4G routers and controllers for lights amongst other things.

     

    I wrote the piece as the evidence we have so far seen is that the Raspberry Pi single board computers have a very strong opportunity in the industrial marketplace without the need for modification in most instances. You'll find the ranges I've mentioned in stock at Farnell and they have been very successful in the sale of the units since adding them to their portfolios.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • garynelson
    garynelson over 6 years ago

    Hi Allen,

    We have worked with a number of industrial customers who were using the off the shelf Raspberry Pi 3B & 3B+ for their designs and needed an enclosure that sits on a DIN rail with easy access to the ports. The designs have ranged from reporting modules along a production line sending status reports via blue-tooth to a cloud based server, to industrial I/O modules. Our RPI-BC enclosure was the first version released that is purely based on a DIN rail and we have sold 10's of 1000's of them to industrial customers since it's launch. The latest enclosure system we have is our UCS-RPI which is being used by customers designing 4G routers and controllers for lights amongst other things.

     

    I wrote the piece as the evidence we have so far seen is that the Raspberry Pi single board computers have a very strong opportunity in the industrial marketplace without the need for modification in most instances. You'll find the ranges I've mentioned in stock at Farnell and they have been very successful in the sale of the units since adding them to their portfolios.