Würth Elektronik
  • Products
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog ANP098: Effect of layout, vias and design on the blocking quality of filter capacitors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Würth Elektronik
  • Date Created: 23 May 2022 6:39 AM Date Created
  • Views 1461 views
  • Likes 6 likes
  • Comments 0 comments
  • mlcc
  • layout
  • wurth_electronics
  • filter capacitors
  • würth elektronik
  • Design
  • application_note
Related
Recommended

ANP098: Effect of layout, vias and design on the blocking quality of filter capacitors

Würth Elektronik
Würth Elektronik
23 May 2022
ANP098: Effect of layout, vias and design on the blocking quality of filter capacitors

Application Noteimage

Effect of layout, vias and design on the blocking quality of filter capacitors

ANP098 BY ANDREAS NADLER

01. INTRODUCTION

In the general technical literature much can be found about correct PCB layout techniques, multi-stage filters and blocking capacitors for supply pins of digital ICs. However, real measurements or practical simulations are often missing. The goal of this Application Note is to show the influence of design, the number of ground vias and the placement of the MLCC filter components to each other. Furthermore, it will be shown that an unfortunate dimensioning of capacitor banks can cause more problems than initially expected. Blocking capacitors at supply pins have the task to close the clocked current loop of the digital circuits locally in the shortest way with the help of a low impedance. This reduces the radiated magnetic field strength and the RF interference currents coupled into the supply voltage level as much as possible. If the capacitors are optimally selected with regard to their impedance curve and geometrically optimally placed at the VCC pins, then the clocked RF current can be blocked in the best possible way. To demonstrate the various influences in practice, the insertion loss S21 was determined over a wide frequency range from 300 kHz to 3 GHz using a 4-layer PCB designed for exactly 50 Ω impedance. In addition, two supporting simulations were created using the freeware LTspice and the professional tool EMCoS. This was to determine how close one can get to the real measurement using E5071C (ENA RF Network Analyzer) and what influence the via positioning has relative to each other. The MMCX connector types of Würth Elektronik eiCan were selected as RF connectors.

image

Figure 1: 3D view of the demo board with the different 50 Ω measurement channels. The top two channels are used to calibrate the measurement setup

02. CIRCUIT DIAGRAM AND MEASUREMENT SETUP

The demo board in Fig.1 has 6 measuring channels. The schematic of the demo board is shown in figure 2. The measurement setup with the network analyzer is shown in figure 3. The top two are for calibration of the measurement setup. The third channel is for measuring the oscillation which occurs when several MLCCs are connected in parallel. In addition, it is to be compared to what extent class 1 NP0/C0G differs from class 2 X5R/X7R ceramics with otherwise identical component values. In the remaining 5 channels always the same 0603 HF SMD ferrite 742863122 and two 100 nF X7R MLCCs each are used. However, differences can be found in the number of GND vias, the design and in the geometrical arrangement of the MLCCs.

image

Figure 2: Altium circuit diagram of the demo board with the different 50 Ω measuring channels (without calibration channels)

Basically, the higher and more broadband the insertion loss S21 is, the better the effect of the entire filter and/or the individual blocking capacitor. Since the same ferrite and two 100 nF MLCCs are placed everywhere in all 6 measurement channels, the insertion loss in the measurements depends on:

  1. Design of the MLCCs (especially their ESL)
  2. Number of vias to GND (more vias = lower parasitic inductance to GND)
  3. Arrangement of MLCCs to ferrite (parasitic inductive & capacitive coupling)
  4. Length of the traces to the MLCC pads (adds up to the ESL of the MLCC)

image

Figure 3: Measurement setup with E5071C (ENA RF Network Analyzer) and MMCX RF connectors

03. LAYOUT IN DETAIL

In advance, the smallest MLCC designs, 0403, with 3 vias per GND pad, are expected to give the best result because their equivalent series inductance (ESL) is the smallest (Fig. 4).

image

Figure 4: Measuring channel with 0403 MLCC and 3 vias each at the GND pad

The largest MLCC designs, 0805 with only one via per GND pad are expected to have significantly worse insertion loss above the resonant frequency (Fig. 5).

image

Figure 5: Measuring channel with 0805 MLCC and 1 via each at the GND pad

The worst result is expected from the measurement channel with the 0805 MLCCs in combination with the poor layout (Fig. 6). Here, only a single GND via was used for both MLCCs GND pads. In addition, the MLCCs are arranged in parallel with the ferrite, resulting in parasitic inductive and capacitive couplings. Furthermore, the trace connections of the MLCC pads are unnecessarily long. 1-2 mm in length corresponds to approximately 0.5 nH of additional ESL. Fig. 7 illustrates the parasitic impedances caused by the design and layout.

image

Figure 6: Measuring channel with 0805 MLCC, only 1 via for both GND pads, unnecessary stubs and geometrically unfavorable arrangement compared to the ferrite

image

Figure 7: Parasitic inductances and capacitances of the poor layout, which reduce the insertion loss of the filter

For the measurement channels with the capacitors of the 0603 types, results are expected which lie between the 0402 and 0805 types.

In addition, a measurement channel was designed to investigate the effects of several MLCC capacitors of class 1 ceramic (NP0/C0G) with different capacitances connected in parallel. In this comparison, one 100 pF, one 1 nF and one 4.7 nF were selected. Since these are particularly high Q capacitors, where the dielectric is titanium oxide, unfavorable resonances between the various capacitive and inductive elements of the capacitors are expected. These resonances would greatly reduce the insertion loss S21 in certain frequency ranges. Furthermore, the same experiment was performed with MLCCs with class 2 ceramics (X7R). X7R ceramic is made of barium titanate. Since this ceramic is more lossy than class 1 ceramics, and thus has a slightly lower Q, i.e., a larger loss angle tan, a less pronounced resonance amplitude is expected. The layout is shown in Fig. 8.

image

Figure 8: Measuring channel with 3 different capacitance values, but the same dielectric. The fourth MLCC between the labels, was not populated during the tests

04. LT SPICE & EMCOS SIMULATION

Würth Elektronik has been providing a wide range of suitable LT Spice models for most of the passive components for many years. These can be easily downloaded from the WE website at any time. If the vias and their parasitic properties are added to the models in LTspice, the waveforms of the real S21 measurement can be reproduced relatively accurately (Fig. 11). However, this only affects the relative and not the absolute insertion loss. The parasitic inductance and parallel capacitance of the vias depends on their length and inner diameter. In addition, the vias also influence each other by a mutual inductance, which mainly depends on the distance between the vias. The further the vias with the same electrical potential are away from each other, the smaller is their mutual inductance and thus also the total inductance.

A supporting simulation was also performed using the EMCoS software, which is available for a fee. Among other things, this software must be fed with the exact PCB raw data from the CAD (e.g. Altium). With the help of the EMCoS software, the effect of different positioning of the 3 GND vias was investigated. In theory, vias with the same electrical potential are expected to form a mutual mutual inductance and thus the total inductance increases the closer they are placed to each other. If the vias are placed at a 90° angle around the GND pad of the MLCCs, they can be connected close to the pad and still result in a large distance between the 3 vias.

image

Figure 9: Possible variants of the GND via positioning. Shown in red is the mutual influence due to the mutual inductance. The further away the vias with the same electrical potential are, the smaller the mutual inductance.

05. SIMULATIONS- & MEASUREMENT RESULTS

image

Figure 10: Circuit diagram LT Spice simulation. The vias were modeled using inductances and capacitances

image

Figure 11: LT Spice Simulation result insertion loss S21

image

Figure 12: Measurement results for insertion loss S21 with E5071C (ENA RF Network Analyzer)

As expected, the smallest layout (0402) in combination with several vias per GND pad provides the best result due to the smallest ESL. The insertion loss of the bad layout example turns out to be blatantly worse than the rest. Depending on the measurement point, there is a difference of more than 40 dB to the next best channel. If the basic layout rules such as 90° arrangement of MLCCs to ferrite and short pad connection to vias as well as traces are observed, a broadband filter can be successfully designed. The differences in the insertion loss are then only maximum 10 dB depending on the design and via count.

The relatively simple LT Spice simulation can also nicely represent the basic properties of the different measurement channels, although not 100%. The many parasitic properties of the connectors, PCB etc. cannot be easily represented in LTspice.

image

Figure 13: Comparison measurement of insertion loss of capacitor groups with class 1(NP0/C0G blue) and class 2 (X5R/X7R red) ceramics with E5071C (ENA RF Network Analyzer)

The comparison measurement of the three MLCCs in NP0 and X7R also shows the difference in quality in a practical way. Although the NP0s achieve better values in the insertion loss at the individual resonant frequencies, the amplitude deflections are also higher in negative form. The NP0 MLCCs generate an LC resonant circuit with higher Q, which in certain frequency regions brings with it the danger of an unwanted amplification of interference components.

image

Figure 14: EMCoS simulation of the 0403 measurement channel with different positions of the GND vias. The 90° arrangement around the pad results in up to 4 dB more attenuation in this case than if the vias are very close to each other. If the vias are placed in a row with 0.5 mm spacing, then the insertion loss curve is approximately in between

06. SUMMARY

From the differences shown, it can be seen that this PI filter can only work optimally if the textbook layout rules are followed. There are differences of over 40 dB, depending on the frequency in the insertion loss, which in practice can mean the difference between success and failure in the EMC measurement. What has not been considered in this application note is the voltage dependence of the class 2 MLCCs and the DC current dependence of the chip bead ferrite. These influencing factors mean further differences in insertion loss in practice. If one wants to successfully block supply pins on digital ICs, it is recommended to use several vias per GND pad on the capacitors. In addition, it has been shown that very short stubs to the capacitors and a geometrically unfavorable arrangement also significantly worsen the blocking quality. The ferrite and the capacitors should be arranged at 90° to each other to avoid unwanted coupling. With the help of the EMCoS simulation it was shown that GND vias should be placed as far away from each other as possible but always close to the MLCC pad. This way a few dB attenuation can be achieved in the higher frequency range. The best result was achieved by placing the vias 90° around the GND pad and with a small distance (max. 0.3 mm) to the pad.

The broadband insertion loss without undesired oscillations also shows the enormous advantages of chip bead ferrites over pure capacitor groups. If one nevertheless wants to connect several capacitors in a group, this group should contain a class 2 capacitor (ceramic e.g. X7R) in order to limit the resulting oscillations in amplitude. However, a sufficiently high insertion loss can only be achieved with an additional chip bead ferrite.

A Appendix

A.1 Formulas

Calculation of parasitic inductance and capacitance of a via.

image

kL = 0.2 nH/mm PCB inductance per unit length

kC = 0.056 pF/mm PCB capacitance per unit length

h = length of the via

d = Via inner diameter

d1 = Via pad outer diameter

d2 = Via clearance diameter on internal layers

image

A.2 BOM

image

Importante Notice

The Application Note is based on our knowledge and experience of typical requirements concerning these areas. It serves as general guidance and should not be construed as a commitment for the suitability for customer applications by Würth Elektronik eiSos GmbH & Co. KG. The information in the Application Note is subject to change without notice. This document and parts thereof must not be reproduced or copied without written permission, and contents thereof must not be imparted to a third party nor be used for any unauthorized purpose. Würth Elektronik eiSos GmbH & Co. KG and its subsidiaries and affiliates (WE) are not liable for application assistance of any kind. Customers may use WE’s assistance and product recommendations for their applications and design. The responsibility for the applicability and use of WE Products in a particular customer design is always solely within the authority of the customer. Due to this fact it is up to the customer to evaluate and investigate, where appropriate, and decide whether the device with the specific product characteristics described in the product specification is valid and suitable for the respective customer application or not. The technical specifications are stated in the current data sheet of the products. Therefore the customers shall use the data sheets and are cautioned to verify that data sheets are current. The current data sheets can be downloaded at www.we-online.com. Customers shall strictly observe any product-specific notes, cautions and warnings. WE reserves the right to make corrections, modifications, enhancements, improvements, and other changes to its products and services. WE DOES NOT WARRANT OR REPRESENT THAT ANY LICENSE, EITHER EXPRESS OR IMPLIED, IS GRANTED UNDER ANY PATENT RIGHT, COPYRIGHT, MASK WORK RIGHT, OR OTHER INTELLECTUAL PROPERTY RIGHT RELATING TO ANY COMBINATION, MACHINE, OR PROCESS IN WHICH WE PRODUCTS OR SERVICES ARE USED. INFORMATION PUBLISHED BY WE REGARDING THIRD-PARTY PRODUCTS OR SERVICES DOES NOT CONSTITUTE A LICENSE FROM WE TO USE SUCH PRODUCTS OR SERVICES OR A WARRANTY OR ENDORSEMENT THEREOF. WE products are not authorized for use in safety-critical applications, or where a failure of the product is reasonably expected to cause severe personal injury or death. Moreover, WE products are neither designed nor intended for use in areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc. Customers shall inform WE about the intent of such usage before design-in stage. In certain customer applications requiring a very high level of safety and in which the malfunction or failure of an electronic component could endanger human life or health, customers must ensure that they have all necessary expertise in the safety and regulatory ramifications of their applications. Customers acknowledge and agree that they are solely responsible for all legal, regulatory and safety-related requirements concerning their products and any use of WE products in such safety-critical applications, notwithstanding any applications-related information or support that may be provided by WE. CUSTOMERS SHALL INDEMNIFY WE AGAINST ANY DAMAGES ARISING OUT OF THE USE OF WE PRODUCTS IN SUCH SAFETYCRITICAL APPLICATIONS.

  

DIRECT LINK

ANP098: Effect of layout, vias and design on the blocking quality of filter capacitors

 

USEFUL LINKS:

Application Notes : https://we-online.com/en/support/knowledge/application-notes

Services: https://we-online.com/en/products/components/service

Contact : https://we-online.com/en/support/contact

 

CONTACT INFORMATION

Würth Elektronik eiSos GmbH & Co. KG

Max-Eyth-Str. 1, 74638 Waldenburg, Germany

Tel.: +49 (0) 7942 / 945 – 0

Email: appnotes@we-online.de

Web: https://www.we-online.com