Würth Elektronik
  • Products
  • Manufacturers
  • Würth Elektronik
  • More
  • Cancel
Würth Elektronik
Blog Challenges and advantages of high-bandwidth uncompressed video connectivity for medical diagnostic equipment
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Würth Elektronik to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Würth Elektronik
  • Date Created: 15 Apr 2024 1:09 PM Date Created
  • Views 628 views
  • Likes 5 likes
  • Comments 1 comment
  • würth elektronik
  • featured article
  • wurth_elektronik
Related
Recommended

Challenges and advantages of high-bandwidth uncompressed video connectivity for medical diagnostic equipment

Würth Elektronik
Würth Elektronik
15 Apr 2024
Challenges and advantages of high-bandwidth uncompressed video connectivity for medical diagnostic equipment

Application Noteimage

Challenges and advantages of high-bandwidth uncompressed video connectivity for medical diagnostic equipment

FA002 by Walter Fusto, Gavin Lei, Just Tang and Carlos Guo

in cooperation with  image

VALENS SEMICONDUCTOR | www.valens.com | investors@valens.com

The technological overhaul taking place in hospitals and medical centers is undoubtedly improving medical procedures. Doctors and health professionals benefit from operating with the highest possible video image quality for the most accurate representation of patients’ conditions. With the advent of medical-grade visualization systems, procedural workflows improve, and high-quality, zero latency uncompressed video images are transmitted over longdistances for better collaboration, education and monitoring. This paper introduces high-bandwidth uncompressed video connectivity for medical diagnostic equipment based on Valens' chipset VS3000 HDBaseT reference design solution, developed in collaboration with Würth Elektronik passive components.

01. BASIC REQUIREMENTS FOR A VISUAL MEDICAL DIAGNOSTIC SYSTEM

The advanced medical imaging systems demand highbandwidth connectivity and increased video performance, thus introducing new requirements in the operating room, including: 

  • Color accuracy with high-dynamic range (HDR)
  • High-quality imaging - uncompressed video
  • Real-time, zero latency video distribution
  • Long-distance transmission
  • Flexible and efficient infrastructure
  • Range of supported interfaces
  • Cross-vendor interoperability

HDBaseT enables high-bandwidth, long-distance, highquality video images to be transmitted in real time over a single cable, while supporting interoperability between different devices, thus enabling a visual medical diagnostic system connected inside and outside the operating room.

02. WHAT IS HDBASET?

HDBaseT is a global standard that allows for the convergence and distribution of the 5Play feature set –audio, video, Ethernet, controls, USB 2.0 and up to 100 W of power– over a single LAN cable (Cat 6 or above), for up to 100 m and even up to 1000 m over optical fiber.

03. WHAT ARE THE BENEFITS OF HDBASET FOR MEDICAL APPLICATIONS?

Real-time transmission During surgical procedures, accurate and real-time video images are critical, and HDBaseT delivers uncompressed UHD video, enabling the best possible quality image with virtually no latency since it does not compress the data.

image

Figure 1:  Diagram of the HDBaseT scheme

Superior performance

When using diagnostic imaging systems such as MRIs, displaying X-rays, or conducting endoscopic procedures, medical professionals depend on high-resolution and color accuracy, with no loss of visual information. HDBaseT provides an advanced connectivity solution that meets the high demands of medical visualization systems and enables bit exact transmission of high bandwidth data.

One Cable Solution

With the proliferation of advanced digital video imaging, more devices and cabling must fit into small and crowded procedure rooms. HDBaseT can improve workflow efficiency by reducing cables and connectors, facilitating sterilization methods and increasing flexibility of equipment location.

04. EVALUATION KIT OF HDBASET IC FOR MEDICAL GRADE APPLICATIONS

The Valens Semiconductor's VS3000 integrated circuit leverages the HDBaseT Spec 3.0 standard technology and it features HDBaseT port duality, where the same chipset can be configured to operate as either a TX (transmitter) device on the video source side, or an RX (receiver) device on the video receive side. The same design of TX and RX devices brings considerable cost savings for manufacturers. In order to evaluate the characteristics of the VS3000 chip family, Valens Semiconductor has realized an evaluation kit that demonstrates the implementation of the devices’ feature set over a single CAT6a cable. The data transfer between the HDBaseT TX or RX and the peripheral device is shown in Figure 3.

To achieve a connection with a network cable that satisfies both the high speed signal output and the electrical isolation between the source and the receiver, a signal transformer is required. The design of the above mentioned transformer can be challenging because of the requirements given from the medical applications. First of all, to ensure long-distance signal transmission, CAT6 and above are recommended for the network cables.

image

Figure 2: Schematic diagram of the medical visualization and diagnosis system

image

Figure 3: HDBaseT and peripheral interface communication schematic

A withstand voltage of 4000 Vrms / 1 min is required to meet IEC 60601, technical standard for the safety and essential performance of medical electrical equipment. Thus, the HDBaseT connection is made with a 4-channel HDBaseT front-end, routed to a CAT6A RJ45 connector through the Würth Elektronik WE-LAN HDBaseT Transformer–749054010; a 10 G Base-T PoE transformer with 4 pairs, up to 150 W power capability and 4 kV isolation voltage, specifically verified for the VS3000 interface. The isolation requirements, as well as the normal operating voltage requirements of 250 Vrms, are met with specific design of the electrical spacing: the creepage distance is 8 mm and the electrical clearance is 5 mm. Furthermore, the transformer windings are realized with reinforced insulation (Figure 4).

The VS3-EVK implements the HDBaseT Power over HDBaseT (PoH). Per PoH, one side is the power supplier PSE (Power Source Element) and the other side (Remote side) accepts the power delivered, also called PD (Powered Device). On the able side of the HDBaseT transformer, the center taps are connected to the PoH PD Controller. Long distance, high speed transmission, PoH power supply may bring EMC issues. It can be shown how the signal transformer addresses isolation, insertion loss and return loss requirements of HDBaseT applications without decreasing the system performance.

Circuit considerations in an HDBaseT application Since the data rate is 16 Gbps and the connection is PoH, the power path has to go through the center tap of the signal transformer, creating common mode noise propagation in the data transmission. Typically, the clock source of the IC also generates noise at its frequency and its multipliers (Figure 5). To overcome these issues, common mode chokes are integrated in the signal transformer, as shown in Figure 6, with different common mode rejection ratios at the different frequencies.

image

Figure 4: Details of insulation strengthening measures

image

Figure 5: Typical network line radiation problem caused by 125 M clock and multiplier

Improved rejection of common mode noise by adding built-in common mode chokes on the PHY side of the network transformer can be seen in Figure 7.

By adding common mode chokes to the transformer, the network cable radiation is effectively suppressed. Noise problems can arise also from PoH transmission. A flyback transformer, MID-FLYTI-750312791 is used to provide power to the PD, capable of stepping up the input voltage to 56 V. Noise generated by isolated power supplies, which may cause conduction and radiation problems, require additional common mode chokes (Figure 8) close to the power supply to filter this type of noise. Chokes like the WE-SL5 and SL5 HC series for PoE power supply filtering achieve high common mode impedance over a wide frequency band (in this evaluation kit, WE-SL5 HC – 744273102 have been selected). The transformers do not provide protection against ESD or surge impulses. Since these voltages are associated with rapid current increases, they can couple onto the transformer from the cable side to the VS3000 chip and damage it. It is therefore recommended to connect each signal line between the transformer and PHY chip to a TVS diode, as highlighted in Figure 9.

The TVS needs to be placed between the VS3000 and the network transformer, as close to the network transformer as possible, to provide the first protection in case ESD noise enters the system. The TVS is connected between the signal line and ground, to the reference ground of the VS3000 and the original side of the network transformer, not to earth PE. The board from the reference design EVS3-EVK2-KT-3000- MD is shown in Figure 10.

image

Figure 6: Schematic of adding common mode inductor on the PHY side

image

Figure7:  Diagram of the effect after adding common mode inductor

image

Figure 8: Schematic of adding common mode chokes at PoH power supply output

image

Figure 9: Schematic of adding TVS on the PHY side of the network transformer

image

Figure 10:  Valens EVS3-EVK2-KT-3000-MD Evaluation Kit for Medical application

05. CONCLUSION

HDBaseT provides an elegant solution to several requirements in the medical sector and it has the ability to converge multiple peripheral interfaces into one interface and achieve long-distance bit exact, zero latency transmission of high bandwidth signals through a single network cable, saving cabling space in the operating room and outside, while ensuring compatibility between different devices. The Valens VS3000 chip represents an ideal device to optimize connectivity for audio/video transmission. To ensure the connections high level of performance according to the HDBaseT specification it is recommended to follow the chip manufactures reference design that uses high quality electronic and electromechanical companion components that support the Valens chipset on the board. For this purpose, the HDBaseT signal transformer is designed from Würth Elektronik to meet medical grade voltage withstand requirements, ensuring high quality signal transmission in terms of EMC performance, as well as the filter components that provide the finest solution to meet the requirements of the medical applications.

IMPORTANT NOTICE

The Application Note is based on our knowledge and experience of typical requirements concerning these areas. It serves as general guidance and should not be construed as a commitment for the suitability for customer applications by Würth Elektronik eiSos GmbH & Co. KG. The information in the Application Note is subject to change without notice. This document and parts thereof must not be reproduced or copied without written permission, and contents thereof must not be imparted to a third party nor be used for any unauthorized purpose. Würth Elektronik eiSos GmbH & Co. KG and its subsidiaries and affiliates (WE) are not liable for application assistance of any kind. Customers may use WE’s assistance and product recommendations for their applications and design. The responsibility for the applicability and use of WE Products in a particular customer design is always solely within the authority of the customer. Due to this fact it is up to the customer to evaluate and investigate, where appropriate, and decide whether the device with the specific product characteristics described in the product specification is valid and suitable for the respective customer application or not. The technical specifications are stated in the current data sheet of the products. Therefore the customers shall use the data sheets and are cautioned to verify that data sheets are current. The current data sheets can be downloaded at www.we-online.com. Customers shall strictly observe any product-specific notes, cautions and warnings. WE reserves the right to make corrections, modifications, enhancements, improvements, and other changes to its products and services. WE DOES NOT WARRANT OR REPRESENT THAT ANY LICENSE, EITHER EXPRESS OR IMPLIED, IS GRANTED UNDER ANY PATENT RIGHT, COPYRIGHT, MASK WORK RIGHT, OR OTHER INTELLECTUAL PROPERTY RIGHT RELATING TO ANY COMBINATION, MACHINE, OR PROCESS IN WHICH WE PRODUCTS OR SERVICES ARE USED. INFORMATION PUBLISHED BY WE REGARDING THIRD-PARTY PRODUCTS OR SERVICES DOES NOT CONSTITUTE A LICENSE FROM WE TO USE SUCH PRODUCTS OR SERVICES OR A WARRANTY OR ENDORSEMENT THEREOF. WE products are not authorized for use in safety-critical applications, or where a failure of the product is reasonably expected to cause severe personal injury or death. Moreover, WE products are neither designed nor intended for use in areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc. Customers shall inform WE about the intent of such usage before design-in stage. In certain customer applications requiring a very high level of safety and in which the malfunction or failure of an electronic component could endanger human life or health, customers must ensure that they have all necessary expertise in the safety and regulatory ramifications of their applications. Customers acknowledge and agree that they are solely responsible for all legal, regulatory and safety-related requirements concerning their products and any use of WE products in such safety-critical applications, notwithstanding any applications-related information or support that may be provided by WE. CUSTOMERS SHALL INDEMNIFY WE AGAINST ANY DAMAGES ARISING OUT OF THE USE OF WE PRODUCTS IN SUCH SAFETYCRITICAL APPLICATIONS.

DIRECT LINK

FA002 | Challenges and advantages of high-bandwidth uncompressed video connectivity for medical diagnostic equipment

USEFUL LINKS:

Application Notes : https://we-online.com/en/support/knowledge/application-notes

Services: https://we-online.com/en/products/components/service

Contact : https://we-online.com/en/support/contact

 

CONTACT INFORMATION

Würth Elektronik eiSos GmbH & Co. KG

Max-Eyth-Str. 1, 74638 Waldenburg, Germany

Tel.: +49 (0) 7942 / 945 – 0

Email: appnotes@we-online.de

Web: https://www.we-online.com

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    Nice to know they are keeping my medical imaging free of outside interference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 2 years ago

    Nice to know they are keeping my medical imaging free of outside interference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
No Data