Proprietary
Introduction
Proprietary Radio Stack
All Wireless Connectivity RF Modules have the WE-ProWare pre-loaded
Our module added value is the WE-ProWare operating system which is fully included. Communication functions are configured with simple AT commands. You can easily swap between radio channels and protocols. All this makes it very easy to enter new markets with your application.
Proprietary Radio as Bluetooth® LE Alternative

- Connection only with authorized devices by the manufacturer
- Security aspect as argument for the endcustomers
- Closed communication is „invisible“ for Smart devices
- Higher throughput possible – no effort with big overhead of Bluetooth®
- Saving Bluetooth® Listing costs
- Business model to build the whole chain as user experience
- Binding the end customer to the product with additional accessory with the same communication

Radio Frequency Spectrum
The radio frequency spectrum is regulated by designated regulatory nauthorities that define how specific spectrum bands can be used. The ISM (Industrial, Scientific and Medical) and SRD (Short Range Device) bands are free to use without license costs. As there is no single worldwide regulation, national authorities define which of the frequency bands are open for access in each specific country.
Furthermore in ISM bands regulation there is no directive about a specific radio protocol. That means, it doesn’t matter if a proprietary radio protocol or standard radio protocols will be chosen. Everybody can use individual firmware within the regulations of the frequency bands (output power, duty cycle, …). The correlation between data rate, range and battery life could be arranged individually.
Advantages
- Security due to closed system
- More flexibility compared to standard
- More scope for design
- No dependences
- No umbrella organization
- No license fees
Short Range Device (SRD)
Short Range Devices (SRD) are radio devices that offer a low risk of interference with other radio services, usually
because their transmitted power, and hence their range, is low., typically few hundred meters. SRD often benefit from
a relaxed regulaltory regime compared with other radio communication equipment. The use is lecence free in general.
However the radio regulations have to be considered, as the Radio Equipment Directive in Europe.

Areas of Application

NETWORK TOPOLOGIES
Point to point

Point to point topology is the type of network topology which is used to connect to network nodes directly with each other through some link. In between these two nodes, the data is transmitted using this link.
Star

In a star topology all nodes are connected via a central station. All communication is only possible via the central node
Peer to Peer

In peer to peer topology every node has a direct connection to the other nodes and can communicate to each other.
Flooding Mesh

In a flooding mesh topology an indirect communication between nodes is possible. The message will be repeated until it reaches the receiver.
If you want to read more find here the whole Product Guide.

-
DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
nwieland
in reply to DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
nwieland
in reply to DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children