<?xml version="1.0" encoding="UTF-8" ?>
<?xml-stylesheet type="text/xsl" href="https://community.element14.com/cfs-file/__key/system/syndication/rss.xsl" media="screen"?><rss version="2.0" xmlns:dc="http://purl.org/dc/elements/1.1/"><channel><title>Electromechanics - Basic Principles</title><link>https://community.element14.com/products/manufacturers/wuerth-elektronik/w/documents/10958/electromechanics---basic-principles</link><description /><dc:language>en-US</dc:language><generator>Telligent Community 12</generator><item><title>Electromechanics - Basic Principles</title><link>https://community.element14.com/products/manufacturers/wuerth-elektronik/w/documents/10958/electromechanics---basic-principles</link><pubDate>Fri, 08 Oct 2021 05:27:27 GMT</pubDate><guid isPermaLink="false">93d5dcb4-84c2-446f-b2cb-99731719e767:6aa3ef79-1dc5-44b3-8671-319504622007</guid><dc:creator>sleuz</dc:creator><comments>https://community.element14.com/products/manufacturers/wuerth-elektronik/w/documents/10958/electromechanics---basic-principles#comments</comments><description>Current Revision posted to Documents by sleuz on 10/8/2021 5:27:27 AM&lt;br /&gt;
&lt;p style="margin:0;"&gt;&lt;span style="font-size:18pt;"&gt;Basic Principles of Electromechanics&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;[...] In overall, plating the entire contact surface is plated with a single material; tin finishes are often overall plated. In selective plating, the plating is applied only to defined functional areas of the contact; gold plating is generally done selectively, with the gold applied only at the portion of the plug and receptacle contacts that define the mating interface. In duplex plating, different platings are applied at the separable connection and termination portions of the contact. The most common duplex plating is tin at the termination end, for soldering, and gold over nickel at the separable connection end. Electroplating and selective/duplex plating practices are highly proprietary and only a general description will be provided in this discussion.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;&lt;strong&gt;1.4.1.1 Electroplating Basics&lt;/strong&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;Electroplating, or electrodeposition, in connector technology refers to the plating of a material, selected for the properties discussed in Chapter I/1.2.3 Contact Finishes, onto a contact spring material, selected for the mechanical and electrical properties discussed in Chapter I/1.2.2 Contact Springs, to optimize the overall electrical performance of the plated contact system.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;&lt;br /&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span&gt;&lt;a href="https://community.element14.com/resized-image/__size/620x300/__key/communityserver-wikis-components-files/00-00-00-00-56/contentimage_5F00_21655.bmp"&gt;&lt;img alt="image" src="/cfs-file/__key/communityserver-wikis-components-files/00-00-00-00-56/contentimage_5F00_21655.bmp" style="max-height: 300px;max-width: 620px;" /&gt;&lt;/a&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;text-align:center;"&gt;&lt;span style="font-size:10pt;"&gt;&lt;em&gt;Fig. 1.20: Plating principle&lt;/em&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;Figure 1.20 schematically illustrates a simple electrochemical plating system. The “electro” part of the system includes the voltage/current source and the electrodes, anode and cathode, immersed in the “chemical” part of the system, the electrolyte or plating bath, with the circuit being completed by the flow of ions from the plating bath to the electrodes. The metal to be deposited may be the anode and be ionized and goes into solution in the electrolyte, or comes from the composition of the plating bath. Copper, tin, silver and nickel metal usually comes from anodes, while gold salts are usually added to the plating bath in a controlled process to maintain the composition of the bath. The plating bath generally contains other ions to facilitate current flow between the electrodes. The deposition of metal takes place at the cathode.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;&lt;br /&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;The overall plating process occurs in the following sequence:&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;&lt;br /&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;1. Power supply pumps electrons into the cathode.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;2. An electron from the cathode transfers to a positively charged metal ion in the &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;solution &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;and the reduced metal plates onto the cathode.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;3. Ionic conduction through the plating bath completes the circuit to the anode.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;4. At the anode two different processes take place depending on whether the anode &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;material is soluble, the source of the metal to be plated, or insoluble, inert. If the anode &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;material is soluble, a metal atom gives up an electron and goes into the solution &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;as a positively charged metal ion replenishing the metal content of the plating &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;bath. &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;If the anode is inert a negatively charged ion from the plating bath gives up an &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;electron to the anode.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;5. The electron flows from the anode to the power supply completing the circuit.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;Note that the deposition of metal at the cathode requires an electron so the rate of deposition depends on the flow of electrons, that is, the current flowing from the rectifier. The thickness of the deposit, therefore, depends on the current and the length of time the current is applied. This relationship is a result of Faraday’s law which relates the weight of a substance produced by an anodic or cathodic electrode reaction during electrolysis as being directly proportional to the quantity of electricity passed through the cell.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;While Faraday’s law fixes the amount of metal deposited, the distribution of that metal is dependent on the distribution of the current. This fact allows for selective deposition of the metal, a process commonly used in connector contact electroplating. &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;Figure 1.21 schematically illustrates the relationship between current distribution and deposited metal thickness. The same amount of current flows in the two geometries so the total metal deposited is the same, but the distribution is very different. The anode and cathode geometries and spacings in connector electroplating practice are designed to &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;shape the current flow between the anode and cathode so as to control the deposition of the finish material, both thickness and distribution, onto the contact. This capability is critical to the successful implementation of selective and duplex plating processes. The sizes, shapes and distance between electrodes are among the proprietary processes of connector electroplating. Plating bath compositions and applied current practices may also be proprietary.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;&lt;br /&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span&gt;&lt;a href="https://community.element14.com/resized-image/__size/300x300/__key/communityserver-wikis-components-files/00-00-00-00-56/contentimage_5F00_21656.bmp"&gt;&lt;img loading="lazy" alt="image" src="/cfs-file/__key/communityserver-wikis-components-files/00-00-00-00-56/contentimage_5F00_21656.bmp" style="max-height: 300px;max-width: 300px;" /&gt;&lt;/a&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;text-align:center;"&gt;&lt;span style="font-size:10pt;"&gt;&lt;em&gt;Fig. 1.21: Current distribution – metal thickness&lt;/em&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;&lt;strong&gt;1.4.1.2 Reel-to-Reel Strip Plating&lt;/strong&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;The following discussion provides a basic overview of the stages of electrodeposition during a reel-to-reel strip plating process. The manufacturing processes leading to reels of stamped and formed contacts will be described in Chapter II. The function of each stage will be described, but the details of accomplishing the function are not included because, as noted previously, electroplating practices are highly proprietary.&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;Stage 0 – Incoming inspection:&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;"&gt;&lt;span style="font-size:12pt;"&gt;While inspection of the incoming reel is independent of the electroplating process, it is not overstating to say that the quality of the electroplate is controlled by the quality of the incoming reel. Successful electroplating requires a “clean” metal surface and &lt;/span&gt;&lt;span style="font-size:12pt;"&gt;[...]&lt;br /&gt;&lt;/span&gt;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;padding:0px;"&gt;&amp;nbsp;&lt;/p&gt;&lt;p style="margin:0;text-align:center;"&gt;&lt;span style="font-size:14pt;"&gt;Electromechanics - Basic Principles and Connector Design Explanations&lt;/span&gt;&lt;/p&gt;&lt;div style="clear:both;"&gt;&lt;/div&gt;

&lt;div style="font-size: 90%;"&gt;Tags: basic_principles, connector_design_explanations, connector_application, electromechanics, material_requirements, electromechanical&lt;/div&gt;
</description></item></channel></rss>