XP Power
  • Products
  • Manufacturers
  • XP Power
  • More
  • Cancel
XP Power
Forum LDU1416S1000 EMI Input Filter Component Selection
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join XP Power to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 5 subscribers
  • Views 1034 views
  • Users 0 members are here
Related

LDU1416S1000 EMI Input Filter Component Selection

jgroleau
jgroleau over 8 years ago

The  LDU1416S1000LDU1416S1000 LED Driver datasheet Identifies an input filter consisting of 2 capacitors in parallel and an inductor in series The datasheet specifies the values for the capacitors and inductor but not the max voltage for the caps or the max current for the inductor The capacitor voltage is easy I am having difficulty determining the max current for the 68uH inductor Any help would be appreciated

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 8 years ago +2 verified
    Jim, The input filtering is most likely used to suppress any back ripple from within the driver. The current could be in the order of 1.5 to 2.0 times the load load current. This device can drive up to…
  • genebren
    0 genebren over 8 years ago

    Jim,

     

    The input filtering is most likely used to suppress any back ripple from within the driver.  The current could be in the order of 1.5 to 2.0 times the load load current.  This device can drive up to 1.0 A, but depending on your loading it could be less.  This is just a ballpark figure based on similar devices.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jgroleau
    0 jgroleau over 8 years ago in reply to genebren

    Thanks for the input I am limiting the output current on the  LDU1416S1000LDU1416S1000 to 700MA with a voltage divider on the control pin The load is a single LED I have ordered a 1.4A inductor so that should do the trick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer