PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 21 Jan 2023 7:10 PM Date Created
  • Views 3639 views
  • Likes 12 likes
  • Comments 8 comments
  • kicad
  • footprint
  • pcb
  • amphenol
  • SF2921-61506
  • SF2921-61506-1S
Related
Recommended

Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads

Jan Cumps
Jan Cumps
21 Jan 2023
Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads

Part 2b of the exercise to create a custom footprint for the Amphenol /  SV Microwave SF2921-61506-1S   SMA coaxial connector. In the previous post created the initial footprint boundaries. Now: the rest.

image

Copper pour and the pads

I first drew a theoretical - good enough - outline on the silkscreen.

image

It will have to go later, because the whole area will become exposed copper plane. But for now, it's a good guideline for the other activities:

  • copper plane and solder mask clearance should at least cover this area
  • it shows the centre of poth drill holes, and for the centre pin

I then drew the 2 pours with a polygon:

image 

and SMD pads:

image

When you right - click a pad, select Edit as Graphical Shapes, then click again and end that mode, all copper that touches the pad becomes "pad". So I end with two copper polygons that have PAD number 1 and 2. I also put 2 keepout areas on the copper  layer:

image

On the front courtyard layer, I drew the real estate that should be respected (purple rectangle in the first image)

Mask clearance

I then put a filled polygon on the front mask, similar to the main copper pour outline. This allows the connector base to sit flush on the plane.

image

I added a little clearance on the side where the microstrip exits the connector. This as a hint for the PCB designer that the whole microstrip area should be maskless.

Drill holes

Easy. Because I had the centers on silkscreen , I just had to put pads on those locations. I removed their number, made the copper size 0 and the drill size the correct one for a 0-80 UNF-2B bolt: 

image

3/64, according to the internet, is a 0.05 inch hole.

image

That's it. The result is this:

On a PCB :

image

In 3D view (using the image I downloaded in the very first post):

image

image

Blog Index

  • Overview: Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector series
  • Amphenol / SV Microwave SF2921-61506-1S SMA coaxial connector: behavior under vibration
  • Create a custom footprint in KiCad 7 - 1: collect info and component details
  • Create a custom footprint in KiCad 7 - 2a: create the footprint for an SMA coax connector with the editor - initial outline
  • Create a custom footprint in KiCad 7 - 2b: create the footprint for an SMA coax connector with the editor - copper pour, solder mask clearance, holes, pads
  • Use a LibraryLoader Footprint in KiCad 7
  • Sign in to reply
Parents
  • scottiebabe
    scottiebabe over 3 years ago

    Soon enough your going to have your RF wizards hat! Interesting Pasternak at least provides a sample pcb footprint for use on top of 8mil (0.2mm) of rogers RO4003C

    Different connector but similar idea

    image

    https://www.pasternack.com/images/ProductPDF/PE45459.pdf 

    great work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to scottiebabe

    Soon enough your going to have your RF wizards hat!

    I should team up with my brother. He's a civil engineer with specialisation in high frequency and antennas.
    Just like me he sold his soul and is doing corporate software management :).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Such is life, currency is quite valuable!

     image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Such is life, currency is quite valuable!