PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs DC switching board
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: neuromodulator
  • Date Created: 2 Feb 2023 12:21 PM Date Created
  • Views 3765 views
  • Likes 16 likes
  • Comments 30 comments
Related
Recommended

DC switching board

neuromodulator
neuromodulator
2 Feb 2023

As owner of some DC test equipment and as a big fan of automated tests, I've needed more than once to be able to route the instrument channels to multiple paths. Doing this by hand is of course not convenient, so I looked for better ways to do it. One way would be to use a switching systems such as the Keithley DAQ6510, but this would be costly. On the inexpensive end I could have bought cheap relay board, but it would not integrate seamlessly to be controlled through the Keithley instruments. In-between these 2 price ends I could buy a Keithley 2000-SCAN board to plug it to the Keithley DMM6500 bay, but this would limit me only to the DMM.

This led me to design a board that I could control directly from my Keithley DMM6500 and 2450 SMU digital I/O ports. Later I thought that it would be even more flexible if I also supported other instruments, so I added other control interfaces such as USB, WIFI, 5V and 3V3 logic.

image

The board can be used in 2- and 4-wire modes and uses the following topology.

image

I used reed relays mainly because of their longer lifespan than electromechanical ones and better behavior than solid state ones. I made the switching tracks 0.5 mm wide with a clearance of of 1.4 mm so as to keep resistance low and enough clearance for higher voltage. I added an extra layer of isolation just to be safe that current would no take the "wrong" path. And for flexibility I designed it so that I could powered through USB, JTAG, or directly from the Keithley.

Here is a video that shows how the 2450 is powering it and controlling it to test different digits of a Nixie.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I've been thinking on releasing this to Crowdsupply. So I would like to get some feedback from the E14 community. Any comment is more than welcome.

2022-2-2 Update

I'll address some of the comments here to keep everything more organized (and also keep editability).

As Andrew J suggested, use cases are probably a good start, because it will allow me to guide the effort on implementing what actually would be useful to the final user.

Target use cases:

A) PCB testing (e.g., Proper operation of the PDN, power safety, detection of shorts or unsoldered joints, etc.)

B) Analog sensor measurements (e.g, temperature sensors, pressure sensors, vibration sensors, or any low frequency analog sensor)

C) Component characterization (e.g, electronic components in ambient conditions or in special conditions such as high temperature, where the same board be could used to measure the component properties and the conditions that affect the component)

Control use case:

A) The board is controlled through the USB virtual serial port using a Python program that controls the board through an arbitrary protocol.

B) The board is controlled through SCPI driver from LabVIEW, Python or any other software that supports SCPI. This could be done through the WIFI or virtual serial port.

C) A TSP program that runs on a Keithley controls the board through the Digital I/O port.

D) The board is manually controlled through a simple webpage.

E) An app connects to the board through the boards Bluetooth or WIFI and manually controls it (this may take a lot of effort as I don't have experience with mobile phone programming).

F) The board controls the instrument(s), and makes the measurements itself through its WIFI.

G) The board is controlled through an ethernet connection (So far it does not support ethernet, but it could be added, but I may run short on pins)

H) Multiple boards are "stacked" to reduce the bench space and used either as a virtual large board or as separated boards.

On some decisions, selection of components and some unsolved issues:

- Price target, as much as I would like to add more features to it, I'm not sure how much would customers be willing to pay for it. Whatever price target I set, the rule of thumb says that final price should be around ~2.5 the cost of the board.

- Of the 3 type of relays, they all have their pros and cons, so its hard to stick to just one type. The 2 ways to support more than one are to either build boards for every type of relay, or to make it possible to solder different relays into the same board.

- I don't like the terminal block that I used. Pluggable block connectors look much more convenient because cables are connected to a block instead of to the board, and also because it is possible to have multiple semipermanent connected blocks which can be quickly plugged into the board.

- In some way this would have to be encased. Laser-cut acrylics could work, but there might be better alternatives.

  • Sign in to reply
Parents
  • shabaz
    shabaz over 3 years ago

    Nice-looking instrument!

    I had these suggestions:

    (a) Maybe change the sense banana sockets to different colors for unambiguity, e.g. orange and blue instead of red and black perhaps

    (b) spread them out, i.e make the board bigger, so that the connectors don't need to be so close. I don't think anyone would mind if the board was bigger.

    (c) Either for all of the sense relays, or for a couple of them, have space for a footprint for normal relays too, so that users can choose themselves to solder in reed relays or normal relays in those positions. That way, the board can be used for injecting source signals/power as well as measuring. For source signals, the users would apply that to the sense terminals (orange/blue or whatever)

    (d) If it's not already present, a temperature sensor chip on-board could be handy for recording ambient temperature

    (e) A minor thing, perhaps either a row of LEDs at the front, or a 7-segment LED showing which connections are made could be handy. The LEDs seem to be in an inconvenient place, since they won't be visible in a testbed perhaps. I guess it could even be a separate small board with flat flex cable, to mount it wherever desired.

    Anyway, these are just some ideas, maybe not important/relevant. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neuromodulator
    neuromodulator over 3 years ago in reply to shabaz

    Thanks for all the suggestions. 
    A) Here I'm doing it the same way as they do it on instruments, using the same colors for in the sense and input plugs. I suppose the reason behind it is that mixing them up is not a problem as long as polarity stays correct. Orange/blue might still give a good hint on polarity though.
    B) The board was made 10 x 10 cm just to keep price low at JLC, but I'll eventually move to something bigger, and there it would make sense to spread them
    C) The current reed relays support up to 1A, which i think is ok for many application, but I agree that supporting electromechanical ones would give better flexibility. A single PCB that supports reed and electromechanical is definitely a good idea if I can mange to support both so as they use the same physical space. I would use DTSP or DPDT there so even when they would be larger, they probably would use less space than 2 reed ones.

    D) That could be interesting too, and it could help with thermocouple measurement too.
    E) Yes from that image they are hardly visible, even though I made as much space as I could. On a bigger board It should be easier to see them, and 7 would be helpful. But I would not remove the LEDs next to output, since they are more visual as to where the signal is going.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to neuromodulator

    By coincidence I had a similar-ish requirement for two relays on a board recently (not reed relays in this case), and I messed about with the footprint and settled on this! It's a bit ugly (and not great for mains where pads would be exposed on the top side of the board), but it is what it is. I was trying to accomodate two relay sizes since there are often component shortages.

    image

    I also tried doing something similar with BNC, not sure if this will be successful! It was to accomodate many different BNC sockets (some have the pins at 45 degrees for the same orientation of the connector side, hence the star-pattern! I think I messed up the hole dimensions however, but I'll know soon enough when the PCBs arrive:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neuromodulator
    neuromodulator over 3 years ago in reply to shabaz

    Why didn't you align the pins of those relays?

    In the case of the reed ones the pins are inline so I will have to see how they can be used to fit in the same space?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neuromodulator
    neuromodulator over 3 years ago in reply to shabaz

    Why didn't you align the pins of those relays?

    In the case of the reed ones the pins are inline so I will have to see how they can be used to fit in the same space?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 3 years ago in reply to neuromodulator

    I could, but I'm not settled on the relay choices or pinouts, so it's likely I will need to stagger.

    Currently I'm lucky the two relays I've got are similar footprint, just one is longer. But I'm not happy with either of them, because of the cost (£8 and £12) because of the certifications. I want to find cheaper latching relays.

    image 

    • Cancel
    • Vote Up 0 Vote Down