PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs Raspberry Pi RP2350 based PCB design
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: embeddedguy
  • Date Created: 19 Jun 2025 8:16 AM Date Created
  • Views 3114 views
  • Likes 10 likes
  • Comments 16 comments
  • pcb
  • raspberry pi
  • rp2040
Related
Recommended

Raspberry Pi RP2350 based PCB design

embeddedguy
embeddedguy
19 Jun 2025

Sometimes back, I was designing a PCB based on RP2350 and now I received the finished PCB. So this post is about the experience that I would like to share about my PCB design.

Firstly, the original plan of creating this PCB was to create RP2350 based Single Pair Ethernet development board. For that I had used ADIN-1111 chip. Unfortunately, it was not available during the PCBA making. Hence the original idea was not possible. But I have tested the RP2350 chip and it is working fine.  The design is based on KiCAD and is 4-layer design.

The easiest idea to test this board is to use Micropython so that the board can be tested fast. I tested a simple blink program on this board and it works fine.

image

image

imageimage

image

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • BigG
    BigG over 1 year ago +1
    Very nice. Does your SPE board include PoDL (power over data lines)? That's a design challenge just on it's own. I've always fancied the microchip SPE ICEs over ADIN-1111, purely on price. I see Arduino…
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 1 year ago

    Interesting.

    Are you going to test the SPE in the future, now that the ADIN-1111 is available at Digikey or LCSC?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 1 year ago in reply to wolfgangfriedrich

    Yes, I will for sure, I received this PCB two days ago. I was waiting for it to arrive and check that it is working.

    Also, I need to find someone who can probably do SMD soldering because I have tried that in the past and I cannot.Smirk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 1 year ago in reply to embeddedguy

    Stencils are now an easy add-on when getting boards made at fab house. Then just need solder paste and hot plate. It's never perfect but SMD soldering this method is also easier than anticipated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 1 year ago in reply to BigG

    Right. Thanks for this nice suggestion. 
    I will keep making PCBs and next time I will try to get when ordering the PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to embeddedguy

    For future reference it is possible to hand solder (using a soldering iron) QFN parts like the ADIN chip.

    The trick is to make a footprint with a single large hole for the big centre pad. Make the hole as big as you can without breaking out of the pad.

    To solder the chip, apply solder past with a small pointy thing (I would use a needle in a holder)  - it doesn't matter if the paste bridges the outer pads but try not to bridge from the signal pads to the centre. Don't put any paste on the centre pad.

    Use a spring ar of some kind (I use a bit of bent "piano" wire held in a tiny vice) to hold the chip in place on the board and reflow the paste on the outer pads with a hot and very fine tipped soldering iron. It will need to be hot to get any heat down a really fine needle tip. Don't worry about bridging outer pads or soldering all of them.

    Once the paste has all been melted apply a lot of really runny flux (I use Warburtons 315))

    image

    You can get this from Rapid Electronics.

    Touch up the solder on the outer pads to solder any that are not and remove bridges. If there is too much solder remove some with solder wick. Keep it fluxy !

    Then solder the chip centre pad (if a connection is needed) using a bigger iron bit and some wire solder.

    Don't solder the centre pad unless you have to !

    The big centre hole concept is useful for removing chips even if you have a full reflow set up. Only do the multiple tiny holes thing if you need them for RF or thermal purposes.

    Obviously this isn't the ideal way to do things but if you need to add a QFN part after the rest of the board has been re-flowed it's the best cheap way I know. It can, of course, be done better if you have a fancy rework machine costing many £k and all the required add ons.

    It may help solder a QFN if you apply hot air to the underside of the board and get it up to about 120C.

    It is much, much easier to do all this with leaded solder - the unleaded stuff doesn't flow so well and has a much higher melting point.

    You can get ultra low melting point solder which might be even better but I have not tried it.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 1 year ago in reply to BigG

    And the board looks like it has paste already on the un-populated pads. To mount the chip it would need some flux, good enough placement and sufficient heat for assembly. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 1 year ago in reply to wolfgangfriedrich

    Right it has the paste already in place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • embeddedguy
    embeddedguy over 1 year ago in reply to wolfgangfriedrich

    Right it has the paste already in place.